![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
Linear Technology DC1190A Demonstration Board. More...
Linear Technology DC1190A Demonstration Board.
LTC2360-12: 12-Bit, 100Ksps ADC. LTC2361-12: 12-Bit, 250Ksps ADC. LTC2362-12: 12-Bit, 500Ksps ADC LTC2365-12: 12-Bit, 1Msps ADC LTC2366-12: 12-Bit, 3Msps ADC
NOTES Setup: Set the terminal baud rate to 115200 and select the newline terminator. Equipment required is a voltage source (preferably low-noise) and a precision voltmeter. Ensure all jumpers on the demo board are installed in their default positions from the factory. Refer to Demo Manual DC1190A. How to test: The voltage source should be connected to input AIN. Ensure the input is within its specified absolute input voltage range. (It is easiest to tie the voltage source negative terminal to COM.) Ensure the voltage source is set within the range of 0V to +2.5V for low range, or within 0V to +3V for high range. USER INPUT DATA FORMAT: decimal : 1024 hex : 0x400 octal : 02000 (leading 0 "zero") binary : B10000000000 float : 1024.0
http://www.linear.com/product/LTC2360-12 http://www.linear.com/product/LTC2361-12 http://www.linear.com/product/LTC2362-12 http://www.linear.com/product/LTC2365-12 http://www.linear.com/product/LTC2366-12
http://www.linear.com/product/LTC2360-12#demoboards http://www.linear.com/product/LTC2361-12#demoboards http://www.linear.com/product/LTC2362-12#demoboards http://www.linear.com/product/LTC2365-12#demoboards http://www.linear.com/product/LTC2366-12#demoboards
Copyright 2018(c) Analog Devices, Inc.
All rights reserved.
Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:
THIS SOFTWARE IS PROVIDED BY ANALOG DEVICES "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, NON-INFRINGEMENT, MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL ANALOG DEVICES BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, INTELLECTUAL PROPERTY RIGHTS, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
Definition in file DC1190A.ino.
Go to the source code of this file.
Functions | |
| static void | print_title () |
| Prints the title block when program first starts. More... | |
| static void | print_prompt () |
| Prints main menu. More... | |
| static void | print_user_command (uint8_t menu) |
| static void | menu_1_read_input () |
| Read channel. More... | |
| static void | menu_2_select_vref () |
| static void | setup () |
| Initialize Linduino. More... | |
| static void | loop () |
| Repeats Linduino loop. More... | |
Variables | |
| static uint8_t | LTC2366_bits = 12 |
| Default set for 12 bits. More... | |
| static float | LTC2366_vref = 2.5 |
| Default set for 2.5V with JP1 in the 2.5V position. More... | |
|
static |
Repeats Linduino loop.
Definition at line 124 of file DC1190A.ino.
|
static |
|
static |
|
static |
Prints main menu.
Definition at line 203 of file DC1190A.ino.
|
static |
Prints the title block when program first starts.
Definition at line 182 of file DC1190A.ino.
|
static |
|
static |
Initialize Linduino.
Definition at line 110 of file DC1190A.ino.
|
static |
Default set for 12 bits.
Definition at line 105 of file DC1190A.ino.
|
static |
Default set for 2.5V with JP1 in the 2.5V position.
Definition at line 106 of file DC1190A.ino.