![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
Linear Technology DC1096B Demonstration Board. More...
Linear Technology DC1096B Demonstration Board.
LTC2642: 16-/14-/12-Bit VOUT DAC with SPI Interface
LTC2641: 16-/14-/12-Bit VOUT DAC with SPI Interface
NOTES Set the terminal baud rate to 115200 and select the newline terminator. No external power supply is required. Two on-board reference voltages of 2.5V and 5V are available. The board features LTC2642A with direct and buffered output. The program displays calculated voltages which are based on the reference voltage used. A precision voltmeter is needed to verify the actual measured voltages against the calculated voltage displayed. There is also an option of generating a square wave of required voltage levels and frequency. This proves the fast settling time of the corresponding parts. Setting the software to unipolar or bipolar will not set the hardware to bipolar mode. The jumpers need to be placed in their proper positions in order to accomplish this. Jumper settings: JP3: Sets DAC2 to either unipolar or bipolar mode. In bipolar mode, set JP6 and JP7 to EXT and apply an appropriate supply to AMP V+, AMP V–, and GND turret posts. JP4: Sets DAC3 to either unipolar or bipolar mode. In bipolar mode, set JP6 and JP7 to EXT and apply an appropriate supply to AMP V+, AMP V–, and GND turret posts. Explanation of Commands: Option 1: Enter a digital value or voltage to obtain analog voltage output. Option 2: Enter the voltage levels to obtain a square wave. Option 3: Vary the reference voltage used. Option 4: Select Bipolar/Unipolar. USER INPUT DATA FORMAT: decimal : 1024 hex : 0x400 octal : 02000 (leading 0 "zero") binary : B10000000000 float : 1024.0
http://www.linear.com/product/LTC2642 http://www.linear.com/product/LTC2641
http://www.linear.com/product/LTC2642#demoboards http://www.linear.com/product/LTC2641#demoboards
Copyright 2018(c) Analog Devices, Inc.
All rights reserved.
Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:
THIS SOFTWARE IS PROVIDED BY ANALOG DEVICES "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, NON-INFRINGEMENT, MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL ANALOG DEVICES BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, INTELLECTUAL PROPERTY RIGHTS, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
Definition in file DC1096B.ino.
Go to the source code of this file.
Functions | |
| static void | print_title () |
| Prints the title block when program first starts. More... | |
| static void | print_prompt () |
| Prints main menu. More... | |
| static uint8_t | menu1_voltage_output () |
| Function to enter a digital value and get the analog output. More... | |
| static uint8_t | menu2_square_wave_output () |
| Function to generate a square wave of desired frequency and voltage ranges. More... | |
| static void | menu3_change_reference_voltage () |
| Function to change the reference voltage to be used. More... | |
| static void | menu4_select_range () |
| Select between unipolar/bipolar. More... | |
| static void | setup () |
| Initialize Linduino. More... | |
| static void | loop () |
| Repeats Linduino loop. More... | |
| static int16_t | prompt_voltage_or_code () |
| Prompt user to enter a voltage or digital code to send to DAC. More... | |
| static uint16_t | get_voltage () |
| Get voltage from user input, calculate DAC code based on lsb, offset. More... | |
| static uint16_t | get_code () |
| Get code to send to DAC directly, in decimal, hex, or binary. More... | |
Macros | |
| #define | VREF1 5.0 |
| #define | VREF2 2.5 |
Enumerations | |
| enum | { PROMPT_VOLTAGE = 0, PROMPT_CODE = 1 } |
| Used to choose between voltage and code. More... | |
Variables | |
| static float | reference_voltage = VREF1 |
| static uint8_t | range = UNIPOLAR |
|
static |
Get code to send to DAC directly, in decimal, hex, or binary.
Definition at line 300 of file DC1096B.ino.
|
static |
Get voltage from user input, calculate DAC code based on lsb, offset.
Definition at line 287 of file DC1096B.ino.
|
static |
Repeats Linduino loop.
Definition at line 152 of file DC1096B.ino.
|
static |
Function to enter a digital value and get the analog output.
Definition at line 186 of file DC1096B.ino.
|
static |
Function to generate a square wave of desired frequency and voltage ranges.
Definition at line 206 of file DC1096B.ino.
|
static |
Function to change the reference voltage to be used.
Definition at line 241 of file DC1096B.ino.
|
static |
Select between unipolar/bipolar.
Definition at line 250 of file DC1096B.ino.
|
static |
Prints main menu.
Definition at line 326 of file DC1096B.ino.
|
static |
Prints the title block when program first starts.
Definition at line 314 of file DC1096B.ino.
|
static |
Prompt user to enter a voltage or digital code to send to DAC.
Definition at line 272 of file DC1096B.ino.
|
static |
Initialize Linduino.
Definition at line 129 of file DC1096B.ino.
| #define VREF1 5.0 |
Definition at line 106 of file DC1096B.ino.
| #define VREF2 2.5 |
Definition at line 107 of file DC1096B.ino.
| anonymous enum |
Used to choose between voltage and code.
| Enumerator | |
|---|---|
| PROMPT_VOLTAGE | 0 |
| PROMPT_CODE | 1 |
Definition at line 122 of file DC1096B.ino.
|
static |
Definition at line 111 of file DC1096B.ino.
|
static |
Definition at line 110 of file DC1096B.ino.