![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
Linear Technology DC1011A-B Demonstration Board. More...
Linear Technology DC1011A-B Demonstration Board.
LTC2496: 16-Bit 8-/16-Channel Delta Sigma ADC with Easy Drive Input Current Cancellation
NOTES
Setup:
Set the terminal baud rate to 115200 and select the newline terminator.
Equipment required is a precision voltage source and a precision
voltmeter. No external power supply is required. Ensure all jumpers on
the demo board are installed in their default positions from the
factory.
How to test Single-Ended mode:
The voltage source should be connected to the ADC such that the negative
lead is connected to COM. The positive lead may be connected to any
channel input. Ensure voltage is within analog input voltage range -2.5V to
+2.5V.
How to test Differential Mode:
The voltage source should be connected with positive and negative leads to
paired channels. The voltage source negative output must also be connected to
the COM pin in order to provide a ground-referenced voltage. Ensure voltage is
within analog input voltage range -2.5V to +2.5V. Swapping input voltages
results in a reversed polarity reading.
USER INPUT DATA FORMAT:
decimal : 1024
hex : 0x400
octal : 02000 (leading 0 "zero")
binary : B10000000000
float : 1024.0http://www.linear.com/product/LTC2496
http://www.linear.com/product/LTC2496#demoboards
Copyright 2018(c) Analog Devices, Inc.
All rights reserved.
Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:
THIS SOFTWARE IS PROVIDED BY ANALOG DEVICES "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, NON-INFRINGEMENT, MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL ANALOG DEVICES BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, INTELLECTUAL PROPERTY RIGHTS, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
Definition in file DC1011AB.ino.
Go to the source code of this file.
Functions | |
| static void | print_title () |
| Prints the title block when program first starts. More... | |
| static void | print_prompt () |
| Prints main menu. More... | |
| static void | print_user_command (uint8_t menu) |
| Display selected differential channels. More... | |
| static uint8_t | menu_1_read_single_ended () |
| read from ADC single-ended More... | |
| static uint8_t | menu_2_read_differential () |
| Read channels in differential mode. More... | |
| static void | setup () |
| Initialize Linduino. More... | |
| static void | loop () |
| Repeats Linduino loop. More... | |
Variables | |
| static uint8_t | demo_board_connected |
| Set to 1 if the board is connected. More... | |
| static float | reference_voltage = 5 |
| The reference voltage range, set to 5v through JP2 and JP3 by default. More... | |
| const uint16_t | MISO_TIMEOUT = 1000 |
| The MISO timeout (ms) More... | |
| const uint8_t | BUILD_COMMAND_SINGLE_ENDED [16] |
| Builds the command for single-ended mode. More... | |
| const uint8_t | BUILD_COMMAND_DIFF [16] |
|
static |
Repeats Linduino loop.
Definition at line 166 of file DC1011AB.ino.
|
static |
read from ADC single-ended
Definition at line 230 of file DC1011AB.ino.
|
static |
Read channels in differential mode.
Definition at line 308 of file DC1011AB.ino.
|
static |
Prints main menu.
Definition at line 218 of file DC1011AB.ino.
|
static |
Prints the title block when program first starts.
Definition at line 202 of file DC1011AB.ino.
|
static |
Display selected differential channels.
Displaying Single-Ended channels is straightforward; not so with differential because the inputs can take either polarity.
| menu | the selected channels |
Definition at line 398 of file DC1011AB.ino.
|
static |
Initialize Linduino.
Definition at line 148 of file DC1011AB.ino.
| const uint8_t BUILD_COMMAND_DIFF[16] |
Definition at line 128 of file DC1011AB.ino.
| const uint8_t BUILD_COMMAND_SINGLE_ENDED[16] |
Builds the command for single-ended mode.
Definition at line 109 of file DC1011AB.ino.
|
static |
Set to 1 if the board is connected.
Definition at line 103 of file DC1011AB.ino.
| const uint16_t MISO_TIMEOUT = 1000 |
The MISO timeout (ms)
Definition at line 107 of file DC1011AB.ino.
|
static |
The reference voltage range, set to 5v through JP2 and JP3 by default.
Definition at line 104 of file DC1011AB.ino.