|
MAXREFDES62# Code Documentation
V01.00
RS-485 Micro PLC
|
Go to the source code of this file.
Functions | |
| void | maxim_uart_init (void) |
| Initialize the UART peripheral. | |
| void | maxim_gpio_init (void) |
| Initialize the GPIO peripheral. | |
******************************************************
Project: MAXREFDES62# Filename: init_config.h Description: This module contains all the functions used to initialize the STM32F1 peripherals
Revision History:
9-17-2014 Rev 01.00 GL Initial release.
This code follows the following naming conventions:
char ch_pmod_value
char (array) s_pmod_string[16]
float f_pmod_value
int n_pmod_value
int (array) an_pmod_value[16]
u16 u_pmod_value
u16 (array) au_pmod_value[16]
u8 uch_pmod_value
u8 (array) auch_pmod_buffer[16]
unsigned int un_pmod_value
int * pun_pmod_value
Definition in file init_config.h.
| void maxim_gpio_init | ( | void | ) |
Initialize the GPIO peripheral.
| None |
| None |
Definition at line 171 of file init_config.c.
| void maxim_uart_init | ( | void | ) |
Initialize the UART peripheral.
| None |
| None |
Definition at line 71 of file init_config.c.