DEMO BOARD DC239A ASSEMBLY NOTES, UNLESS OTHERWISE SPECIFIED...

 1. DOCUMENTATION PRECEDENCE IN DESCENDING ORDER:
    PURCHASE ORDER, THIS DOCUMENT, IPC-A-610B.

 2. WORKMANSHIP SHALL BE IN ACCORDANCE WITH IPC-A-610B.

 3. (BLANK)

 4. NOTE POSITIONS OF POLARIZED COMPONENTS.

 5. COMPONENTS ARE MOUNTED ON 1-SIDE(s) OF THE BOARD.
    SECURE STANDOFFS TO THE BOTTOM OF THE BOARD.

 6. ASSEMBLY PROCESSES SHALL INCLUDE:
    REFLOW SOLDER TOP SIDE.
    WAVE SOLDER BOTTOM.
       OPTION: HAND SOLDER THRU-HOLE COMPONENTS.

 7. USE ASCII CENTROID DATA FOR AUTOMATED SURFACEMOUNT PLACEMENT.
    ROTATION DATA IS RELATIVE TO THE FOOTPRINT LIBRARY, AND
    THEREFOR MAY NEED TO BE ALTERED DURING PROGRAMMING.

 8. PARTS TO OMIT WILL BE SO SPECIFIED IN THE PARTS LIST.
    PRIOR TO WAVE SOLDERING, MASK WHERE THD-PARTS ARE OMITTED.
    MASK THE SOLDER STENCIL WHERE SMT PARTS ARE OMITTED.

 9. SHORTAGES SHALL EXIST ON THE MINIMUM NUMBER OF BOARDS.

10. DO NOT OTHERWISE MARK BOARDS (e.g. NO QA-STAMP).

11. ADHERE TO TEMPERATURE PROFILES, WHEN PROVIDED.

12. DEPANELIZE BOARDS AFTER ASSEMBLY.

13. TRIM LEADS WHEN APPLICABLE.

END.