The adl5205 control software requires the ADL5205-EVALZ evaluation board connected through Analog Devices SDP-S controller board (EVAL-SDP-CS1Z), available from the ADI website at www.analog.com/sdp.

Connect the SDP-S controller (USB interface) board to the ADL5205-EVALZ eval board. Connect the USBcable from the PC to the SDP-S board.  Apply 5V or 3.3V supply and input and output cables to the ADL5205-EVALZ.  More information on the ADL5205 control software and the needed configuration of the ADL5205-EVALZ are available from the ADL5205 datasheet (http://www.analog.com/en/products/rf-microwave/rf-amplifiers/rfif-differential-amps/adl5205.html)

Installation instructions for adl5205_regwr software:
1. Extract .zip file
2. Run SDP driver installer, SDPDrivers.exe
3. Copy adl5205_regwr_1r3.exe and sdpApi1.dll to a directory where the software will be running in.
4. Issue the command "adl5205_regwr_1r3" with the list of desired arguments.