TMWritePacket Overview GroupThe TMWritePacket API call writes a Universal Data Packet (UDP) starting on 'start_page' in a 1-Wire device. The 'num_write' bytes of data in 'write_buffer' is written. Returns a byte length greater than or equal to 0 for success or one of the TRANSPORT error values for a failure. TMWritePacket works only with the nvram 1-Wire devices such as the DS1993 iButton. See the description of the Universal Data Packet.
For a description of the above types, see the TMEX Type Descriptions.
Parameters
session_handle
Specifies the session handle returned from the API function TMExtendedStartSession that specifies the desired 1-Wire network port. This parameter is required by most TMEX API functions.
state_buffer
Specifies a pointer to a memory location that TMEX keeps all of the state information for the 1-Wire networks. This parameter is required by most TMEX API functions.
start_page
Specifies the page that the packet will begin being written at. A CRC-16 verified packet always starts at the beginning of a page boundary. The valid range of a start page depends on the device type. Current 1-Wire devices range from 0 to 256 pages.
write_buffer
Specifies a pointer to a memory location that contains the data to write. The amount of data to write is expressed in ‘num_write’.
num_write
Specifies the number of bytes in the ‘write_buffer’ to write.
Return Value
>=0 => length of valid data writtenSee Also