TMEX Type DescriptionsGeneral Types
short 16 bit signed integer
long 32 bit signed integer
char 8 bit signed number
unsigned char 8 bit unsigned number
far pascal far function using pascal calling convention
void far * generic far pointer
short far * far pointer to a 16 bit signed integer
TMEX Specific Types
FileEntry structure containing all of the information on a TMEX file
DirectoryPath structure containing all of the information on a TMEX Directory path
Specification structure containing descriptive information for each 1-Wire device based on its family code