TMSetup Overview GroupThe TMSetup API function must be called before any other TMEX functions except the Session layer of API calls. No other TMEX API calls will operate correctly until the 1-Wire network has been called with this function. It is intended to be called once at the beginning of an application to initialize the 1-Wire network and verify the physical integrity of the 1-Wire network. Note that execution of this function will reset all the parts on the specified 1-Wire network.
For a description of the above types, see the TMEX Type Descriptions.
Parameters
session_handle
Specifies the session handle returned from the API function TMExtendedStartSession that specifies the desired 1-Wire network port. This parameter is required by most TMEX API functions.
Return Value
0 => Setup failed.
1 => Setup ok.
2 => Setup ok but 1-Wire network shorted.
3 => 1-Wire network does not exist.
4 => TMSetup not supported
< 0 => TMEX Hardware Specific Error Return Codes
See Also