TMOneWireCom Overview GroupThe TMOneWireCom API call reads (‘Operation’ = 1) or sets (‘Operation’ = 0) the 1-Wire communication state. The following are the values allowed for ‘TimeMode’:
00 hex - Normal timing (15-60 microsecond time slots)
01 hex - Overdrive timing
02 hex - Relaxed timing for long lines
Note that not all of the above modes will be available for all hardware platforms.
For a description of the above types, see the TMEX Type Descriptions.
Parameters
session_handle
Specifies the session handle returned from the API function TMExtendedStartSession that specifies the desired 1-Wire network port. This parameter is required by most TMEX API functions.
operation
Specifies whether reading or setting the 1-Wire network communication rate. (1) indicates reading and (0) indicates setting.
TimeMode
Specifies the 1-Wire network communication rate if the ‘Operation’ parameter is (0) for setting.
Return Value
>=0 => TimeMode that was set or read.
<0 => TMEX Hardware Specific Error Return Code
See Also