TMFamilySearchSetup Overview roupThe TMFamilySearchSetup API call sets the ROM buffer and search status to attempt to find a certain 1-Wire device family type. This does not effect the 1-Wire network in any way, it just sets the search algorithm up to find a certain 1-Wire device family type the next time a search function is called (i.e. TMNext or TMNextAlarm). This function will be successful if the port requested to do this on is valid. This function sets up the search to find a certain type on the next call only if there is one available. If there is not one available, TMNext or TMNextAlarm may still find a device of a different type. The normal sequence to search for a particular family type is as follows:
1) Call TMFamilySearchSetup with the desired family type
2) Call TMNext or TMNextAlarm
3) if step 2 is successful then check the family code using TMRom to see if the correct type was found.
4) if step 2 is not successful or the incorrect family code was found in step 3 then no devices of that type were on the 1-Wire network at the time of the search.
For a description of the above types, see the TMEX Type Descriptions.
Parameters
session_handle
Specifies the session handle returned from the API function TMExtendedStartSession that specifies the desired 1-Wire network port. This parameter is required by most TMEX API functions.
state_buffer
Specifies a pointer to a memory location that TMEX keeps all of the state information for the 1-Wire networks. This parameter is required by most TMEX API functions.
family_type
Specifies the family type to search for on the next search function call. Each 1-Wire device type has an associated family type number.
Return Value
1 => search setup to find family_type
<0 => TMEX Network Error Return Code
See Also
TMNext, TMSkipFamily, TMRom, TMNextAlarm