1-Wire File Structure OverviewThe definitions and rules of the 1-Wire File Structure are sufficient to store multiple files in nested directories using device capacities up to 64K bytes. These devices may be organized as 4...256 pages of 32...256 bytes. The rules given in this document are scaleable to all combinations of memory organization within this range. (Note that in all discussions of iButton data structure, the first available page of memory is called page 0.)
The TMEX API implements a subset of the following 1-Wire File Structure specification.
Data Organization
The data organization of the 1-Wire File Structure is very similar to that of a floppy disk. A sector of a floppy roughly corresponds to a page of an iButton. The directory tells which files are stored, where the data is located in the device, and how many pages it occupies. In this way information can be randomly accessed for quick response.
The organization of data within a page of a file or directory is shown below. (The numbers shown assume a 32 byte page length, but the same structure applies for devices with page lengths up to 256 bytes.)
+-------------------------------------------------------+
| length | data | cont.- | /CRC16 | not |
| binary |ASCII or binary| pointer | binary | used |
| 1...29 | | binary | | |
| 1 byte | 0 to 28 bytes | 1 byte | 2 bytes | 28 to 0 |
+-------------------------------------------------------+
Each page of a file or directory begins with a length byte, contains a continuation pointer, and ends with an inverted CRC16 check. The continuation pointer is the page address where the file or directory is continued. A continuation pointer value of 0 marks the last page. The length byte indicates how many valid bytes a page contains, not counting the length byte itself or the CRC. The CRC calculation, however, also includes the length byte. The CRC accumulator is initialized by setting it equal to the iButton page number. Every byte of a page is transmitted to or from an iButton least significant bit first. The length byte is the first to be transmitted. Of the two CRC bytes, the least significant will be sent first.
Each touch memory must be formatted before it can be used with the 1-Wire file structure. During the process of formatting, the root directory file is created. The root directory always begins in the first page of the iButton (page 0). The organization of data within the first page of the root directory is shown below:
+-------------------------------------------------------+
| length |control| file entries |cont.- |/CRC16 | not |
| binary | data |ASCII & binary|pointer|binary | used |
| 8...29 | | |binary | | |
| 1 byte |7 bytes| 0 to 21 bytes|1 byte |2 bytes|21 to 0|
+--------+-------+--------------------------------------+
| |
+--------+ +--------------------------------------+
| |
+-------------------------------------------------------|
| directory | re- | bitmap | bitmap of used pages or |
| mark |served| control | address of bitmap file |
| "AA" | "00" | xyyyyyzp | 4 byte binary number |
| 1 byte |1 byte| 1 byte | LS-byte/ / /MS-byte |
+-------------------------------------------------------+
Instead of data, the directory contains management information and file entries. The control field of seven bytes has the same length as a file entry. The bitmap supports TMEX in allocation of memory space for writing files. In the bitmap, used pages are marked with a 1, empty pages with a 0. The least significant bit corresponds to page 0. This local bitmap is only used for non-EPROM devices with less then 32 pages of data. All other devices have remote bitmap files. In large NV-RAM iButton the bitmap file page number refers to normal data space. In EPROM devices the page number refers to status memory. For EPROM devices the unprogrammed state is 1 and the programmed state is 0. Due to this constraint the bits in the EPROM bitmap's are inverted. An empty page has a 1 and an occupied page has a 0.
The most significant bit, "x", of the bitmap control byte specifies whether the bitmap is stored immediately in the first directory packet or in a separate file. If this bit is a 1, the 4 byte bitmap immediately follows the bitmap control byte. If this bit is a 0, the two bytes following the bitmap control byte are zero. The "y" bits in the bitmap control byte specify directory attributes. These bits are from most significant to least significant.
read-only : The directory that contains this attribute and all files and sub-directories can be read but not deleted or modified. If it is set on the root level then the entire device is read-only.The "z" bit in the bitmap control byte is not used. The least significant bit "p" is an in-progress bit. This bit can be set when doing non-interruptible operations like file optimization. Note that TMEX does not set this attribute because none of its operations are non-interruptible. The bit is cleared after the operations are complete.
The next two bytes contain the starting page address and the number of pages required by the bitmap file. Note that the bitmap or the nameless bitmap file is created during the process of formatting. Continuation pages of the directory don't need a control field. This space is available to store another file entry.
File entries consist of the 4-byte file name, one-byte file extension, the starting page address where the file begins, and the number of pages the file occupies. This structure is shown below:
+---------------------------------------------------------+
| file name | extension | start page | # pages |
| ASCII, blank filled, | binary | binary | binary |
| left justified | aeeeeeee | | |
| 4 bytes | 1 byte | 1 byte | 1 byte |
+---------------------------------------------------------+
File names must consist of ASCII characters only, as with DOS. However, if the first byte of a file entry has a value greater than 127, then it represents the first byte of an extended directory entry. The extended directory entry is a 7-byte or multiple 7-byte data packet that applies to the next directory entry. Each 7-byte data packet must have a first byte greater than 127. The additional bytes in an extended directory entry may be used to specify additional file attributes, passwords, file ownership, date/time stamps, and other special-purpose information regarding the file.
The 7 least significant "e" bits of the extension represent the extension number of the file entry. Extensions 0-99 decimal are reserved for normal file entries, 100 for an AddFile that resides on an EPROM iButton device and 101 for a Monetary File that is only created on a DS1962, DS1963, DS2422 and DS2423. The data page of the Monetary File can only be located on a page that has a corresponding counter. If a page with a counter is not available on the device then the Monetary File will not be created. Extension 127 decimal designates a sub-directory. Extensions 102-126 are reserved for future specialty file types. The most significant bit of the file extension "a" is an attribute flag for the entry. If it is set and the entry is a normal file with extensions 0-99 then the file is read-only. If it is set and the entry is a sub-directory with extension 127 then the sub-directory is hidden. File entries denoting sub-directories contain the real "start page" of the sub-directory file. The "# pages" specifier for a sub-directory entry does not contain a valid number. It always contains 0 and need not be updated when the length of a sub-directory file changes. A sub-directory file contains a back reference to the next higher directory file. If there is no higher sub-directory file the entry will be "ROOT". The start page of ROOT is always 0. The first packet of a sub-directory file has the following structure:
+-------------------------------------------------------+
| length |control| file entries |cont.- |/CRC16 | not |
| binary | data |ASCII & binary|pointer|binary | used |
| 8...29 | | |binary | | |
| 1 byte |7 bytes| 0 to 21 bytes|1 byte |2 bytes|21 to 0|
+--------+-------+--------------------------------------+
| |
+--------+ +--------------------------------------+
| |
+-------------------------------------------------------|
| directory | re- | reference to higher | start page |
| mark |served| directory level | higher dir. |
| "AA" | "00" | ASCII | binary |
| 1 byte |1 byte| 4 bytes | 1 byte |
+-------------------------------------------------------+
Again, the numbers shown above presume a 32-byte page length, but the basic structure applies for greater page lengths. A continuation packet of a root directory or a sub-directory file follows the definition of a data packet. It has the following structure:
+-------------------------------------------------------+
| length | file entries | cont.- | /CRC16 | not |
| binary | ASCII & binary| pointer | binary | used |
| 1...29 | (0 ... 4) | binary | | |
| 1 byte | 0 to 28 bytes | 1 byte | 2 bytes | 28 to 0 |
+-------------------------------------------------------+
The 1-Wire File Structure is carefully designed to provide high speed and optimal performance in a Touch environment. Every memory page can be read, CRC-checked or written without the need to access other pages. If a file is modified, only the affected pages need to be rewritten. This provides a significant speed advantage. Pages of a file need not be contiguous. Files can be extended by redefining continuation pointers. Files can be grouped into nested sub-directories. Attributes defined for a directory apply for all files within it. The iButton file structure also accommodates future types of iButtons with up to 256 pages with a maximum of 256 bytes per page.
The notes below summarize many of the significant properties of the 1-Wire File Structure as specified above. These notes may be helpful in understanding the implications of the 1-Wire File Structure with regard to data storage and management.
See Also