TMEndSession Overview GroupThe TMEndSession API call ends the session on the 1-Wire network that was designated by the session handle 'session_handle'. It returns a 1 if the session specified by 'session_handle' was successfully closed, and 0 if there was no valid session established with the specified session handle.
For a description of the above types, see the TMEX Type Descriptions.
Parameters
session_handle
Specifies session handle on an 1-Wire network. The session handle must be set as a result of a call to TMExtendedStartSession.
Return Value
0 => session_handle already invalid
1 => session ended, session_handle no longer valid
<0 => TMEX Session Error Return Codes
See Also
TMExtendedStartSession, TMValidSession