TMDirectoryMR Overview GroupThe TMDirectoryMR API call Makes or Removes a sub-directory from the current directory. There is an 'operation' flag that indicates if the call is to make or remove a sub-directory. Here are the values of 'operation':
0 : make sub-directory specified by FileEntry 'dir_buf'
1 : remove sub-directory specified by FileEntry 'dir_buf'
Only the 'name' field of the FileEntry structure need be filled in before calling TMDirectoryMR. Note that a sub-directory is created empty and only an empty sub-directory can be removed.
For a description of the above types, see the TMEX Type Descriptions.
Parameters
session_handle
Specifies the session handle returned from the API function TMExtendedStartSession that specifies the desired 1-Wire network port. This parameter is required by most TMEX API functions.
state_buffer
Specifies a pointer to a memory location that TMEX keeps all of the state information for the 1-Wire networks. This parameter is required by most TMEX API functions.
operation
Specifies whether making or removing the current directory. (1) indicates removing and (0) indicates making.
fentry
Specifies a pointer to a memory location that contains a FileEntry structure. This structure must have the name and extension portions set before calling this API.
Return Value
1 => operation is successful
<0 => TMEX File Operations Error Return Code
See Also
TMChangeDirectory, TMFirstFile