TMDeleteFile Overview GroupThe TMDeleteFile API call deletes the file specified in the FileEntry structure 'fentry'. Only the 'name' and 'extension' portions of 'fentry' need be set before calling TMDeleteFile. The file must be in the current directory on the current device on the 1-Wire network specified by the session handle 'session_handle'.
For a description of the above types, see the TMEX Type Descriptions.
Parameters
session_handle
Specifies the session handle returned from the API function TMExtendedStartSession that specifies the desired 1-Wire network port. This parameter is required by most TMEX API functions.
state_buffer
Specifies a pointer to a memory location that TMEX keeps all of the state information for the 1-Wire networks. This parameter is required by most TMEX API functions.
fentry
Specifies a pointer to a memory location that contains a FileEntry structure. This structure must have the name and extension portions set before calling this API.
Return Value
1 => file successfully deleted
<0 => TMEX File Operations Error Return Code
See Also