TMCRC Overview GroupThe TMCRC API call provides CRC calculation facilities. The Type parameter specifies either 8-bit CRC (Type=0) or 16-bit CRC (Type=1). Since the last byte of the unique registration number embedded into every 1-Wire device is an 8-bit CRC, this function call, in 8-bit CRC mode can verify the integrity of a 1-Wire registration number. The 16-bit CRC mode can be used to help make and verify Universal Data Packets (UDPs). Creating UDPs is a TMEX-supported way to packetize data before writing to a 1-Wire device. UDPs use 16-bit CRCs to verify data integrity.
A detailed description of the 8-bit CRC and 16-bit CRC can be found in Application Note 27 “Understanding and Using Cyclic Redundancy Checks with Dallas Semiconductor iButton Products”. The Application Note is located on MAXIM/Dallas Semiconductor’s website: http://pdfserv.maxim-ic.com/arpdf/AppNotes/app27.pdf.
For a description of the above types, see the TMEX Type Descriptions.
Parameters
length
Specifies the length of the buffer to CRC.
buf
Specifies a pointer the byte buffer containing the data.to CRC.
seed
Specifies the CRC seed to use.
Type
Specifies the type of CRC to perform: It can either be an 8-bit CRC (Type=0) or a 16-bit CRC (Type=1)
Return Value
>=0 => the CRC result
<0 => TMEX Transport Error Return Code
See Also