TMClose Overview GroupThe TMClose API call closes access to a particular 1-Wire network. After this function is called on a 1-Wire network, the only way to use it again is to call TMSetup. A common use of this API call is in hardware situations where a port needs to be powered down when not in use. Note that in the Windows situation where multiple programs may be using a 1-Wire network, closing a port may be disastrous so this function is callable but it does not have an effect in Windows.
For a description of the above types, see the TMEX Type Descriptions.
Parameters
session_handle
Specifies the session handle returned from the API function TMExtendedStartSession that specifies the desired 1-Wire network port. This parameter is required by most TMEX API functions.
Return Value
1 => 1-Wire network is closed.
<0 => TMEX Hardware Specific Error Return Code
See Also