TMCloseFile Overview GroupThe TMCloseFile API call closes the file specified by the file handle 'file_handle'. All files that have been opened for reading with TMOpenFile or created for writing with TMCreateFile must be closed after use.
For a description of the above types, see the TMEX Type Descriptions.
Parameters
session_handle
Specifies the session handle returned from the API function TMExtendedStartSession that specifies the desired 1-Wire network port. This parameter is required by most TMEX API functions.
state_buffer
Specifies a pointer to a memory location that TMEX keeps all of the state information for the 1-Wire networks. This parameter is required by most TMEX API functions.
file_handle
Specifies a file handle to release from use.
Return Value
1 => file closed
<0 => TMEX File Operations Error Return Code
See Also