TMAttribute Overview GroupThe TMAttribute API call changes the attributes of the file or directory 'fentry' to the attributes 'attribute'. Only the 'name' and 'extension' portions of 'fentry' need be set before calling TMAttribute. See FileEntry for a description of the type. 'attribute' contains bits that are set to apply an attribute and cleared to remove an attribute. 'bit 0' represents the least significant bit in 'attribute'. Here are the attributes for TMEX 3.00:
bit 0 : set to make file read-only, for files only
bit 1 : set to make directory hidden, for directories only
bit 2-7 : reserved for future attributes
For a description of the above types, see the TMEX Type Descriptions.
Parameters
session_handle
Specifies the session handle returned from the API function TMExtendedStartSession that specifies the desired 1-Wire network port. This parameter is required by most TMEX API functions.
state_buffer
Specifies a pointer to a memory location that TMEX keeps all of the state information for the 1-Wire networks. This parameter is required by most TMEX API functions.
attribute
Specifies an integer with the bit positions representing the attibutes to apply to the file as described above.
fentry
Specifies a pointer to a memory location that contains a FileEntry structure. This structure must have the name and extension portions set before calling this API.
Return Value
1 => file attribute changed to 'attribute'
<0 => TMEX File Operations Error Return Code
See Also