|
1-Wire API for .NET Version 4.00
|
Inherits com::dalsemi::onewire::container::OneWireSensor.
Inherited by OneWireContainer05, OneWireContainer12, OneWireContainer1C, OneWireContainer1F, OneWireContainer29, OneWireContainer3A, and OneWireContainer42.
Public Member Functions | |
| boolean | isHighSideSwitch () |
| Checks to see if the channels of this switch are 'high side' switches. | |
| boolean | hasActivitySensing () |
| Checks to see if the channels of this switch support activity sensing. | |
| boolean | hasLevelSensing () |
| Checks to see if the channels of this switch support level sensing. | |
| boolean | hasSmartOn () |
| Checks to see if the channels of this switch support 'smart on'. | |
| boolean | onlySingleChannelOn () |
| Checks to see if the channels of this switch require that only one channel is on at any one time. | |
| int | getNumberChannels (byte[] state) |
| Gets the number of channels supported by this switch. | |
| boolean | getLevel (int channel, byte[] state) throws OneWireException |
| Checks the sensed level on the indicated channel. | |
| boolean | getLatchState (int channel, byte[] state) |
| Checks the latch state of the indicated channel. | |
| boolean | getSensedActivity (int channel, byte[] state) throws OneWireException |
| Checks if the indicated channel has experienced activity. | |
| void | setLatchState (int channel, boolean latchState, boolean doSmart, byte[] state) |
| Sets the latch state of the indicated channel. | |
| void | clearActivity () throws OneWireException |
Interface class for 1-Wire® switch devices. This class should be implemented for each switch type 1-Wire device.
SwitchContainer extends OneWireSensor, so the general usage model applies to any SwitchContainer:
SwitchContainer Consider this interaction with a SwitchContainer that toggles all of the switches on the device:
//switchcontainer is a com.dalsemi.onewire.container.SwitchContainer
byte[] state = switchcontainer.readDevice();
int number_of_switches = switchcontainer.getNumberChannels(state);
System.out.println("This device has "+number_of_switches+" switches");
for (int i=0; i < number_of_switches; i++)
{
boolean switch_state = switchcontainer.getLatchState(i, state);
System.out.println("Switch "+i+" is "+(switch_state ? "on" : "off"));
switchcontainer.setLatchState(i,!switch_state,false,state);
}
switchcontainer.writeDevice(state);
| void clearActivity | ( | ) | throws OneWireException |
Clears the activity latches the next time possible. For example, on a DS2406/07, this happens the next time the status is read with readDevice().
The activity latches will only be cleared once. With the DS2406/07, this means that only the first call to readDevice() will clear the activity latches. Subsequent calls to readDevice() will leave the activity latch states intact, unless this method has been invoked since the last call to readDevice().
| OneWireException | if this device does not support activity sensing |
Implemented in OneWireContainer05, OneWireContainer12, OneWireContainer1C, OneWireContainer1F, OneWireContainer29, OneWireContainer3A, and OneWireContainer42.
| boolean getLatchState | ( | int | channel, |
| byte[] | state | ||
| ) |
Checks the latch state of the indicated channel.
| channel | channel to execute this operation, in the range [0 to (getNumberChannels(byte[]) - 1)] |
| state | current state of the device returned from readDevice() |
true if channel latch is 'on' or conducting and false if channel latch is 'off' and not conducting. Note that the actual output when the latch is 'on' is returned from the isHighSideSwitch() method.Implemented in OneWireContainer05, OneWireContainer12, OneWireContainer1C, OneWireContainer1F, OneWireContainer29, OneWireContainer3A, and OneWireContainer42.
| boolean getLevel | ( | int | channel, |
| byte[] | state | ||
| ) | throws OneWireException |
Checks the sensed level on the indicated channel.
To avoid an exception, verify that this switch has level sensing with the hasLevelSensing(). Level sensing means that the device can sense the logic level on its PIO pin.
| channel | channel to execute this operation, in the range [0 to (getNumberChannels(byte[]) - 1)] |
| state | current state of the device returned from readDevice() |
true if level sensed is 'high' and false if level sensed is 'low'Implemented in OneWireContainer05, OneWireContainer12, OneWireContainer1C, OneWireContainer1F, OneWireContainer29, OneWireContainer3A, and OneWireContainer42.
| int getNumberChannels | ( | byte[] | state | ) |
Gets the number of channels supported by this switch.
Channel specific methods will use a channel number specified by an integer from [0 to (getNumberChannels(byte[]) - 1)]. Note that all devices of the same family will not necessarily have the same number of channels. The DS2406 comes in two packages--one that has a single channel, and one that has two channels.
| state | current state of the device returned from readDevice() |
Implemented in OneWireContainer05, OneWireContainer12, OneWireContainer1C, OneWireContainer1F, OneWireContainer29, OneWireContainer3A, and OneWireContainer42.
| boolean getSensedActivity | ( | int | channel, |
| byte[] | state | ||
| ) | throws OneWireException |
Checks if the indicated channel has experienced activity.
This occurs when the level on the PIO pins changes. To clear the activity that is reported, call clearActivity(). To avoid an exception, verify that this device supports activity sensing by calling the method hasActivitySensing().
| channel | channel to execute this operation, in the range [0 to (getNumberChannels(byte[]) - 1)] |
| state | current state of the device returned from readDevice() |
true if activity was detected and false if no activity was detected| OneWireException | if this device does not have activity sensing |
Implemented in OneWireContainer05, OneWireContainer12, OneWireContainer1C, OneWireContainer1F, OneWireContainer29, OneWireContainer3A, and OneWireContainer42.
| boolean hasActivitySensing | ( | ) |
Checks to see if the channels of this switch support activity sensing.
If this method returns true then the method getSensedActivity(int,byte[]) can be used.
true if channels support activity sensingImplemented in OneWireContainer05, OneWireContainer12, OneWireContainer1C, OneWireContainer1F, OneWireContainer29, OneWireContainer3A, and OneWireContainer42.
| boolean hasLevelSensing | ( | ) |
Checks to see if the channels of this switch support level sensing.
If this method returns true then the method getLevel(int,byte[]) can be used.
true if channels support level sensingImplemented in OneWireContainer05, OneWireContainer12, OneWireContainer1C, OneWireContainer1F, OneWireContainer29, OneWireContainer3A, and OneWireContainer42.
| boolean hasSmartOn | ( | ) |
Checks to see if the channels of this switch support 'smart on'.
Smart on is the ability to turn on a channel such that only 1-Wire device on this channel are awake and ready to do an operation. This greatly reduces the time to discover the device down a branch. If this method returns true then the method setLatchState(int,boolean,boolean,byte[]) can be used with the doSmart parameter true.
true if channels support 'smart on'Implemented in OneWireContainer05, OneWireContainer12, OneWireContainer1C, OneWireContainer1F, OneWireContainer29, OneWireContainer3A, and OneWireContainer42.
| boolean isHighSideSwitch | ( | ) |
Checks to see if the channels of this switch are 'high side' switches.
This indicates that when 'on' or true, the switch output is connect to the 1-Wire data. If this method returns false then when the switch is 'on' or true, the switch is connected to ground.
true if the switch is a 'high side' switch, false if the switch is a 'low side' switchImplemented in OneWireContainer05, OneWireContainer12, OneWireContainer1C, OneWireContainer1F, OneWireContainer29, OneWireContainer3A, and OneWireContainer42.
| boolean onlySingleChannelOn | ( | ) |
Checks to see if the channels of this switch require that only one channel is on at any one time.
If this method returns true then the method setLatchState(int,boolean,boolean,byte[]) will not only affect the state of the given channel but may affect the state of the other channels as well to insure that only one channel is on at a time.
true if only one channel can be on at a time.Implemented in OneWireContainer05, OneWireContainer12, OneWireContainer1C, OneWireContainer1F, OneWireContainer29, OneWireContainer3A, and OneWireContainer42.
| void setLatchState | ( | int | channel, |
| boolean | latchState, | ||
| boolean | doSmart, | ||
| byte[] | state | ||
| ) |
Sets the latch state of the indicated channel.
The method writeDevice() must be called to finalize changes to the device. Note that multiple 'set' methods can be called before one call to writeDevice().
| channel | channel to execute this operation, in the range [0 to (getNumberChannels(byte[]) - 1)] |
| latchState | true to set the channel latch 'on' (conducting) and false to set the channel latch 'off' (not conducting). Note that the actual output when the latch is 'on' is returned from the isHighSideSwitch() method. |
| doSmart | If latchState is 'on'/true then doSmart indicates if a 'smart on' is to be done. To avoid an exception check the capabilities of this device using the hasSmartOn() method. |
| state | current state of the device returned from readDevice() |
Implemented in OneWireContainer05, OneWireContainer12, OneWireContainer1C, OneWireContainer1F, OneWireContainer29, OneWireContainer3A, and OneWireContainer42.
1.7.3