|
1-Wire API for .NET Version 4.00
|
Scratchpad interface for Memory banks that require it. More...
Inherited by MemoryBankScratch.
Public Member Functions | |
| void | readScratchpad (byte[] readBuf, int offset, int len, byte[] extraInfo) throws OneWireIOException, OneWireException |
| Read the scratchpad page of memory from a NVRAM device This method reads and returns the entire scratchpad after the byte offset regardless of the actual ending offset. | |
| void | writeScratchpad (int startAddr, byte[] writeBuf, int offset, int len) throws OneWireIOException, OneWireException |
| Write to the scratchpad page of memory a NVRAM device. | |
| void | copyScratchpad (int startAddr, int len) throws OneWireIOException, OneWireException |
| Copy the scratchpad page to memory. | |
| int | getExtraInfoLength () |
| Query to get the length in bytes of extra information that is read when read a page in the current memory bank. | |
| void | checkSpeed () throws OneWireIOException, OneWireException |
| Check the device speed if has not been done before or if an error was detected. | |
| void | forceVerify () |
| Set the flag to indicate the next 'checkSpeed()' will force a speed set and verify. | |
Scratchpad interface for Memory banks that require it.
| void checkSpeed | ( | ) | throws OneWireIOException, OneWireException |
Check the device speed if has not been done before or if an error was detected.
| OneWireIOException | |
| OneWireException |
Implemented in MemoryBankScratch.
| void copyScratchpad | ( | int | startAddr, |
| int | len | ||
| ) | throws OneWireIOException, OneWireException |
Copy the scratchpad page to memory.
| startAddr | starting address |
| len | length in bytes that was written already |
| OneWireIOException | |
| OneWireException |
Implemented in MemoryBankScratch, MemoryBankScratchCRCPW, MemoryBankScratchEE, MemoryBankScratchEx, and MemoryBankScratchSHAEE.
| int getExtraInfoLength | ( | ) |
Query to get the length in bytes of extra information that is read when read a page in the current memory bank.
See 'hasExtraInfo()'.
Implemented in MemoryBankScratch.
| void readScratchpad | ( | byte[] | readBuf, |
| int | offset, | ||
| int | len, | ||
| byte[] | extraInfo | ||
| ) | throws OneWireIOException, OneWireException |
Read the scratchpad page of memory from a NVRAM device This method reads and returns the entire scratchpad after the byte offset regardless of the actual ending offset.
| readBuf | byte array to place read data into length of array is always pageLength. |
| offset | offset into readBuf to pug data |
| len | length in bytes to read |
| extraInfo | byte array to put extra info read into (TA1, TA2, e/s byte) length of array is always extraInfoLength. Can be 'null' if extra info is not needed. |
| OneWireIOException | |
| OneWireException |
Implemented in MemoryBankScratch, MemoryBankScratchCRC, MemoryBankScratchCRCPW, and MemoryBankScratchSHAEE.
| void writeScratchpad | ( | int | startAddr, |
| byte[] | writeBuf, | ||
| int | offset, | ||
| int | len | ||
| ) | throws OneWireIOException, OneWireException |
Write to the scratchpad page of memory a NVRAM device.
| startAddr | starting address |
| writeBuf | byte array containing data to write |
| offset | offset into readBuf to place data |
| len | length in bytes to write |
| OneWireIOException | |
| OneWireException |
Implemented in MemoryBankScratch, MemoryBankScratchCRCPW, MemoryBankScratchEE, MemoryBankScratchEx, MemoryBankScratchSHA, and MemoryBankScratchSHAEE.
1.7.3