|
1-Wire API for .NET Version 4.00
|
Public interface for all devices which implement some form of password protection. More...
Inherited by OneWireContainer37, and OneWireContainer41.
Public Member Functions | |
| int | getReadOnlyPasswordLength () throws OneWireException |
| Returns the length in bytes of the Read-Only password. | |
| int | getReadWritePasswordLength () throws OneWireException |
| Returns the length in bytes of the Read/Write password. | |
| int | getWriteOnlyPasswordLength () throws OneWireException |
| Returns the length in bytes of the Write-Only password. | |
| int | getReadOnlyPasswordAddress () throws OneWireException |
| Returns the absolute address of the memory location where the Read-Only password is written. | |
| int | getReadWritePasswordAddress () throws OneWireException |
| Returns the absolute address of the memory location where the Read/Write password is written. | |
| int | getWriteOnlyPasswordAddress () throws OneWireException |
| Returns the absolute address of the memory location where the Write-Only password is written. | |
| boolean | hasReadOnlyPassword () |
| Returns true if this device has a Read-Only password. | |
| boolean | hasReadWritePassword () |
| Returns true if this device has a Read/Write password. | |
| boolean | hasWriteOnlyPassword () |
| Returns true if this device has a Write-Only password. | |
| boolean | getDeviceReadOnlyPasswordEnable () throws OneWireException |
| Returns true if the device's Read-Only password has been enabled. | |
| boolean | getDeviceReadWritePasswordEnable () throws OneWireException |
| Returns true if the device's Read/Write password has been enabled. | |
| boolean | getDeviceWriteOnlyPasswordEnable () throws OneWireException |
| Returns true if the device's Write-Only password has been enabled. | |
| boolean | hasSinglePasswordEnable () |
| Returns true if this device has the capability to enable one type of password while leaving another type disabled. | |
| void | setDevicePasswordEnable (boolean enableReadOnly, boolean enableReadWrite, boolean enableWriteOnly) throws OneWireException, OneWireIOException |
| void | setDevicePasswordEnableAll (boolean enableAll) throws OneWireException, OneWireIOException |
| void | setDeviceReadOnlyPassword (byte[] password, int offset) throws OneWireException, OneWireIOException |
| void | setDeviceReadWritePassword (byte[] password, int offset) throws OneWireException, OneWireIOException |
| void | setDeviceWriteOnlyPassword (byte[] password, int offset) throws OneWireException, OneWireIOException |
| void | setContainerReadOnlyPassword (byte[] password, int offset) throws OneWireException |
| Sets the Read-Only password used by the API when reading from the device's memory. | |
| void | setContainerReadWritePassword (byte[] password, int offset) throws OneWireException |
| Sets the Read/Write password used by the API when reading from or writing to the device's memory. | |
| void | setContainerWriteOnlyPassword (byte[] password, int offset) throws OneWireException |
| Sets the Write-Only password used by the API when writing to the device's memory. | |
| boolean | isContainerReadOnlyPasswordSet () throws OneWireException |
| Returns true if the password used by the API for reading from the device's memory has been set. | |
| boolean | isContainerReadWritePasswordSet () throws OneWireException |
| Returns true if the password used by the API for reading from or writing to the device's memory has been set. | |
| boolean | isContainerWriteOnlyPasswordSet () throws OneWireException |
| Returns true if the password used by the API for writing to the device's memory has been set. | |
| void | getContainerReadOnlyPassword (byte[] password, int offset) throws OneWireException |
| Gets the Read-Only password used by the API when reading from the device's memory. | |
| void | getContainerReadWritePassword (byte[] password, int offset) throws OneWireException |
| Gets the Read/Write password used by the API when reading from or writing to the device's memory. | |
| void | getContainerWriteOnlyPassword (byte[] password, int offset) throws OneWireException |
| Gets the Write-Only password used by the API when writing to the device's memory. | |
Public interface for all devices which implement some form of password protection.
The operation protected could be reading from the device, writing to the device, or both. These interface methods will allow you to set the passwords on the device, enable/disable the passwords on the device, and set the passwords for the API to use when interacting with the device.
| void getContainerReadOnlyPassword | ( | byte[] | password, |
| int | offset | ||
| ) | throws OneWireException |
Gets the Read-Only password used by the API when reading from the device's memory.
This password is not read from the device's Read-Only password register. It is the password used by the software for interacting with the device only and must have been set using the setContainerReadOnlyPassword method.
| password | array for holding the password that is used by the API when reading from the device's memory. Length must be (offset + getWriteOnlyPasswordLength) |
| offset | the starting point for copying into the given password array |
Implemented in OneWireContainer37, and OneWireContainer41.
| void getContainerReadWritePassword | ( | byte[] | password, |
| int | offset | ||
| ) | throws OneWireException |
Gets the Read/Write password used by the API when reading from or writing to the device's memory.
This password is not read from the device's Read/Write password register. It is the password used by the software for interacting with the device only and must have been set using the setContainerReadWritePassword method.
| password | array for holding the password that is used by the API when reading from or writing to the device's memory. Length must be (offset + getReadWritePasswordLength) |
| offset | the starting point for copying into the given password array |
Implemented in OneWireContainer37, and OneWireContainer41.
| void getContainerWriteOnlyPassword | ( | byte[] | password, |
| int | offset | ||
| ) | throws OneWireException |
Gets the Write-Only password used by the API when writing to the device's memory.
This password is not read from the device's Write-Only password register. It is the password used by the software for interacting with the device only and must have been set using the setContainerWriteOnlyPassword method.
| password | array for holding the password that is used by the API when writing to the device's memory. Length must be (offset + getWriteOnlyPasswordLength) |
| offset | the starting point for copying into the given password array |
Implemented in OneWireContainer37, and OneWireContainer41.
| boolean getDeviceReadOnlyPasswordEnable | ( | ) | throws OneWireException |
Returns true if the device's Read-Only password has been enabled.
true if the device's Read-Only password has been enabled. Implemented in OneWireContainer37, and OneWireContainer41.
| boolean getDeviceReadWritePasswordEnable | ( | ) | throws OneWireException |
Returns true if the device's Read/Write password has been enabled.
true if the device's Read/Write password has been enabled. Implemented in OneWireContainer37, and OneWireContainer41.
| boolean getDeviceWriteOnlyPasswordEnable | ( | ) | throws OneWireException |
Returns true if the device's Write-Only password has been enabled.
true if the device's Write-Only password has been enabled. Implemented in OneWireContainer37, and OneWireContainer41.
| int getReadOnlyPasswordAddress | ( | ) | throws OneWireException |
Returns the absolute address of the memory location where the Read-Only password is written.
Implemented in OneWireContainer37, and OneWireContainer41.
| int getReadOnlyPasswordLength | ( | ) | throws OneWireException |
Returns the length in bytes of the Read-Only password.
Implemented in OneWireContainer37, and OneWireContainer41.
| int getReadWritePasswordAddress | ( | ) | throws OneWireException |
Returns the absolute address of the memory location where the Read/Write password is written.
Implemented in OneWireContainer37, and OneWireContainer41.
| int getReadWritePasswordLength | ( | ) | throws OneWireException |
Returns the length in bytes of the Read/Write password.
Implemented in OneWireContainer37, and OneWireContainer41.
| int getWriteOnlyPasswordAddress | ( | ) | throws OneWireException |
Returns the absolute address of the memory location where the Write-Only password is written.
Implemented in OneWireContainer37, and OneWireContainer41.
| int getWriteOnlyPasswordLength | ( | ) | throws OneWireException |
Returns the length in bytes of the Write-Only password.
Implemented in OneWireContainer37, and OneWireContainer41.
| boolean hasReadOnlyPassword | ( | ) |
Returns true if this device has a Read-Only password.
If false, all other functions dealing with the Read-Only password will throw an exception if called.
true if this device has a Read-Only password. Implemented in OneWireContainer37, and OneWireContainer41.
| boolean hasReadWritePassword | ( | ) |
Returns true if this device has a Read/Write password.
If false, all other functions dealing with the Read/Write password will throw an exception if called.
true if this device has a Read/Write password. Implemented in OneWireContainer37, and OneWireContainer41.
| boolean hasSinglePasswordEnable | ( | ) |
Returns true if this device has the capability to enable one type of password while leaving another type disabled.
i.e. if the device has Read-Only password protection and Write-Only password protection, this method indicates whether or not you can enable Read-Only protection while leaving the Write-Only protection disabled.
true if the device has the capability to enable one type of password while leaving another type disabled. Implemented in OneWireContainer37, and OneWireContainer41.
| boolean hasWriteOnlyPassword | ( | ) |
Returns true if this device has a Write-Only password.
If false, all other functions dealing with the Write-Only password will throw an exception if called.
true if this device has a Write-Only password. Implemented in OneWireContainer37, and OneWireContainer41.
| boolean isContainerReadOnlyPasswordSet | ( | ) | throws OneWireException |
Returns true if the password used by the API for reading from the device's memory has been set.
The return value is not affected by whether or not the read password of the container actually matches the value in the device's password register.
true if the password used by the API for reading from the device's memory has been set. Implemented in OneWireContainer37, and OneWireContainer41.
| boolean isContainerReadWritePasswordSet | ( | ) | throws OneWireException |
Returns true if the password used by the API for reading from or writing to the device's memory has been set.
The return value is not affected by whether or not the read/write password of the container actually matches the value in the device's password register.
true if the password used by the API for reading from or writing to the device's memory has been set. Implemented in OneWireContainer37, and OneWireContainer41.
| boolean isContainerWriteOnlyPasswordSet | ( | ) | throws OneWireException |
Returns true if the password used by the API for writing to the device's memory has been set.
The return value is not affected by whether or not the write password of the container actually matches the value in the device's password register.
true if the password used by the API for writing to the device's memory has been set. Implemented in OneWireContainer37, and OneWireContainer41.
| void setContainerReadOnlyPassword | ( | byte[] | password, |
| int | offset | ||
| ) | throws OneWireException |
Sets the Read-Only password used by the API when reading from the device's memory.
This password is not written to the device's Read-Only password register. It is the password used by the software for interacting with the device only.
| password | the new password to be used by the API when reading from the device's memory. Length must be (offset + getReadOnlyPasswordLength) |
| offset | the starting point for copying from the given password array |
Implemented in OneWireContainer37, and OneWireContainer41.
| void setContainerReadWritePassword | ( | byte[] | password, |
| int | offset | ||
| ) | throws OneWireException |
Sets the Read/Write password used by the API when reading from or writing to the device's memory.
This password is not written to the device's Read/Write password register. It is the password used by the software for interacting with the device only.
| password | the new password to be used by the API when reading from or writing to the device's memory. Length must be (offset + getReadWritePasswordLength) |
| offset | the starting point for copying from the given password array |
Implemented in OneWireContainer37, and OneWireContainer41.
| void setContainerWriteOnlyPassword | ( | byte[] | password, |
| int | offset | ||
| ) | throws OneWireException |
Sets the Write-Only password used by the API when writing to the device's memory.
This password is not written to the device's Write-Only password register. It is the password used by the software for interacting with the device only.
| password | the new password to be used by the API when writing to the device's memory. Length must be (offset + getWriteOnlyPasswordLength) |
| offset | the starting point for copying from the given password array |
Implemented in OneWireContainer37, and OneWireContainer41.
| void setDevicePasswordEnable | ( | boolean | enableReadOnly, |
| boolean | enableReadWrite, | ||
| boolean | enableWriteOnly | ||
| ) | throws OneWireException, OneWireIOException |
Enables/Disables passwords for this Device. This method allows you to individually enable the different types of passwords for a particular device. If hasSinglePasswordEnable() returns true, you can selectively enable particular types of passwords. Otherwise, this method will throw an exception if all supported types are not enabled.
For this to be successful, either write-protect passwords must be disabled, or the write-protect password(s) for this container must be set and must match the value of the write-protect password(s) in the device's register.
| enableReadOnly | if true Read-Only passwords will be enabled. |
| enableReadWrite | if true Read/Write passwords will be enabled. |
| enableWriteOnly | if true Write-Only passwords will be enabled. |
Implemented in OneWireContainer37, and OneWireContainer41.
| void setDevicePasswordEnableAll | ( | boolean | enableAll | ) | throws OneWireException, OneWireIOException |
Enables/Disables passwords for this device. If the part has more than one type of password (Read-Only, Write-Only, or Read/Write), all passwords will be enabled. This function is equivalent to the following: owc41.setDevicePasswordEnable( owc41.hasReadOnlyPassword(), owc41.hasReadWritePassword(), owc41.hasWriteOnlyPassword() );
For this to be successful, either write-protect passwords must be disabled, or the write-protect password(s) for this container must be set and must match the value of the write-protect password(s) in the device's register.
| enableAll | if true, all passwords are enabled. Otherwise, all passwords are disabled. |
Implemented in OneWireContainer37, and OneWireContainer41.
| void setDeviceReadOnlyPassword | ( | byte[] | password, |
| int | offset | ||
| ) | throws OneWireException, OneWireIOException |
Writes the given password to the device's Read-Only password register. Note that this function does not enable the password, just writes the value to the appropriate memory location.
For this to be successful, either write-protect passwords must be disabled, or the write-protect password(s) for this container must be set and must match the value of the write-protect password(s) in the device's register.
| password | the new password to be written to the device's Read-Only password register. Length must be (offset + getReadOnlyPasswordLength) |
| offset | the starting point for copying from the given password array |
Implemented in OneWireContainer37, and OneWireContainer41.
| void setDeviceReadWritePassword | ( | byte[] | password, |
| int | offset | ||
| ) | throws OneWireException, OneWireIOException |
Writes the given password to the device's Read/Write password register. Note that this function does not enable the password, just writes the value to the appropriate memory location.
For this to be successful, either write-protect passwords must be disabled, or the write-protect password(s) for this container must be set and must match the value of the write-protect password(s) in the device's register.
| password | the new password to be written to the device's Read-Write password register. Length must be (offset + getReadWritePasswordLength) |
| offset | the starting point for copying from the given password array |
Implemented in OneWireContainer37, and OneWireContainer41.
| void setDeviceWriteOnlyPassword | ( | byte[] | password, |
| int | offset | ||
| ) | throws OneWireException, OneWireIOException |
Writes the given password to the device's Write-Only password register. Note that this function does not enable the password, just writes the value to the appropriate memory location.
For this to be successful, either write-protect passwords must be disabled, or the write-protect password(s) for this container must be set and must match the value of the write-protect password(s) in the device's register.
| password | the new password to be written to the device's Write-Only password register. Length must be (offset + getWriteOnlyPasswordLength) |
| offset | the starting point for copying from the given password array |
Implemented in OneWireContainer37, and OneWireContainer41.
1.7.3