|
1-Wire API for .NET Version 4.00
|
Inherits com::dalsemi::onewire::container::MemoryBank.
Inherited by MemoryBankAD, MemoryBankEE, MemoryBankNV, MemoryBankScratch, MemoryBankSHAEE, and OTPMemoryBank.
Public Member Functions | |
| int | getNumberPages () |
| Gets the number of pages in this memory bank. | |
| int | getPageLength () |
| Gets raw page length in bytes in this memory bank. | |
| int | getMaxPacketDataLength () |
| Gets Maximum data page length in bytes for a packet read or written in this memory bank. | |
| boolean | hasPageAutoCRC () |
| Checks to see if this memory bank's pages can be read with the contents being verified by a device generated CRC. | |
| boolean | haveExtraInfo () |
| Checks to see if this memory bank's pages deliver extra information outside of the normal data space, when read. | |
| boolean | hasExtraInfo () |
| Checks to see if this memory bank's pages deliver extra information outside of the normal data space, when read. | |
| int | getExtraInfoLength () |
| Gets the length in bytes of extra information that is read when reading a page in this memory bank. | |
| String | getExtraInfoDescription () |
| Gets a string description of what is contained in the Extra Information returned when reading pages in this memory bank. | |
| void | readPage (int page, boolean readContinue, byte[] readBuf, int offset) throws OneWireIOException, OneWireException |
| Reads a page in this memory bank with no CRC checking (device or data). | |
| void | readPage (int page, boolean readContinue, byte[] readBuf, int offset, byte[] extraInfo) throws OneWireIOException, OneWireException |
| Reads a page in this memory bank with extra information with no CRC checking (device or data). | |
| int | readPagePacket (int page, boolean readContinue, byte[] readBuf, int offset) throws OneWireIOException, OneWireException |
| Reads a Universal Data Packet. | |
| int | readPagePacket (int page, boolean readContinue, byte[] readBuf, int offset, byte[] extraInfo) throws OneWireIOException, OneWireException |
| Reads a Universal Data Packet and extra information. | |
| void | writePagePacket (int page, byte[] writeBuf, int offset, int len) throws OneWireIOException, OneWireException |
| Writes a Universal Data Packet. | |
| void | readPageCRC (int page, boolean readContinue, byte[] readBuf, int offset) throws OneWireIOException, OneWireException |
| Reads a complete memory page with CRC verification provided by the device. | |
| void | readPageCRC (int page, boolean readContinue, byte[] readBuf, int offset, byte[] extraInfo) throws OneWireIOException, OneWireException |
| Reads a complete memory page with CRC verification provided by the device with extra information. | |
Paged Memory bank interface for iButtons (or 1-Wire devices) with page based memory. This interface extents the base functionality of the super-interface MemoryBank by providing paged based services.
This interface has methods to read and write a packet structure called the UDP (Universal Data Packet). This structure has a length byte, data, and an inverted CRC16. See Maxim Integrated Products Application Note 114 for details: http://dbserv.maxim-ic.com/appnotes.cfm?appnote_number=114
The MemoryBank methods can be organized into the following categories:
Display some features of PagedMemoryBank instance 'pmb':
System.out.print("PagedMemoryBank has: " + pmb.getNumberPages() + " pages of length ");
System.out.print(pbank.getPageLength() + " bytes ");
if (bank.isGeneralPurposeMemory())
System.out.print("giving " + pbank.getMaxPacketDataLength() + " bytes Packet data payload");
System.out.println(); if (pbank.hasPageAutoCRC())
System.out.print("PagedMemoryBank has device generated CRC");
Write a packet into the first page of a PagedMemoryBank instance 'pmb':
byte[] write_buf = new byte[pmb.getMaxPacketDataLength()];
for (int i = 0; i < write_buf.length; i++)
write_buf[i] = (byte)0; mb.writePagePacket(0, write_buf, 0, write_buf.length);
Read all of the pages of a PagedMemoryBank instance 'pmb' with device CRC verification:
byte[] read_buf = new byte[pmb.getPageLength()]; if (pmb.hasAutoCRC())
{
// loop to read each page with CRC
for (int pg = 0; pg < pmb.getNumberPages(); pg++)
{
// use 'readContinue' arguement to only access device on first page
pmb.readPageCRC(pg, (pg == 0), read_buf, 0); // do something with data in read_buf ...
}
}
else
System.out.println("PagedMemoryBank does not support device generated CRC"); | String getExtraInfoDescription | ( | ) |
Gets a string description of what is contained in the Extra Information returned when reading pages in this memory bank.
Implemented in MemoryBankAD, MemoryBankAppReg, MemoryBankEE, MemoryBankEEPROM, MemoryBankEEPROMblock, MemoryBankEPROM, MemoryBankNV, MemoryBankScratch, and MemoryBankSHAEE.
| int getExtraInfoLength | ( | ) |
Gets the length in bytes of extra information that is read when reading a page in this memory bank.
Implemented in MemoryBankAD, MemoryBankAppReg, MemoryBankEE, MemoryBankEEPROM, MemoryBankEEPROMblock, MemoryBankEPROM, MemoryBankNV, MemoryBankScratch, and MemoryBankSHAEE.
| int getMaxPacketDataLength | ( | ) |
Gets Maximum data page length in bytes for a packet read or written in this memory bank.
See the readPagePacket and writePagePacket methods. This method is only usefull if this memory bank is general purpose memory.
Implemented in MemoryBankAD, MemoryBankAppReg, MemoryBankEE, MemoryBankEEPROM, MemoryBankEEPROMblock, MemoryBankEPROM, MemoryBankNV, MemoryBankScratch, and MemoryBankSHAEE.
| int getNumberPages | ( | ) |
Gets the number of pages in this memory bank.
The page numbers are then always 0 to (getNumberPages() - 1).
Implemented in MemoryBankAD, MemoryBankAppReg, MemoryBankEE, MemoryBankEEPROM, MemoryBankEEPROMblock, MemoryBankEPROM, MemoryBankNV, MemoryBankScratch, and MemoryBankSHAEE.
| int getPageLength | ( | ) |
Gets raw page length in bytes in this memory bank.
Implemented in MemoryBankAD, MemoryBankAppReg, MemoryBankEE, MemoryBankEEPROM, MemoryBankEEPROMblock, MemoryBankEPROM, MemoryBankNV, MemoryBankScratch, and MemoryBankSHAEE.
| boolean hasExtraInfo | ( | ) |
Checks to see if this memory bank's pages deliver extra information outside of the normal data space, when read.
Examples of this may be a redirection byte, counter, tamper protection bytes, or SHA-1 result. If this method returns true then the methods with an 'extraInfo' parameter can be used: readPage, readPageCRC, and readPagePacket.
true if reading the this memory bank's pages provides extra informationImplemented in MemoryBankAD, MemoryBankAppReg, MemoryBankEE, MemoryBankEEPROM, MemoryBankEEPROMblock, MemoryBankEPROM, MemoryBankNV, MemoryBankScratch, and MemoryBankSHAEE.
| boolean hasPageAutoCRC | ( | ) |
Checks to see if this memory bank's pages can be read with the contents being verified by a device generated CRC.
This is used to see if the readPageCRC method can be used.
true if this memory bank can be read with self generated CRCImplemented in MemoryBankAD, MemoryBankAppReg, MemoryBankEE, MemoryBankEEPROM, MemoryBankEEPROMblock, MemoryBankEPROM, MemoryBankNV, MemoryBankScratch, and MemoryBankSHAEE.
| boolean haveExtraInfo | ( | ) |
Checks to see if this memory bank's pages deliver extra information outside of the normal data space, when read.
Examples of this may be a redirection byte, counter, tamper protection bytes, or SHA-1 result. If this method returns true then the methods with an 'extraInfo' parameter can be used: readPage, readPageCRC, and readPagePacket.
true if reading the this memory bank's pages provides extra informationImplemented in MemoryBankAD, MemoryBankAppReg, MemoryBankEE, MemoryBankEEPROM, MemoryBankEEPROMblock, MemoryBankEPROM, MemoryBankNV, MemoryBankScratch, and MemoryBankSHAEE.
| void readPage | ( | int | page, |
| boolean | readContinue, | ||
| byte[] | readBuf, | ||
| int | offset | ||
| ) | throws OneWireIOException, OneWireException |
Reads a page in this memory bank with no CRC checking (device or data).
The resulting data from this API may or may not be what is on the 1-Wire device. It is recommends that the data contain some kind of checking (CRC) like in the readPagePacket method or have the 1-Wire device provide the CRC as in readPageCRC. However device CRC generation is not supported on all memory types, see hasPageAutoCRC. If neither is an option then this method could be called more then once to at least verify that the same data is read consistently.
The readContinue parameter is used to eliminate the overhead in re-accessing a part already being read from. For example, if pages 0 - 4 are to be read, readContinue would be set to false for page 0 and would be set to true for the next four calls.
Note: Using readContinue = true can only be used if the new read continues where the last one left off and it is inside a 'beginExclusive/endExclusive' block.
| page | page number to read packet from |
| readContinue | true then device read is continued without re-selecting |
| readBuf | location for data read |
| offset | offset into readBuf to place data |
| OneWireIOException | on a 1-Wire communication error such as no 1-Wire device present. This could be caused by a physical interruption in the 1-Wire Network due to shorts or a newly arriving 1-Wire device issuing a 'presence pulse'. |
| OneWireException | on a communication or setup error with the 1-Wire adapter |
Implemented in MemoryBankAD, MemoryBankAppReg, MemoryBankEE, MemoryBankEEPROM, MemoryBankEEPROMblock, MemoryBankEPROM, MemoryBankNV, MemoryBankNVCRC, and MemoryBankScratch.
| void readPage | ( | int | page, |
| boolean | readContinue, | ||
| byte[] | readBuf, | ||
| int | offset, | ||
| byte[] | extraInfo | ||
| ) | throws OneWireIOException, OneWireException |
Reads a page in this memory bank with extra information with no CRC checking (device or data).
The resulting data from this API may or may not be what is on the 1-Wire device. It is recommends that the data contain some kind of checking (CRC) like in the readPagePacket method or have the 1-Wire device provide the CRC as in readPageCRC. However device CRC generation is not supported on all memory types, see hasPageAutoCRC. If neither is an option then this method could be called more then once to at least verify that the same data is read consistently.The readContinue parameter is used to eliminate the overhead in re-accessing a part already being read from. For example, if pages 0 - 4 are to be read, readContinue would be set to false for page 0 and would be set to true for the next four calls.
Note: Using readContinue = true can only be used if the new read continues where the last one left off and it is inside a 'beginExclusive/endExclusive' block.
| page | page number to read packet from |
| readContinue | true then device read is continued without re-selecting |
| readBuf | location for data read |
| offset | offset into readBuf to place data |
| extraInfo | location for extra info read |
| OneWireIOException | on a 1-Wire communication error such as no 1-Wire device present. This could be caused by a physical interruption in the 1-Wire Network due to shorts or a newly arriving 1-Wire device issuing a 'presence pulse'. |
| OneWireException | on a communication or setup error with the 1-Wire adapter |
Implemented in MemoryBankAD, MemoryBankAppReg, MemoryBankEE, MemoryBankEEPROM, MemoryBankEEPROMblock, MemoryBankEPROM, MemoryBankNV, MemoryBankNVCRC, and MemoryBankScratch.
| void readPageCRC | ( | int | page, |
| boolean | readContinue, | ||
| byte[] | readBuf, | ||
| int | offset, | ||
| byte[] | extraInfo | ||
| ) | throws OneWireIOException, OneWireException |
Reads a complete memory page with CRC verification provided by the device with extra information.
Not supported by all devices. The readContinue parameter is used to eliminate the overhead in re-accessing a part already being read from. For example, if pages 0 - 4 are to be read, readContinue would be set to false for page 0 and would be set to true for the next four calls.
Note: Using readContinue = true can only be used if the new read continues where the last one left off and it is inside a 'beginExclusive/endExclusive' block.
| page | page number to read |
| readContinue | true true then device read is issued without continued without re-selecting |
| readBuf | location for data read |
| offset | offset into readBuf to place data |
| extraInfo | location for extra info read |
| OneWireIOException | on a 1-Wire communication error such as an invalid CRC read from device. This could be caused by a physical interruption in the 1-Wire Network due to shorts or a newly arriving 1-Wire device issuing a 'presence pulse'. |
| OneWireException | on a communication or setup error with the 1-Wire adapter |
Implemented in MemoryBankAD, MemoryBankAppReg, MemoryBankEE, MemoryBankEEPROM, MemoryBankEEPROMblock, MemoryBankEPROM, MemoryBankNV, MemoryBankNVCRC, MemoryBankNVCRCPW, MemoryBankScratch, MemoryBankScratchCRC, MemoryBankScratchCRCPW, and MemoryBankScratchSHAEE.
| void readPageCRC | ( | int | page, |
| boolean | readContinue, | ||
| byte[] | readBuf, | ||
| int | offset | ||
| ) | throws OneWireIOException, OneWireException |
Reads a complete memory page with CRC verification provided by the device.
Not supported by all devices. The readContinue parameter is used to eliminate the overhead in re-accessing a part already being read from. For example, if pages 0 - 4 are to be read, readContinue would be set to false for page 0 and would be set to true for the next four calls.
Note: Using readContinue = true can only be used if the new read continues where the last one left off and it is inside a 'beginExclusive/endExclusive' block.
| page | page number to read |
| readContinue | true true then device read is continued without re-selecting |
| readBuf | location for data read |
| offset | offset into readBuf to place data |
| OneWireIOException | on a 1-Wire communication error such as an invalid CRC read from device. This could be caused by a physical interruption in the 1-Wire Network due to shorts or a newly arriving 1-Wire device issuing a 'presence pulse'. |
| OneWireException | on a communication or setup error with the 1-Wire adapter |
Implemented in MemoryBankAD, MemoryBankAppReg, MemoryBankEE, MemoryBankEEPROM, MemoryBankEEPROMblock, MemoryBankEPROM, MemoryBankNV, MemoryBankNVCRC, MemoryBankScratch, MemoryBankScratchCRC, MemoryBankScratchCRCPW, and MemoryBankScratchSHAEE.
| int readPagePacket | ( | int | page, |
| boolean | readContinue, | ||
| byte[] | readBuf, | ||
| int | offset | ||
| ) | throws OneWireIOException, OneWireException |
Reads a Universal Data Packet.
The Universal Data Packet always starts on page boundaries but can end anywhere in the page. The structure specifies the length of data bytes not including the length byte and the CRC16 bytes. There is one length byte. The CRC16 is first initialized to the page number. This provides a check to verify the page that was intended is being read. The CRC16 is then calculated over the length and data bytes. The CRC16 is then inverted and stored low byte first followed by the high byte. The structure is used by this method to verify the data but only the data payload is returned. The readContinue parameter is used to eliminate the overhead in re-accessing a part already being read from. For example, if pages 0 - 4 are to be read, readContinue would be set to false for page 0 and would be set to true for the next four calls.
See Maxim Integrated Products Application Note 114 for details: http://dbserv.maxim-ic.com/appnotes.cfm?appnote_number=114
Note: Using readContinue = true can only be used if the new read continues where the last one left off and it is inside a 'beginExclusive/endExclusive' block.
| page | page number to read packet from |
| readContinue | true true then device read is continued without re-selecting |
| readBuf | location for data read |
| offset | offset into readBuf to place data |
| OneWireIOException | on a 1-Wire communication error such as an invalid CRC16 or length found in the packet. This could be caused by a physical interruption in the 1-Wire Network due to shorts or a newly arriving 1-Wire device issuing a 'presence pulse'. It could also be caused due to the device page not containing a valid packet. |
| OneWireException | on a communication or setup error with the 1-Wire adapter |
Implemented in MemoryBankAD, MemoryBankAppReg, MemoryBankEE, MemoryBankEEPROM, MemoryBankEEPROMblock, MemoryBankEPROM, MemoryBankNV, and MemoryBankScratch.
| int readPagePacket | ( | int | page, |
| boolean | readContinue, | ||
| byte[] | readBuf, | ||
| int | offset, | ||
| byte[] | extraInfo | ||
| ) | throws OneWireIOException, OneWireException |
Reads a Universal Data Packet and extra information.
See the method readPagePacket for a description of the packet structure. The readContinue parameter is used to eliminate the overhead in re-accessing a part already being read from. For example, if pages 0 - 4 are to be read, readContinue would be set to false for page 0 and would be set to true for the next four calls.
Note: Using readContinue = true can only be used if the new read continues where the last one left off and it is inside a 'beginExclusive/endExclusive' block.
| page | page number to read packet from |
| readContinue | true then device read is continued without re-selecting |
| readBuf | location for data read |
| offset | offset into readBuf to place data |
| extraInfo | location for extra info read |
| OneWireIOException | on a 1-Wire communication error such as an invalid CRC16 or length found in the packet. This could be caused by a physical interruption in the 1-Wire Network due to shorts or a newly arriving 1-Wire device issuing a 'presence pulse'. It could also be caused due to the device page not containing a valid packet. |
| OneWireException | on a communication or setup error with the 1-Wire adapter |
Implemented in MemoryBankAD, MemoryBankAppReg, MemoryBankEE, MemoryBankEEPROM, MemoryBankEEPROMblock, MemoryBankEPROM, MemoryBankNV, MemoryBankNVCRC, and MemoryBankScratch.
| void writePagePacket | ( | int | page, |
| byte[] | writeBuf, | ||
| int | offset, | ||
| int | len | ||
| ) | throws OneWireIOException, OneWireException |
Writes a Universal Data Packet.
See the method readPagePacket for a description of the packet structure.
| page | page number to write packet to |
| writeBuf | data to write |
| offset | offset into writeBuf where data to write is |
| len | number of bytes to write with a max of getMaxPacketDataLength elements |
| OneWireIOException | on a 1-Wire communication error such as read verification error on write. This could be caused by a physical interruption in the 1-Wire Network due to shorts or a newly arriving 1-Wire device issuing a 'presence pulse'. It could also be caused due to the device page being write protected. |
| OneWireException | on a communication or setup error with the 1-Wire adapter |
Implemented in MemoryBankAD, MemoryBankAppReg, MemoryBankEE, MemoryBankEEPROM, MemoryBankEEPROMblock, MemoryBankEPROM, MemoryBankNV, and MemoryBankScratch.
1.7.3