|
1-Wire API for .NET Version 4.00
|
Inherits com::dalsemi::onewire::container::PagedMemoryBank.
Inherited by MemoryBankAppReg, MemoryBankEEPROM, MemoryBankEEPROMblock, and MemoryBankEPROM.
Public Member Functions | |
| boolean | canRedirectPage () |
| Checks to see if this memory bank has pages that can be redirected to a new page. | |
| boolean | canLockPage () |
| Checks to see if this memory bank has pages that can be locked. | |
| boolean | canLockRedirectPage () |
| Checks to see if this memory bank has pages that can be locked from being redirected. | |
| void | lockPage (int page) throws OneWireIOException, OneWireException |
| Locks the specifed page in this memory bank. | |
| boolean | isPageLocked (int page) throws OneWireIOException, OneWireException |
| Checks to see if the specified page is locked. | |
| void | redirectPage (int page, int newPage) throws OneWireIOException, OneWireException |
| Redirects the specifed page to a new page. | |
| int | isPageRedirected (int page) throws OneWireIOException, OneWireException |
| Checks to see if the specified page is redirected. | |
| int | getRedirectedPage (int page) throws OneWireIOException, OneWireException |
| Gets the page redirection of the specified page. | |
| void | lockRedirectPage (int page) throws OneWireIOException, OneWireException |
| Locks the redirection of the specifed page. | |
| boolean | isRedirectPageLocked (int page) throws OneWireIOException, OneWireException |
| Checks to see if the specified page has redirection locked. | |
One-Time-Programmable (OTP) Memory bank interface for iButtons (or 1-Wire devices) with OTP features. This interface extents the base functionality of the super-interfaces MemoryBank and PagedMemoryBank by providing One-Time-Programmable services.
The OTPMemoryBank methods can be organized into the following categories:
Read the OTP status of page 0 in the OTPMemoryBank instance 'otp':
if (otp.canRedirectPage())
{
int new_page = getRedirectedPage(0);
if (new_page != 0)
System.out.println("Page 0 is redirected to " + new_page);
} if (otp.canLockPage())
{
if (otp.isPageLocked(0))
System.out.println("Page 0 is locked");
} if (otp.canLockRedirectPage())
{
if (otp.isRedirectPageLocked(0))
System.out.println("Page 0 redirection is locked");
}
Lock all of the pages in the OTPMemoryBank instance 'otp':
if (otp.canLockPage())
{
// loop to lock each page
for (int pg = 0; pg < otp.getNumberPages(); pg++)
{
otp.lockPage(pg);
}
}
else
System.out.println("OTPMemoryBank does not support page locking");
| boolean canLockPage | ( | ) |
Checks to see if this memory bank has pages that can be locked.
A locked page would prevent any changes to it's contents.
true if this memory bank has pages that can be lockedImplemented in MemoryBankAppReg, MemoryBankEEPROM, MemoryBankEEPROMblock, and MemoryBankEPROM.
| boolean canLockRedirectPage | ( | ) |
Checks to see if this memory bank has pages that can be locked from being redirected.
This would prevent a Write-Once memory from being updated.
true if this memory bank has pages that can be locked from being redirected to a new pageImplemented in MemoryBankAppReg, MemoryBankEEPROM, MemoryBankEEPROMblock, and MemoryBankEPROM.
| boolean canRedirectPage | ( | ) |
Checks to see if this memory bank has pages that can be redirected to a new page.
This is used in Write-Once memory to provide a means to update.
true if this memory bank pages can be redirected to a new pageImplemented in MemoryBankAppReg, MemoryBankEEPROM, MemoryBankEEPROMblock, and MemoryBankEPROM.
| int getRedirectedPage | ( | int | page | ) | throws OneWireIOException, OneWireException |
Gets the page redirection of the specified page.
Not supported by all devices.
| page | page to check for redirection |
| OneWireIOException | on a 1-Wire communication error such as no device present or a CRC read from the device is incorrect. This could be caused by a physical interruption in the 1-Wire Network due to shorts or a newly arriving 1-Wire device issuing a 'presence pulse'. |
| OneWireException | on a communication or setup error with the 1-Wire adapter. |
Implemented in MemoryBankAppReg, MemoryBankEEPROM, MemoryBankEEPROMblock, and MemoryBankEPROM.
| boolean isPageLocked | ( | int | page | ) | throws OneWireIOException, OneWireException |
Checks to see if the specified page is locked.
| page | page to check |
true if page is locked| OneWireIOException | on a 1-Wire communication error such as no device present or a CRC read from the device is incorrect. This could be caused by a physical interruption in the 1-Wire Network due to shorts or a newly arriving 1-Wire device issuing a 'presence pulse'. |
| OneWireException | on a communication or setup error with the 1-Wire adapter. |
Implemented in MemoryBankAppReg, MemoryBankEEPROM, MemoryBankEEPROMblock, and MemoryBankEPROM.
| int isPageRedirected | ( | int | page | ) | throws OneWireIOException, OneWireException |
Checks to see if the specified page is redirected.
Not supported by all devices.
| page | page to check for redirection |
| OneWireIOException | on a 1-Wire communication error such as no device present or a CRC read from the device is incorrect. This could be caused by a physical interruption in the 1-Wire Network due to shorts or a newly arriving 1-Wire device issuing a 'presence pulse'. |
| OneWireException | on a communication or setup error with the 1-Wire adapter. |
Implemented in MemoryBankAppReg, MemoryBankEEPROM, MemoryBankEEPROMblock, and MemoryBankEPROM.
| boolean isRedirectPageLocked | ( | int | page | ) | throws OneWireIOException, OneWireException |
Checks to see if the specified page has redirection locked.
Not supported by all devices.
| page | page to check for locked redirection |
true if redirection is locked for this page| OneWireIOException | on a 1-Wire communication error such as no device present or a CRC read from the device is incorrect. This could be caused by a physical interruption in the 1-Wire Network due to shorts or a newly arriving 1-Wire device issuing a 'presence pulse'. |
| OneWireException | on a communication or setup error with the 1-Wire adapter. |
Implemented in MemoryBankAppReg, MemoryBankEEPROM, MemoryBankEEPROMblock, and MemoryBankEPROM.
| void lockPage | ( | int | page | ) | throws OneWireIOException, OneWireException |
Locks the specifed page in this memory bank.
Not supported by all devices.
| page | number of page to lock |
| OneWireIOException | on a 1-Wire communication error such as no device present or a read back verification fails. This could be caused by a physical interruption in the 1-Wire Network due to shorts or a newly arriving 1-Wire device issuing a 'presence pulse'. |
| OneWireException | on a communication or setup error with the 1-Wire adapter. It will also be thrown if the device needs 'program' voltage and the adapter used by this device does not support it. |
Implemented in MemoryBankAppReg, MemoryBankEEPROM, MemoryBankEEPROMblock, and MemoryBankEPROM.
| void lockRedirectPage | ( | int | page | ) | throws OneWireIOException, OneWireException |
Locks the redirection of the specifed page.
Not supported by all devices.
| page | page to redirect |
| OneWireIOException | on a 1-Wire communication error such as no device present or a CRC read from the device is incorrect. This could be caused by a physical interruption in the 1-Wire Network due to shorts or a newly arriving 1-Wire device issuing a 'presence pulse'. |
| OneWireException | on a communication or setup error with the 1-Wire adapter. It will also be thrown if the device needs 'program' voltage and the adapter used by this device does not support it. |
Implemented in MemoryBankAppReg, MemoryBankEEPROM, MemoryBankEEPROMblock, and MemoryBankEPROM.
| void redirectPage | ( | int | page, |
| int | newPage | ||
| ) | throws OneWireIOException, OneWireException |
Redirects the specifed page to a new page.
Not supported by all devices.
| page | number of page to redirect |
| newPage | new page number to redirect to |
| OneWireIOException | on a 1-Wire communication error such as no device present or a CRC read from the device is incorrect. This could be caused by a physical interruption in the 1-Wire Network due to shorts or a newly arriving 1-Wire device issuing a 'presence pulse'. |
| OneWireException | on a communication or setup error with the 1-Wire adapter. It will also be thrown if the device needs 'program' voltage and the adapter used by this device does not support it. |
Implemented in MemoryBankAppReg, MemoryBankEEPROM, MemoryBankEEPROMblock, and MemoryBankEPROM.
1.7.3