Utilities for bit operations on an array.
More...
List of all members.
Static Public Member Functions |
| static void | arrayWriteBit (int state, int index, int offset, byte[] buf) |
| | Write the bit state in a byte array.
|
| static int | arrayReadBit (int index, int offset, byte[] buf) |
| | Read a bit state in a byte array.
|
Detailed Description
Utilities for bit operations on an array.
- Version:
- 0.00, 27 August 2000
- Author:
- DS
Member Function Documentation
| static int arrayReadBit |
( |
int |
index, |
|
|
int |
offset, |
|
|
byte[] |
buf |
|
) |
| [static] |
Read a bit state in a byte array.
- Parameters:
-
| index | bit index into byte array |
| offset | byte offset into byte array to start |
| buf | byte array to read from |
- Returns:
- bit state 1 or 0
| static void arrayWriteBit |
( |
int |
state, |
|
|
int |
index, |
|
|
int |
offset, |
|
|
byte[] |
buf |
|
) |
| [static] |
Write the bit state in a byte array.
- Parameters:
-
| state | new state of the bit 1, 0 |
| index | bit index into byte array |
| offset | byte offset into byte array to start |
| buf | byte array to manipulate |
The documentation for this class was generated from the following file: