|
1-Wire API for .NET Version 4.00
|
Utilities to translate and verify the 1-Wire Network address. More...
Static Public Member Functions | |
| static boolean | isValid (byte[] address) |
| Checks the CRC8 calculation of this 1-Wire Network address. | |
| static boolean | isValid (String address) |
| Checks the CRC8 calculation of this 1-Wire Network address. | |
| static boolean | isValid (long address) |
| Checks the CRC8 calculation of this 1-Wire Network address. | |
| static String | toString (byte[] address) |
| Converts a 1-Wire Network address byte array (little endian) to a hex string representation (big endian). | |
| static String | toString (long address) |
| Converts a 1-Wire Network address long (little endian) to a hex string representation (big endian). | |
| static byte[] | toByteArray (String address) |
| Converts a 1-Wire Network Address string (big endian) to a byte array (little endian). | |
| static byte[] | toByteArray (long address) |
| Convert an iButton or 1-Wire device address as a long (little endian) into an array of bytes. | |
| static long | toLong (byte[] address) |
| Converts a 1-Wire Network Address to a long (little endian). | |
| static long | toLong (String address) |
| Converts a 1-Wire Network Address to a long (little endian). | |
Utilities to translate and verify the 1-Wire Network address.
Q: What is a 1-Wire Network Address?
A: A 1-Wire address is 64 bits consisting of an eight bit family code, forty eight bits of serialized data and an eight bit CRC8 of the first 56 bits.
For example given the following address in hexadecimal:
10 28 E9 14 00 00 00 F3
The above is a family code 10 device with a serialized data of 28 E9 14 00 00 00, and a CRC8 of F3.
The address can be stored in several ways:
As a little-endian byte array:
byte[] address = { 0x10, (byte)0xE9, 0x14, 0x00, 0x00, 0x00, (byte)0xF3 };
As a big-endian long:
long address = (long)0xF300000014E92810;
As a big-endian String:
String address = "F300000014E92810";
| static boolean isValid | ( | byte[] | address | ) | [static] |
Checks the CRC8 calculation of this 1-Wire Network address.
The address is valid if the CRC8 of the first seven bytes of the address gives a result equal to the eighth byte.
| address | iButton or 1-Wire Network address to verify |
true if the family code is non-zero and the CRC8 calculation is correct. | static boolean isValid | ( | String | address | ) | [static] |
Checks the CRC8 calculation of this 1-Wire Network address.
The address is valid if the CRC8 of the first seven bytes of the address gives a result equal to the eighth byte.
| address | iButton or 1-Wire Network address to verify |
true if the family code is non-zero and the CRC8 calculation is correct. | static boolean isValid | ( | long | address | ) | [static] |
Checks the CRC8 calculation of this 1-Wire Network address.
The address is valid if the CRC8 of the first seven bytes of the address gives a result equal to the eighth byte.
| address | iButton or 1-Wire Network address to verify |
true if the family code is non-zero and the CRC8 calculation is correct. | static byte [] toByteArray | ( | String | address | ) | [static] |
Converts a 1-Wire Network Address string (big endian) to a byte array (little endian).
| address | family code last. |
| static long toLong | ( | String | address | ) | [static] |
Converts a 1-Wire Network Address to a long (little endian).
| static long toLong | ( | byte[] | address | ) | [static] |
Converts a 1-Wire Network Address to a long (little endian).
| static String toString | ( | byte[] | address | ) | [static] |
Converts a 1-Wire Network address byte array (little endian) to a hex string representation (big endian).
| address | family code first. |
| static String toString | ( | long | address | ) | [static] |
Converts a 1-Wire Network address long (little endian) to a hex string representation (big endian).
| address | family code first. |
1.7.3