|
1-Wire API for .NET Version 4.00
|
Static Public Member Functions | |
| static final void | setDebugMode (boolean onoff) |
| Sets the debug printing mode for this application. | |
| static final boolean | getDebugMode () |
| Gets the debug printing mode for this application. | |
| static final void | setPrintStream (PrintStream outStream) |
| Sets the output stream for printing the debug info. | |
| static final void | debug (String x) |
Prints the specified java.lang.String object if debug mode is enabled. | |
| static final void | debug (String lbl, byte[] bytes) |
| Prints the specified array of bytes with a given label if debug mode is enabled. | |
| static final void | debug (String lbl, byte[] bytes, int offset, int length) |
| Prints the specified array of bytes with a given label if debug mode is enabled. | |
| static final void | debug (String lbl, Throwable t) |
| Prints the specified exception with a given label if debug mode is enabled. | |
| static final void | stackTrace () |
| Prints out an exception stack trace for debugging purposes. | |
Static Package Functions | |
| [static initializer] | |
| Static constructor. | |
This class is intended to help both developers of the 1-Wire API for Java and developers using the 1-Wire API for Java to have a standard method for printing debug messages. Applications that want to see debug messages should call the setDebugMode(boolean) method. Classes that want to print information under debugging circumstances should call the debug(String) method.
Debug printing is turned off by default.
| [static initializer] | ( | ) | [static, package] |
Static constructor.
Checks system properties to see if debugging is enabled by default. Also, will redirect debug output to a log file if specified.
| static final void debug | ( | String | x | ) | [static] |
Prints the specified java.lang.String object if debug mode is enabled.
This method calls PrintStream.println(String), and pre-pends the String ">> " to the message, so taht if a program were to call (when debug mode was enabled):
com.dalsemi.onewire.debug.Debug.debug("Some notification...");
the resulting output would look like:
>> Some notification...
| x | the message to print out if in debug mode |
| static final void debug | ( | String | lbl, |
| Throwable | t | ||
| ) | [static] |
Prints the specified exception with a given label if debug mode is enabled.
This method calls PrintStream.println(String), and pre-pends the String ">> " to the message, so taht if a program were to call (when debug mode was enabled):
com.dalsemi.onewire.debug.Debug.debug("Some notification...", exception);
the resulting output would look like:
>> my label
>> OneWireIOException: Device Not Present
| lbl | the message to print out above the array |
| bytes | the byte array to print out |
| offset | the offset to start printing from the array |
| length | the number of bytes to print from the array |
| static final void debug | ( | String | lbl, |
| byte[] | bytes, | ||
| int | offset, | ||
| int | length | ||
| ) | [static] |
Prints the specified array of bytes with a given label if debug mode is enabled.
This method calls PrintStream.println(String), and pre-pends the String ">> " to the message, so taht if a program were to call (when debug mode was enabled):
com.dalsemi.onewire.debug.Debug.debug("Some notification...", myBytes, 0, 8);
the resulting output would look like:
>> my label
>> FF F1 F2 F3 F4 F5 F6 FF
| lbl | the message to print out above the array |
| bytes | the byte array to print out |
| offset | the offset to start printing from the array |
| length | the number of bytes to print from the array |
| static final void debug | ( | String | lbl, |
| byte[] | bytes | ||
| ) | [static] |
Prints the specified array of bytes with a given label if debug mode is enabled.
This method calls PrintStream.println(String), and pre-pends the String ">> " to the message, so taht if a program were to call (when debug mode was enabled):
com.dalsemi.onewire.debug.Debug.debug("Some notification...", myBytes);
the resulting output would look like:
>> my label
>> FF F1 F2 F3 F4 F5 F6 FF
| lbl | the message to print out above the array |
| bytes | the byte array to print out |
| static final boolean getDebugMode | ( | ) | [static] |
Gets the debug printing mode for this application.
true indicates debug messages are on, false supresses them. | static final void setDebugMode | ( | boolean | onoff | ) | [static] |
Sets the debug printing mode for this application.
| <code>true</code> | to see debug messages, false to suppress them |
| static final void setPrintStream | ( | PrintStream | outStream | ) | [static] |
Sets the output stream for printing the debug info.
| out | the output stream for printing the debug info. |
| static final void stackTrace | ( | ) | [static] |
Prints out an exception stack trace for debugging purposes.
This is useful to figure out which functions are calling a particular function at runtime.
1.7.3