|
1-Wire API for .NET Version 4.00
|
Inherits com::dalsemi::onewire::container::OneWireContainer, com::dalsemi::onewire::container::TemperatureContainer, and com::dalsemi::onewire::container::SwitchContainer.
Public Member Functions | |
| OneWireContainer42 () | |
Creates an empty OneWireContainer42. | |
| OneWireContainer42 (DSPortAdapter sourceAdapter, byte[] newAddress) | |
Creates a OneWireContainer42 with the provided adapter object and the address of this One-Wire device. | |
| OneWireContainer42 (DSPortAdapter sourceAdapter, long newAddress) | |
Creates a OneWireContainer42 with the provided adapter object and the address of this One-Wire device. | |
| OneWireContainer42 (DSPortAdapter sourceAdapter, String newAddress) | |
Creates a OneWireContainer42 with the provided adapter object and the address of this One-Wire device. | |
| Enumeration | getMemoryBanks () |
| Gets an enumeration of memory bank instances that implement one or more of the following interfaces: MemoryBank, PagedMemoryBank, and OTPMemoryBank. | |
| String | getName () |
Retrieves the Maxim Integrated Products part number of this OneWireContainer42 as a String. | |
| String | getAlternateNames () |
| Retrieves the alternate Maxim Integrated Products part numbers or names. | |
| String | getDescription () |
Retrieves a short description of the function of this device OneWireContainer42 type. | |
| int | getMaxSpeed () |
| Returns the maximum speed this iButton or 1-Wire device can communicate at. | |
| boolean | hasTemperatureAlarms () |
| Checks to see if this temperature measuring device has high/low trip alarms. | |
| boolean | hasSelectableTemperatureResolution () |
| Checks to see if this device has selectable temperature resolution. | |
| double[] | getTemperatureResolutions () |
| Gets an array of available temperature resolutions in Celsius. | |
| double | getTemperatureAlarmResolution () |
| Gets the temperature alarm resolution in Celsius. | |
| double | getMaxTemperature () |
| Gets the maximum temperature in Celsius. | |
| double | getMinTemperature () |
| Gets the minimum temperature in Celsius. | |
| void | doTemperatureConvert (byte[] state) throws OneWireIOException, OneWireException |
Performs a temperature conversion on state information. | |
| double | getTemperature (byte[] state) throws OneWireIOException |
Gets the temperature value in Celsius from the state data retrieved from the readDevice() method. | |
| double | getTemperatureAlarm (int alarmType, byte[] state) |
Gets the specified temperature alarm value in Celsius from the state data retrieved from the readDevice() method. | |
| double | getTemperatureResolution (byte[] state) |
Gets the current temperature resolution in Celsius from the state data retrieved from the readDevice() method. | |
| void | setTemperatureAlarm (int alarmType, double alarmValue, byte[] state) throws OneWireException, OneWireIOException |
Sets the temperature alarm value in Celsius in the provided state data. | |
| void | setTemperatureResolution (double resolution, byte[] state) throws OneWireException |
Sets the current temperature resolution in Celsius in the provided state data. | |
| byte[] | readDevice () throws OneWireIOException, OneWireException |
Retrieves this OneWireContainer42 state information. | |
| void | writeDevice (byte[] state) throws OneWireIOException, OneWireException |
Writes to this OneWireContainer42 state information that have been changed by 'set' methods. | |
| byte[] | readScratchpad () throws OneWireIOException, OneWireException |
| Reads the Scratchpad of the DS28EA00. | |
| void | writeScratchpad (byte[] data) throws OneWireIOException, OneWireException |
| Writes to the Scratchpad of the DS28EA00. | |
| void | copyScratchpad () throws OneWireIOException, OneWireException |
| Copies the Scratchpad to the E-squared memory of the DS28EA00. | |
| byte[] | recallE2 () throws OneWireIOException, OneWireException |
Recalls the DS28EA00 temperature trigger values (ALARM_HIGH and ALARM_LOW) and the configuration register to the scratchpad and reads the scratchpad. | |
| boolean | isExternalPowerSupplied () throws OneWireIOException, OneWireException |
| Reads the way power is supplied to the DS28EA00. | |
| float | convertToFahrenheit (float celsiusTemperature) |
| Converts a temperature reading from Celsius to Fahrenheit. | |
| int | getNumberChannels (byte[] state) |
| Gets the number of channels supported by this switch. | |
| boolean | isHighSideSwitch () |
| Checks if the channels of this switch are 'high side' switches. | |
| boolean | hasActivitySensing () |
| Checks if the channels of this switch support activity sensing. | |
| boolean | hasLevelSensing () |
| Checks if the channels of this switch support level sensing. | |
| boolean | hasSmartOn () |
| Checks if the channels of this switch support 'smart on'. | |
| boolean | onlySingleChannelOn () |
| Checks if the channels of this switch require that only one channel is on at any one time. | |
| boolean | getLevel (int channel, byte[] state) |
| Checks the sensed level on the indicated channel. | |
| boolean | getLatchState (int channel, byte[] state) |
| Checks the latch state of the indicated channel. | |
| boolean | getSensedActivity (int channel, byte[] state) throws OneWireException |
| This method always returns false for the DS28EA00 (no activity sensing). | |
| void | clearActivity () throws OneWireException |
| This method does nothing for the DS28EA00 (not needed). | |
| void | setLatchState (int channel, boolean latchState, boolean doSmart, byte[] state) |
| Sets the latch state of the indicated channel. | |
| void | setLatchState (byte set, byte[] state) |
| Sets the latch state for all of the channels. | |
| byte[] | readRegister () throws OneWireIOException, OneWireException |
| This method does nothing for the DS28EA00. | |
| void | writeRegister (byte[] register) throws OneWireIOException, OneWireException |
| This method does nothing for the DS28EA00. | |
Static Public Attributes | |
| static final byte | WRITE_SCRATCHPAD_COMMAND = ( byte ) 0x4E |
| DS28EA00 writes data to scratchpad command. | |
| static final byte | READ_SCRATCHPAD_COMMAND = ( byte ) 0xBE |
| DS28EA00 reads data from scratchpad command. | |
| static final byte | COPY_SCRATCHPAD_COMMAND = ( byte ) 0x48 |
| DS28EA00 copys data from scratchpad to E-squared memory command. | |
| static final byte | CONVERT_TEMPERATURE_COMMAND = ( byte ) 0x44 |
| DS28EA00 converts temperature command. | |
| static final byte | RECALL_E2MEMORY_COMMAND = ( byte ) 0xB8 |
| DS28EA00 recalls E-squared memory command. | |
| static final byte | READ_POWER_SUPPLY_COMMAND = ( byte ) 0xB4 |
| DS28EA00 read power supply command. | |
| static final byte | RESOLUTION_12_BIT = ( byte ) 0x7F |
| DS28EA00 12-bit resolution constant for CONFIG byte. | |
| static final byte | RESOLUTION_11_BIT = ( byte ) 0x5F |
| DS28EA00 11-bit resolution constant for CONFIG byte. | |
| static final byte | RESOLUTION_10_BIT = ( byte ) 0x3F |
| DS28EA00 10-bit resolution constant for CONFIG byte. | |
| static final byte | RESOLUTION_9_BIT = ( byte ) 0x1F |
| DS28EA00 9-bit resolution constant for CONFIG byte. | |
| static final byte | PIO_ACCESS_READ = ( byte ) 0xF5 |
| PIO Access read command. | |
| static final byte | PIO_ACCESS_WRITE = ( byte ) 0xA5 |
| PIO Access read command. | |
1-Wire® container for a 1-Wire programmable resolution digital thermometer with "sequence detect" and PIO, the DS28EA00. This container encapsulates the functionality of the iButton family type 42 (hex)
See the temperature usage example in TemperatureContainer for temperature specific operations.
See the switch usage example in SwitchContainer for switch specific operations.
http://www.maxim-ic.com/DS28EA00
Creates an empty OneWireContainer42.
Must call setupContainer() before using this new container.
This is one of the methods to construct a OneWireContainer42. The others are through creating a OneWireContainer42 with parameters.
| OneWireContainer42 | ( | DSPortAdapter | sourceAdapter, |
| byte[] | newAddress | ||
| ) |
Creates a OneWireContainer42 with the provided adapter object and the address of this One-Wire device.
This is one of the methods to construct a OneWireContainer42. The others are through creating a OneWireContainer42 with different parameters types.
| sourceAdapter | adapter object required to communicate with this One-Wire device |
| newAddress | address of this One-Wire device |
| OneWireContainer42 | ( | DSPortAdapter | sourceAdapter, |
| long | newAddress | ||
| ) |
Creates a OneWireContainer42 with the provided adapter object and the address of this One-Wire device.
This is one of the methods to construct a OneWireContainer42. The others are through creating a OneWireContainer42 with different parameters types.
| sourceAdapter | adapter object required to communicate with this One-Wire device |
| newAddress | address of this One-Wire device |
| OneWireContainer42 | ( | DSPortAdapter | sourceAdapter, |
| String | newAddress | ||
| ) |
Creates a OneWireContainer42 with the provided adapter object and the address of this One-Wire device.
This is one of the methods to construct a OneWireContainer42. The others are through creating a OneWireContainer42 with different parameters types.
| sourceAdapter | adapter object required to communicate with this One-Wire device |
| newAddress | address of this One-Wire device |
| void clearActivity | ( | ) | throws OneWireException |
This method does nothing for the DS28EA00 (not needed).
Clears the activity latches the next time possible. For example, on a DS2406/07, this happens the next time the status is read with readDevice().
| OneWireException | if this device does not support activity sensing |
Implements SwitchContainer.
| float convertToFahrenheit | ( | float | celsiusTemperature | ) |
Converts a temperature reading from Celsius to Fahrenheit.
| celsiusTemperature | temperature value in Celsius |
| void copyScratchpad | ( | ) | throws OneWireIOException, OneWireException |
Copies the Scratchpad to the E-squared memory of the DS28EA00.
| OneWireIOException | on a 1-Wire communication error such as reading an incorrect CRC from this OneWireContainer42. This could be caused by a physical interruption in the 1-Wire Network due to shorts or a newly arriving 1-Wire device issuing a 'presence pulse'. |
| OneWireException | on a communication or setup error with the 1-Wire adapter |
| void doTemperatureConvert | ( | byte[] | state | ) | throws OneWireIOException, OneWireException |
Performs a temperature conversion on state information.
| state | byte array with device state information |
| OneWireIOException | on a 1-Wire communication error such as reading an incorrect CRC from this OneWireContainer42. This could be caused by a physical interruption in the 1-Wire Network due to shorts or a newly arriving 1-Wire device issuing a 'presence pulse'. |
| OneWireException | on a communication or setup error with the 1-Wire adapter |
Implements TemperatureContainer.
| String getAlternateNames | ( | ) |
Retrieves the alternate Maxim Integrated Products part numbers or names.
A 'family' of 1-Wire Network devices may have more than one part number depending on packaging. There can also be nicknames such as 'Crypto iButton'.
OneWireContainer42 alternate names Reimplemented from OneWireContainer.
| String getDescription | ( | ) |
Retrieves a short description of the function of this device OneWireContainer42 type.
OneWireContainer42 functional description Reimplemented from OneWireContainer.
| boolean getLatchState | ( | int | channel, |
| byte[] | state | ||
| ) |
Checks the latch state of the indicated channel.
| channel | channel to execute this operation, in the range [0 to (getNumberChannels(byte[]) - 1)] |
| state | current state of the device returned from readDevice() |
true if channel latch is 'on' or conducting and false if channel latch is 'off' and not conducting. Note that the actual output when the latch is 'on' is returned from the isHighSideSwitch() method.Implements SwitchContainer.
| boolean getLevel | ( | int | channel, |
| byte[] | state | ||
| ) |
Checks the sensed level on the indicated channel.
To avoid an exception, verify that this switch has level sensing with the hasLevelSensing(). Level sensing means that the device can sense the logic level on its PIO pin.
| channel | channel to execute this operation, in the range [0 to (getNumberChannels(byte[]) - 1)] |
| state | current state of the device returned from readDevice() |
true if level sensed is 'high' and false if level sensed is 'low'Implements SwitchContainer.
| int getMaxSpeed | ( | ) |
Returns the maximum speed this iButton or 1-Wire device can communicate at.
Reimplemented from OneWireContainer.
| double getMaxTemperature | ( | ) |
Gets the maximum temperature in Celsius.
OneWireContainer42Implements TemperatureContainer.
| Enumeration getMemoryBanks | ( | ) |
Gets an enumeration of memory bank instances that implement one or more of the following interfaces: MemoryBank, PagedMemoryBank, and OTPMemoryBank.
Enumeration of memory banks Reimplemented from OneWireContainer.
| double getMinTemperature | ( | ) |
Gets the minimum temperature in Celsius.
OneWireContainer42Implements TemperatureContainer.
| String getName | ( | ) |
Retrieves the Maxim Integrated Products part number of this OneWireContainer42 as a String.
For example 'DS28EA00'.
OneWireContainer42 name Reimplemented from OneWireContainer.
| int getNumberChannels | ( | byte[] | state | ) |
Gets the number of channels supported by this switch.
Channel specific methods will use a channel number specified by an integer from [0 to (getNumberChannels(byte[]) - 1)]. Note that all devices of the same family will not necessarily have the same number of channels.
| state | current state of the device returned from readDevice() |
Implements SwitchContainer.
| boolean getSensedActivity | ( | int | channel, |
| byte[] | state | ||
| ) | throws OneWireException |
This method always returns false for the DS28EA00 (no activity sensing).
Checks if the indicated channel has experienced activity. This occurs when the level on the PIO pins changes. To clear the activity that is reported, call clearActivity(). To avoid an exception, verify that this device supports activity sensing by calling the method hasActivitySensing().
| channel | channel to execute this operation, in the range [0 to (getNumberChannels(byte[]) - 1)] |
| state | current state of the device returned from readDevice() |
true if activity was detected and false if no activity was detected| OneWireException | if this device does not have activity sensing |
Implements SwitchContainer.
| double getTemperature | ( | byte[] | state | ) | throws OneWireIOException |
Gets the temperature value in Celsius from the state data retrieved from the readDevice() method.
| state | byte array with device state information for this OneWireContainer42 |
doTemperatureConvert()| OneWireIOException | on a 1-Wire communication error such as reading an incorrect CRC from this OneWireContainer42. This could be caused by a physical interruption in the 1-Wire Network due to shorts or a newly arriving 1-Wire device issuing a 'presence pulse'. |
Implements TemperatureContainer.
| double getTemperatureAlarm | ( | int | alarmType, |
| byte[] | state | ||
| ) |
Gets the specified temperature alarm value in Celsius from the state data retrieved from the readDevice() method.
| alarmType | valid value: ALARM_HIGH or ALARM_LOW |
| state | byte array with device state information |
OneWireContainer42Implements TemperatureContainer.
| double getTemperatureAlarmResolution | ( | ) |
Gets the temperature alarm resolution in Celsius.
OneWireContainer42Implements TemperatureContainer.
| double getTemperatureResolution | ( | byte[] | state | ) |
Gets the current temperature resolution in Celsius from the state data retrieved from the readDevice() method.
| state | byte array with device state information |
OneWireContainer42Implements TemperatureContainer.
| double [] getTemperatureResolutions | ( | ) |
Gets an array of available temperature resolutions in Celsius.
OneWireContainer42. The minimum resolution is returned as the first element and maximum resolution as the last element.Implements TemperatureContainer.
| boolean hasActivitySensing | ( | ) |
Checks if the channels of this switch support activity sensing.
If this method returns true then the method getSensedActivity(int,byte[]) can be used.
true if channels support activity sensingImplements SwitchContainer.
| boolean hasLevelSensing | ( | ) |
Checks if the channels of this switch support level sensing.
If this method returns true then the method getLevel(int,byte[]) can be used.
true if channels support level sensingImplements SwitchContainer.
| boolean hasSelectableTemperatureResolution | ( | ) |
Checks to see if this device has selectable temperature resolution.
true if this OneWireContainer42 has selectable temperature resolutionImplements TemperatureContainer.
| boolean hasSmartOn | ( | ) |
Checks if the channels of this switch support 'smart on'.
Smart on is the ability to turn on a channel such that only 1-Wire device on this channel are awake and ready to do an operation. This greatly reduces the time to discover the device down a branch. If this method returns true then the method setLatchState(int,boolean,boolean,byte[]) can be used with the doSmart parameter true.
true if channels support 'smart on'Implements SwitchContainer.
| boolean hasTemperatureAlarms | ( | ) |
Checks to see if this temperature measuring device has high/low trip alarms.
true if this OneWireContainer42 has high/low trip alarmsImplements TemperatureContainer.
| boolean isExternalPowerSupplied | ( | ) | throws OneWireIOException, OneWireException |
Reads the way power is supplied to the DS28EA00.
true for external power, false for parasite power| OneWireIOException | on a 1-Wire communication error such as reading an incorrect CRC from this OneWireContainer42. This could be caused by a physical interruption in the 1-Wire Network due to shorts or a newly arriving 1-Wire device issuing a 'presence pulse'. |
| OneWireException | on a communication or setup error with the 1-Wire adapter |
| boolean isHighSideSwitch | ( | ) |
Checks if the channels of this switch are 'high side' switches.
This indicates that when 'on' or true, the switch output is connect to the 1-Wire data. If this method returns false then when the switch is 'on' or true, the switch is connected to ground.
true if the switch is a 'high side' switch, false if the switch is a 'low side' switchImplements SwitchContainer.
| boolean onlySingleChannelOn | ( | ) |
Checks if the channels of this switch require that only one channel is on at any one time.
If this method returns true then the method setLatchState(int,boolean,boolean,byte[]) will not only affect the state of the given channel but may affect the state of the other channels as well to insure that only one channel is on at a time.
true if only one channel can be on at a time.Implements SwitchContainer.
| byte [] readDevice | ( | ) | throws OneWireIOException, OneWireException |
Retrieves this OneWireContainer42 state information.
The state information is returned as a byte array. Pass this byte array to the 'get' and 'set' methods. If the device state needs to be changed, then call the writeDevice() to finalize the changes.
OneWireContainer42 state information. Device state looks like this: 0 : temperature LSB 1 : temperature MSB 2 : trip high 3 : trip low 4 : configuration register (for resolution) 5 : reserved 6 : reserved 7 : reserved 8 : an 8 bit CRC of the previous 8 bytes 9 : PIO Status bit assignment to write (this is a "don't care" for a read) 10: PIO Status bit assignment to read
PIO Status Bit Assignment from PIO Access Write [A5H]: b7-b2 = all ones b1=PIOB Pin State b0=PIOA Pin State
PIO Status Bit Assignment from PIO Access Read [F5H]: b7-b4 = Complement of b3 to b0 b3= PIOB Output Latch State b2=PIOB Pin State b1=PIOA Output Latch State b0= PIOA Pin State
| OneWireIOException | on a 1-Wire communication error such as reading an incorrect CRC from this OneWireContainer42. This could be caused by a physical interruption in the 1-Wire Network due to shorts or a newly arriving 1-Wire device issuing a 'presence pulse'. |
| OneWireException | on a communication or setup error with the 1-Wire adapter |
Implements OneWireSensor.
| byte [] readRegister | ( | ) | throws OneWireIOException, OneWireException |
This method does nothing for the DS28EA00.
| OneWireIOException | on a 1-Wire communication error such as reading an incorrect CRC from a 1-Wire device. This could be caused by a physical interruption in the 1-Wire Network due to shorts or a newly arriving 1-Wire device issuing a 'presence pulse'. |
| OneWireException | on a communication or setup error with the 1-Wire adapter |
| byte [] readScratchpad | ( | ) | throws OneWireIOException, OneWireException |
Reads the Scratchpad of the DS28EA00.
| OneWireIOException | on a 1-Wire communication error such as reading an incorrect CRC from this OneWireContainer42. This could be caused by a physical interruption in the 1-Wire Network due to shorts or a newly arriving 1-Wire device issuing a 'presence pulse'. |
| OneWireException | on a communication or setup error with the 1-Wire adapter |
| byte [] recallE2 | ( | ) | throws OneWireIOException, OneWireException |
Recalls the DS28EA00 temperature trigger values (ALARM_HIGH and ALARM_LOW) and the configuration register to the scratchpad and reads the scratchpad.
| OneWireIOException | on a 1-Wire communication error such as reading an incorrect CRC from this OneWireContainer42. This could be caused by a physical interruption in the 1-Wire Network due to shorts or a newly arriving 1-Wire device issuing a 'presence pulse'. |
| OneWireException | on a communication or setup error with the 1-Wire adapter |
| void setLatchState | ( | int | channel, |
| boolean | latchState, | ||
| boolean | doSmart, | ||
| byte[] | state | ||
| ) |
Sets the latch state of the indicated channel.
The method writeDevice() must be called to finalize changes to the device. Note that multiple 'set' methods can be called before one call to writeDevice().
| channel | channel to execute this operation, in the range [0 to (getNumberChannels(byte[]) - 1)] |
| latchState | true to set the channel latch 'on' (conducting) and false to set the channel latch 'off' (not conducting). Note that the actual output when the latch is 'on' is returned from the isHighSideSwitch() method. |
| doSmart | If latchState is 'on'/true then doSmart indicates if a 'smart on' is to be done. To avoid an exception check the capabilities of this device using the hasSmartOn() method. |
| state | current state of the device returned from readDevice() |
Implements SwitchContainer.
| void setLatchState | ( | byte | set, |
| byte[] | state | ||
| ) |
Sets the latch state for all of the channels.
The method writeDevice() must be called to finalize changes to the device. Note that multiple 'set' methods can be called before one call to writeDevice().
| set | the state to set all of the channels, in the range [0 to (getNumberChannels(byte[]) - 1)] |
| state | current state of the device returned from readDevice() |
| void setTemperatureAlarm | ( | int | alarmType, |
| double | alarmValue, | ||
| byte[] | state | ||
| ) | throws OneWireException, OneWireIOException |
Sets the temperature alarm value in Celsius in the provided state data.
Use the method writeDevice() with this data to finalize the change to the device.
| alarmType | valid value: ALARM_HIGH or ALARM_LOW |
| alarmValue | alarm trip value in Celsius |
| state | byte array with device state information |
Implements TemperatureContainer.
| void setTemperatureResolution | ( | double | resolution, |
| byte[] | state | ||
| ) | throws OneWireException |
Sets the current temperature resolution in Celsius in the provided state data.
Use the method writeDevice() with this data to finalize the change to the device.
| resolution | temperature resolution in Celsius. Valid values are RESOLUTION_9_BIT, RESOLUTION_10_BIT, RESOLUTION_11_BIT and RESOLUTION_12_BIT. |
| state | byte array with device state information |
Implements TemperatureContainer.
| void writeDevice | ( | byte[] | state | ) | throws OneWireIOException, OneWireException |
Writes to this OneWireContainer42 state information that have been changed by 'set' methods.
Only the device's "changed" state information is written to the part. This is done by referencing a field information appended to the state data.
| state | byte array with device state information from a previous readDevice() |
| OneWireIOException | on a 1-Wire communication error such as reading an incorrect CRC from this OneWireContainer42. This could be caused by a physical interruption in the 1-Wire Network due to shorts or a newly arriving 1-Wire device issuing a 'presence pulse'. |
| OneWireException | on a communication or setup error with the 1-Wire adapter |
Implements OneWireSensor.
| void writeRegister | ( | byte[] | register | ) | throws OneWireIOException, OneWireException |
This method does nothing for the DS28EA00.
| register | 1-Wire device sensor state |
| OneWireIOException | on a 1-Wire communication error such as reading an incorrect CRC from a 1-Wire device. This could be caused by a physical interruption in the 1-Wire Network due to shorts or a newly arriving 1-Wire device issuing a 'presence pulse'. |
| OneWireException | on a communication or setup error with the 1-Wire adapter |
| void writeScratchpad | ( | byte[] | data | ) | throws OneWireIOException, OneWireException |
Writes to the Scratchpad of the DS28EA00.
| data | data to be written to the scratchpad. First byte of data must be the temperature High Trip Point, the second byte must be the temperature Low Trip Point, and the third must be the Resolution (configuration register). |
| OneWireIOException | on a 1-Wire communication error such as reading an incorrect CRC from this OneWireContainer42. This could be caused by a physical interruption in the 1-Wire Network due to shorts or a newly arriving 1-Wire device issuing a 'presence pulse'. |
| OneWireException | on a communication or setup error with the 1-Wire adapter |
| IllegalArgumentException | when data is of invalid length |
final byte READ_POWER_SUPPLY_COMMAND = ( byte ) 0xB4 [static] |
DS28EA00 read power supply command.
This command is used to determine if external power is supplied.
1.7.3