|
1-Wire API for .NET Version 4.00
|
Inherits com::dalsemi::onewire::container::OneWireContainer.
Public Member Functions | |
| OneWireContainer33 () | |
| Default Constructor OneWireContainer33. | |
| OneWireContainer33 (DSPortAdapter sourceAdapter, byte[] newAddress) | |
| Create a container with a provided adapter object and the address of the iButton or 1-Wire device. | |
| OneWireContainer33 (DSPortAdapter sourceAdapter, long newAddress) | |
| Create a container with a provided adapter object and the address of the iButton or 1-Wire device. | |
| OneWireContainer33 (DSPortAdapter sourceAdapter, String newAddress) | |
| Create a container with a provided adapter object and the address of the iButton or 1-Wire device. | |
| void | setupContainer (DSPortAdapter sourceAdapter, byte[] newAddress) |
| Provide this container the adapter object used to access this device and provide the address of this iButton or 1-Wire device. | |
| void | setupContainer (DSPortAdapter sourceAdapter, long newAddress) |
| Provide this container the adapter object used to access this device and provide the address of this iButton or 1-Wire device. | |
| void | setupContainer (DSPortAdapter sourceAdapter, String newAddress) |
| Provide this container the adapter object used to access this device and provide the address of this iButton or 1-Wire device. | |
| String | getName () |
| Retrieve the Maxim Integrated Products part number of the iButton as a string. | |
| String | getAlternateNames () |
| Retrieve the alternate Maxim Integrated Products part numbers or names. | |
| String | getDescription () |
| Retrieve a short description of the function of the iButton type. | |
| int | getMaxSpeed () |
| Returns the maximum speed this iButton can communicate at. | |
| Enumeration | getMemoryBanks () |
| Get an enumeration of memory bank instances that implement one or more of the following interfaces: MemoryBank, PagedMemoryBank, and OTPMemoryBank. | |
| MemoryBankScratchSHAEE | getScratchpadMemoryBank () |
| Returns the instance of the Scratchpad memory bank. | |
| MemoryBankSHAEE | getStatusPageMemoryBank () |
| Returns the instance of the Status page memory bank. | |
| MemoryBankSHAEE | getMemoryBankForPage (int page) |
| Returns the instance of the memory bank for a particular page. | |
| void | setContainerSecret (byte[] newSecret, int offset) |
| Sets the bus master secret for this DS2432. | |
| void | getContainerSecret (byte[] secretBuf, int offset) |
| Get the secret of this device as an array of bytes. | |
| boolean | isContainerSecretSet () throws OneWireIOException, OneWireException |
| Get the current status of the secret. | |
| boolean | isSecretWriteProtected () throws OneWireIOException, OneWireException |
| Get the status of the secret, if it is write protected. | |
| void | setChallenge (byte[] challengeset, int offset) |
| Sets the challenge for the Read Authenticate Page. | |
| void | getChallenge (byte[] get, int offset) |
| Get the challenge of this device as an array of bytes. | |
| boolean | isWriteProtectAllSet () throws OneWireIOException, OneWireException |
| Get the status of all the pages, if they are write protected. | |
| void | writeProtectSecret () throws OneWireIOException, OneWireException |
| Write protects the secret for the DS2432. | |
| void | writeProtectAll () throws OneWireIOException, OneWireException |
| Write protect pages 0 to 3. | |
| void | setEPROMModePageOne () throws OneWireIOException, OneWireException |
| Sets the EPROM mode for page 1. | |
| boolean | isPageOneEPROMmode () throws OneWireIOException, OneWireException |
| Tells if page one is in EPROM mode. | |
| void | writeProtectPageZero () throws OneWireIOException, OneWireException |
| Write protect page zero only. | |
| boolean | isWriteProtectPageZeroSet () throws OneWireIOException, OneWireException |
| Get the status of page zero, if it is write protected. | |
| void | computeNextSecret (int pageNum, byte[] partialsecret, int offset) throws OneWireIOException, OneWireException |
| Compute Next Secret. | |
| void | computeNextSecret (int pageNum) throws OneWireIOException, OneWireException |
| Compute Next Secret using the current contents of data page and scratchpad. | |
| boolean | loadFirstSecret (byte[] data, int offset) throws OneWireIOException, OneWireException |
| Load First Secret. | |
| boolean | refreshPage (int page, int offset) throws OneWireException, OneWireIOException |
| Refreshes a particular 8-byte set of data on a given page. | |
| boolean | refreshPage (int page) throws OneWireException, OneWireIOException |
| Refreshes all 32 bytes of data on a given page. | |
| boolean | installMasterSecret (int page, byte[] newSecret) throws OneWireIOException, OneWireException |
| boolean | bindSecretToiButton (int pageNum, byte[] bindData) throws OneWireIOException, OneWireException |
| boolean | writeDataPage (int targetPage, byte[] pageData) throws OneWireIOException, OneWireException |
| boolean | writeDataPage (int targetPage, byte[] pageData, int offset) throws OneWireIOException, OneWireException |
| boolean | writeScratchpad (int targetPage, int targetPageOffset, byte[] inputbuffer, int start, int length) throws OneWireIOException, OneWireException |
| void | readScratchpad (byte[] scratchpad, int offset, byte[] extraInfo) throws OneWireIOException, OneWireException |
| Read from the Scratch Pad, which is a max of 8 bytes. | |
| boolean | copyScratchpad (int targetPage, int targetPageOffset, byte[] copy_auth, int authStart) throws OneWireIOException, OneWireException |
| Copy all 8 bytes of the Sratch Pad to a certain page and offset in memory. | |
| boolean | copyScratchpad (int targetPage, int targetPageOffset) throws OneWireIOException, OneWireException |
| Copy all 8 bytes of the Sratch Pad to a certain page and offset in memory. | |
| boolean | readMemoryPage (int page, byte[] pageData, int offset) throws OneWireIOException, OneWireException |
| Reads a page of memory. | |
| boolean | readAuthenticatedPage (int page, byte[] pagedata, int offset, byte[] computed_mac, int macStart) throws OneWireIOException, OneWireException |
Static Public Member Functions | |
| static boolean | isMACValid (int addr, byte[] SerNum, byte[] memory, byte[] mac, byte[] challenge, byte[] secret) |
| Authenticates page data given a MAC. | |
Protected Member Functions | |
| boolean | adapterSet () |
| Tells whether an adapter has been set. | |
| boolean | checkStatus () throws OneWireIOException, OneWireException |
| To check the status of the part. | |
Protected Attributes | |
| boolean | secretSet |
| Flag to indicate if the secret has been set. | |
| boolean | secretProtected |
| Flag to indicate if the secret is write protected. | |
| boolean | setAdapter |
| Flag to indicate if the adapter has been specified. | |
| boolean | container_check |
| Flag to indicate if the status has been checked. | |
Static Protected Attributes | |
| static final byte[] | ffBlock |
| block of 0xFF's used for faster read pre-fill of 1-Wire blocks | |
| static final byte[] | zeroBlock |
| block of 0xFF's used for faster erase of blocks | |
1-Wire® container for the '1K-Bit protected 1-Wire EEPROM with SHA-1 Engine' family type 33 (hex), Maxim Integrated Products part number: DS1961S,DS2432.
The memory can also be accessed through the objects that are returned from the getMemoryBanks method.
The following is a list of the MemoryBank instances that are returned:
Display some features of isMACValid where owd is an instanceof OneWireContainer33 and bank is an instanceof PagedMemoryBank:
byte[] read_buf = new byte [bank.getPageLength()];
byte[] extra_buf = new byte [bank.getExtraInfoLength()];
byte[] challenge = new byte [8]; // read a page (use the most verbose and secure method)
if (bank.hasPageAutoCRC())
{
System.out.println("Using device generated CRC"); if (bank.hasExtraInfo())
{
bank.readPageCRC(pg, false, read_buf, 0, extra_buf); owd.getChallenge(challenge,0);
owd.getContainerSecret(secret, 0);
sernum = owd.getAddress();
macvalid = owd.isMACValid(bank.getStartPhysicalAddress()+pg*bank.getPageLength(),
sernum,read_buf,extra_buf,challenge,secret);
}
else
bank.readPageCRC(pg, false, read_buf, 0);
}
else
{
if (bank.hasExtraInfo())
bank.readPage(pg, false, read_buf, 0, extra_buf);
else
bank.readPage(pg, false, read_buf, 0);
}
http://pdfserv.maxim-ic.com/arpdf/DS2432.pdf
Default Constructor OneWireContainer33.
Must call setupContainer before using.
| OneWireContainer33 | ( | DSPortAdapter | sourceAdapter, |
| byte[] | newAddress | ||
| ) |
Create a container with a provided adapter object and the address of the iButton or 1-Wire device.
| sourceAdapter | adapter object required to communicate with this iButton. |
| newAddress | address of this 1-Wire device |
| OneWireContainer33 | ( | DSPortAdapter | sourceAdapter, |
| long | newAddress | ||
| ) |
Create a container with a provided adapter object and the address of the iButton or 1-Wire device.
| sourceAdapter | adapter object required to communicate with this iButton. |
| newAddress | address of this 1-Wire device |
| OneWireContainer33 | ( | DSPortAdapter | sourceAdapter, |
| String | newAddress | ||
| ) |
Create a container with a provided adapter object and the address of the iButton or 1-Wire device.
| sourceAdapter | adapter object required to communicate with this iButton. |
| newAddress | address of this 1-Wire device |
| boolean adapterSet | ( | ) | [protected] |
Tells whether an adapter has been set.
| boolean bindSecretToiButton | ( | int | pageNum, |
| byte[] | bindData | ||
| ) | throws OneWireIOException, OneWireException |
Binds an installed secret to a DS1961S/DS2432 by using well-known binding data and the DS1961S/DS2432's unique address. This makes the secret unique for this iButton.
| page | the page number that has the master secret already installed |
| bind_data | 32 bytes of binding data used to bind the iButton to the system |
true if successful| OneWireIOException | on a 1-Wire communication error such as reading an incorrect CRC from a 1-Wire device. This could be caused by a physical interruption in the 1-Wire Network due to shorts or a newly arriving 1-Wire device issuing a 'presence pulse'. |
| OneWireException | on a communication or setup error with the 1-Wire adapter |
| boolean checkStatus | ( | ) | throws OneWireIOException, OneWireException [protected] |
To check the status of the part.
| void computeNextSecret | ( | int | pageNum | ) | throws OneWireIOException, OneWireException |
Compute Next Secret using the current contents of data page and scratchpad.
| addr | address of page to use for the next secret computation. |
| void computeNextSecret | ( | int | pageNum, |
| byte[] | partialsecret, | ||
| int | offset | ||
| ) | throws OneWireIOException, OneWireException |
Compute Next Secret.
| addr | address of page to use for the next secret computation. |
| parialsecret | the data to put into the scrathpad in computing next secret. |
| boolean copyScratchpad | ( | int | targetPage, |
| int | targetPageOffset, | ||
| byte[] | copy_auth, | ||
| int | authStart | ||
| ) | throws OneWireIOException, OneWireException |
Copy all 8 bytes of the Sratch Pad to a certain page and offset in memory.
| targetPage | the page to copy the data to |
| targetPageOffset | the offset into the page to copy to |
| copy_auth | byte[] containing write authorization |
| authStart | the offset into the copy_auth array where the authorization begins. |
| OneWireIOException | |
| OneWireException |
| boolean copyScratchpad | ( | int | targetPage, |
| int | targetPageOffset | ||
| ) | throws OneWireIOException, OneWireException |
Copy all 8 bytes of the Sratch Pad to a certain page and offset in memory.
The container secret must be set so that the container can produce the correct MAC.
| targetPage | the page to copy the data to |
| targetPageOffset | the offset into the page to copy to |
| OneWireIOException | |
| OneWireException |
| String getAlternateNames | ( | ) |
Retrieve the alternate Maxim Integrated Products part numbers or names.
A 'family' of MicroLAN devices may have more than one part number depending on packaging.
Reimplemented from OneWireContainer.
| void getChallenge | ( | byte[] | get, |
| int | offset | ||
| ) |
Get the challenge of this device as an array of bytes.
| get | array of bytes containing the iButton challenge |
| void getContainerSecret | ( | byte[] | secretBuf, |
| int | offset | ||
| ) |
Get the secret of this device as an array of bytes.
| secretBuf | array of bytes for holding the container secret |
| offset | index into array to copy the secret to |
| String getDescription | ( | ) |
Retrieve a short description of the function of the iButton type.
Reimplemented from OneWireContainer.
| int getMaxSpeed | ( | ) |
Returns the maximum speed this iButton can communicate at.
Reimplemented from OneWireContainer.
| MemoryBankSHAEE getMemoryBankForPage | ( | int | page | ) |
Returns the instance of the memory bank for a particular page.
| page | the page for the requested memory bank; |
| Enumeration getMemoryBanks | ( | ) |
Get an enumeration of memory bank instances that implement one or more of the following interfaces: MemoryBank, PagedMemoryBank, and OTPMemoryBank.
Enumeration of memory banks Reimplemented from OneWireContainer.
| String getName | ( | ) |
Retrieve the Maxim Integrated Products part number of the iButton as a string.
For example 'DS1992'.
Reimplemented from OneWireContainer.
| MemoryBankScratchSHAEE getScratchpadMemoryBank | ( | ) |
Returns the instance of the Scratchpad memory bank.
Contains methods for reading/writing the Scratchpad contents. Also, methods for Load First Secret, Compute Next Secret, and Refresh Scratchpad
| MemoryBankSHAEE getStatusPageMemoryBank | ( | ) |
Returns the instance of the Status page memory bank.
| boolean installMasterSecret | ( | int | page, |
| byte[] | newSecret | ||
| ) | throws OneWireIOException, OneWireException |
Installs a secret on a DS1961S/DS2432. The secret is written in partial phrases of 47 bytes (32 bytes to a memory page, 8 bytes to the scratchpad, 7 bytes are discarded (but included for compatibility with DS193S)) and is cumulative until the entire secret is processed.
On TINI, this method will be slightly faster if the secret's length is divisible by 47. However, since secret key generation is a part of initialization, it is probably not necessary.
| page | the page number used to write the partial secrets to |
| secret | the entire secret, in partial phrases, to be installed |
true if successful| OneWireIOException | on a 1-Wire communication error such as reading an incorrect CRC from a 1-Wire device. This could be caused by a physical interruption in the 1-Wire Network due to shorts or a newly arriving 1-Wire device issuing a 'presence pulse'. |
| OneWireException | on a communication or setup error with the 1-Wire adapter |
| boolean isContainerSecretSet | ( | ) | throws OneWireIOException, OneWireException |
Get the current status of the secret.
| OneWireIOException | |
| OneWireException |
| static boolean isMACValid | ( | int | addr, |
| byte[] | SerNum, | ||
| byte[] | memory, | ||
| byte[] | mac, | ||
| byte[] | challenge, | ||
| byte[] | secret | ||
| ) | [static] |
Authenticates page data given a MAC.
| addr | address of the data to be read |
| memory | the memory read from the page |
| mac | the MAC calculated for this function given back as the extra info |
| challenge | the 3 bytes written to the scratch pad used in calculating the mac |
| boolean isPageOneEPROMmode | ( | ) | throws OneWireIOException, OneWireException |
Tells if page one is in EPROM mode.
| OneWireIOException | |
| OneWireException |
| boolean isSecretWriteProtected | ( | ) | throws OneWireIOException, OneWireException |
Get the status of the secret, if it is write protected.
| OneWireIOException | |
| OneWireException |
| boolean isWriteProtectAllSet | ( | ) | throws OneWireIOException, OneWireException |
Get the status of all the pages, if they are write protected.
| OneWireIOException | |
| OneWireException |
| boolean isWriteProtectPageZeroSet | ( | ) | throws OneWireIOException, OneWireException |
Get the status of page zero, if it is write protected.
| OneWireIOException | |
| OneWireException |
| boolean loadFirstSecret | ( | byte[] | data, |
| int | offset | ||
| ) | throws OneWireIOException, OneWireException |
Load First Secret.
| OneWireIOException | |
| OneWireException |
| boolean readAuthenticatedPage | ( | int | page, |
| byte[] | pagedata, | ||
| int | offset, | ||
| byte[] | computed_mac, | ||
| int | macStart | ||
| ) | throws OneWireIOException, OneWireException |
Reads and authenticates a page. See readMemoryPage() for a description of page numbers and their contents. This method will also generate a signature for the selected page, used in the authentication of roving (User) iButtons.
| pageNum | page number to read and authenticate |
| pagedata | array for the page data. |
| offset | offset to copy into the array |
| computed_mac | array for the MAC returned by the device. |
| macStart | offset to copy into the mac array |
true if successful, false if the operation failed while waiting for the DS1963S's output to alternate| OneWireIOException | on a 1-Wire communication error such as reading an incorrect CRC from a 1-Wire device. This could be caused by a physical interruption in the 1-Wire Network due to shorts or a newly arriving 1-Wire device issuing a 'presence pulse'. |
| OneWireException | on a communication or setup error with the 1-Wire adapter |
| boolean readMemoryPage | ( | int | page, |
| byte[] | pageData, | ||
| int | offset | ||
| ) | throws OneWireIOException, OneWireException |
Reads a page of memory.
| page | page number to read packet from |
| pageData | byte array to place read data into |
| offset | offset into readBuf to place data |
| OneWireIOException | |
| OneWireException |
| void readScratchpad | ( | byte[] | scratchpad, |
| int | offset, | ||
| byte[] | extraInfo | ||
| ) | throws OneWireIOException, OneWireException |
Read from the Scratch Pad, which is a max of 8 bytes.
| scratchpad | byte array to place read data into length of array is always pageLength. |
| offset | offset into readBuf to pug data |
| extraInfo | byte array to put extra info read into (TA1, TA2, e/s byte) Can be 'null' if extra info is not needed. |
| OneWireIOException | |
| OneWireException |
| boolean refreshPage | ( | int | page, |
| int | offset | ||
| ) | throws OneWireException, OneWireIOException |
Refreshes a particular 8-byte set of data on a given page.
This will correct any weakly-programmed EEPROM bits. This feature is only available on the DS1961S, but is safely ignored on the DS2432. The refresh consists of a Refresh Scratchpad command followed by a Load First Secret to the same offset.
| page | the page number that contains the 8-bytes to refresh. |
| offset | the offset into the page for the 8-bytes to refresh. |
true if refresh is successful. | boolean refreshPage | ( | int | page | ) | throws OneWireException, OneWireIOException |
Refreshes all 32 bytes of data on a given page.
This will correct any weakly-programmed EEPROM bits. This feature is only available on the DS1961S, but is safely ignored on the DS2432. The refresh consists of a Refresh Scratchpad command followed by a Load First Secret to the same offset, for all 8-byte offsets on the page.
| page | the page number that will be refreshed. |
true if refresh is successful. | void setChallenge | ( | byte[] | challengeset, |
| int | offset | ||
| ) |
Sets the challenge for the Read Authenticate Page.
| challengeset | Challenge for all the memory banks. |
| void setContainerSecret | ( | byte[] | newSecret, |
| int | offset | ||
| ) |
Sets the bus master secret for this DS2432.
| newSecret | Secret for this DS2432. |
| offset | index into array to copy the secret from |
| void setEPROMModePageOne | ( | ) | throws OneWireIOException, OneWireException |
Sets the EPROM mode for page 1.
After setting, Page One can only be written to once.
| void setupContainer | ( | DSPortAdapter | sourceAdapter, |
| byte[] | newAddress | ||
| ) |
Provide this container the adapter object used to access this device and provide the address of this iButton or 1-Wire device.
| sourceAdapter | adapter object required to communicate with this iButton. |
| newAddress | address of this 1-Wire device |
Reimplemented from OneWireContainer.
| void setupContainer | ( | DSPortAdapter | sourceAdapter, |
| String | newAddress | ||
| ) |
Provide this container the adapter object used to access this device and provide the address of this iButton or 1-Wire device.
| sourceAdapter | adapter object required to communicate with this iButton. |
| newAddress | address of this 1-Wire device |
Reimplemented from OneWireContainer.
| void setupContainer | ( | DSPortAdapter | sourceAdapter, |
| long | newAddress | ||
| ) |
Provide this container the adapter object used to access this device and provide the address of this iButton or 1-Wire device.
| sourceAdapter | adapter object required to communicate with this iButton. |
| newAddress | address of this 1-Wire device |
Reimplemented from OneWireContainer.
| boolean writeDataPage | ( | int | targetPage, |
| byte[] | pageData | ||
| ) | throws OneWireIOException, OneWireException |
Writes a data page to the DS1961S/DS2432.
| page_number | page number to write |
| page_data | page data to write (must be at least 32 bytes long) |
true if successful, false if the operation failed| OneWireIOException | on a 1-Wire communication error such as reading an incorrect CRC from a 1-Wire device. This could be caused by a physical interruption in the 1-Wire Network due to shorts or a newly arriving 1-Wire device issuing a 'presence pulse'. |
| OneWireException | on a communication or setup error with the 1-Wire adapter |
| boolean writeDataPage | ( | int | targetPage, |
| byte[] | pageData, | ||
| int | offset | ||
| ) | throws OneWireIOException, OneWireException |
Writes a data page to the DS1961S/DS2432.
| page_number | page number to write |
| page_data | page data to write (must be at least 32 bytes long) |
| offset | the offset to start copying the 32-bytes of page data. |
true if successful, false if the operation failed| OneWireIOException | on a 1-Wire communication error such as reading an incorrect CRC from a 1-Wire device. This could be caused by a physical interruption in the 1-Wire Network due to shorts or a newly arriving 1-Wire device issuing a 'presence pulse'. |
| OneWireException | on a communication or setup error with the 1-Wire adapter |
| boolean writeScratchpad | ( | int | targetPage, |
| int | targetPageOffset, | ||
| byte[] | inputbuffer, | ||
| int | start, | ||
| int | length | ||
| ) | throws OneWireIOException, OneWireException |
Writes data to the scratchpad. In order to write to a data page using this method, next call readScratchPad(), and then copyScratchPad(). Note that the addresses passed to this method will be the addresses the data is copied to if the copyScratchPad() method is called afterward.
Also note that if too many bytes are written, this method will truncate the data so that only a valid number of bytes will be sent.
| targetPage | the page number this data will eventually be copied to |
| targetPageOffset | the offset on the page to copy this data to |
| inputbuffer | the data that will be copied into the scratchpad |
| start | offset into the input buffer for the data to write |
| length | number of bytes to write |
true if successful, false on a CRC error| OneWireIOException | on a 1-Wire communication error such as reading an incorrect CRC from a 1-Wire device. This could be caused by a physical interruption in the 1-Wire Network due to shorts or a newly arriving 1-Wire device issuing a 'presence pulse'. |
| OneWireException | on a communication or setup error with the 1-Wire adapter |
boolean container_check [protected] |
Flag to indicate if the status has been checked.
boolean secretProtected [protected] |
Flag to indicate if the secret is write protected.
boolean secretSet [protected] |
Flag to indicate if the secret has been set.
boolean setAdapter [protected] |
Flag to indicate if the adapter has been specified.
1.7.3