|
1-Wire API for .NET Version 4.00
|
Inherits com::dalsemi::onewire::container::OneWireContainer.
Public Member Functions | |
| OneWireContainer2D () | |
| Default Constructor OneWireContainer2D. | |
| OneWireContainer2D (DSPortAdapter sourceAdapter, byte[] newAddress) | |
| Create a container with a provided adapter object and the address of the iButton or 1-Wire device. | |
| OneWireContainer2D (DSPortAdapter sourceAdapter, long newAddress) | |
| Create a container with a provided adapter object and the address of the iButton or 1-Wire device. | |
| OneWireContainer2D (DSPortAdapter sourceAdapter, String newAddress) | |
| Create a container with a provided adapter object and the address of the iButton or 1-Wire device. | |
| void | setupContainer (DSPortAdapter sourceAdapter, byte[] newAddress) |
| Provide this container the adapter object used to access this device and provide the address of this iButton or 1-Wire device. | |
| void | setupContainer (DSPortAdapter sourceAdapter, long newAddress) |
| Provide this container the adapter object used to access this device and provide the address of this iButton or 1-Wire device. | |
| void | setupContainer (DSPortAdapter sourceAdapter, String newAddress) |
| Provide this container the adapter object used to access this device and provide the address of this iButton or 1-Wire device. | |
| String | getName () |
| Retrieve the Maxim Integrated Products part number of the iButton as a string. | |
| String | getAlternateNames () |
| Retrieve the alternate Maxim Integrated Products part numbers or names. | |
| String | getDescription () |
| Retrieve a short description of the function of the iButton type. | |
| int | getMaxSpeed () |
| Returns the maximum speed this iButton can communicate at. | |
| Enumeration | getMemoryBanks () |
| Get an enumeration of memory bank instances that implement one or more of the following interfaces: MemoryBank, PagedMemoryBank, and OTPMemoryBank. | |
| boolean | isPageWriteOnce (int page) throws OneWireIOException, OneWireException |
| Query to see if current memory bank is write write once such as with EPROM technology. | |
| void | setPageWriteOnce (int page) throws OneWireIOException, OneWireException |
| Lock the specifed page in the current memory bank. | |
Static Public Attributes | |
| static final byte | WRITEONCE_FLAG = ( byte ) 0xAA |
| Page Lock Flag. | |
1-Wire® container for the '1K-Bit protected 1-Wire EEPROM family type 2D (hex), Maxim Integrated Products part number: DS2431.
The memory can also be accessed through the objects that are returned from the getMemoryBanks method.
Default Constructor OneWireContainer2D.
Must call setupContainer before using.
| OneWireContainer2D | ( | DSPortAdapter | sourceAdapter, |
| byte[] | newAddress | ||
| ) |
Create a container with a provided adapter object and the address of the iButton or 1-Wire device.
| sourceAdapter | adapter object required to communicate with this iButton. |
| newAddress | address of this 1-Wire device |
| OneWireContainer2D | ( | DSPortAdapter | sourceAdapter, |
| long | newAddress | ||
| ) |
Create a container with a provided adapter object and the address of the iButton or 1-Wire device.
| sourceAdapter | adapter object required to communicate with this iButton. |
| newAddress | address of this 1-Wire device |
| OneWireContainer2D | ( | DSPortAdapter | sourceAdapter, |
| String | newAddress | ||
| ) |
Create a container with a provided adapter object and the address of the iButton or 1-Wire device.
| sourceAdapter | adapter object required to communicate with this iButton. |
| newAddress | address of this 1-Wire device |
| String getAlternateNames | ( | ) |
Retrieve the alternate Maxim Integrated Products part numbers or names.
A 'family' of MicroLAN devices may have more than one part number depending on packaging.
Reimplemented from OneWireContainer.
| String getDescription | ( | ) |
Retrieve a short description of the function of the iButton type.
Reimplemented from OneWireContainer.
| int getMaxSpeed | ( | ) |
Returns the maximum speed this iButton can communicate at.
Reimplemented from OneWireContainer.
| Enumeration getMemoryBanks | ( | ) |
Get an enumeration of memory bank instances that implement one or more of the following interfaces: MemoryBank, PagedMemoryBank, and OTPMemoryBank.
Enumeration of memory banks Reimplemented from OneWireContainer.
| String getName | ( | ) |
Retrieve the Maxim Integrated Products part number of the iButton as a string.
For example 'DS1992'.
Reimplemented from OneWireContainer.
| boolean isPageWriteOnce | ( | int | page | ) | throws OneWireIOException, OneWireException |
Query to see if current memory bank is write write once such as with EPROM technology.
| void setPageWriteOnce | ( | int | page | ) | throws OneWireIOException, OneWireException |
Lock the specifed page in the current memory bank.
Not supported by all devices. See the method 'canLockPage()'.
| page | number of page to lock |
| OneWireIOException | |
| OneWireException |
| void setupContainer | ( | DSPortAdapter | sourceAdapter, |
| long | newAddress | ||
| ) |
Provide this container the adapter object used to access this device and provide the address of this iButton or 1-Wire device.
| sourceAdapter | adapter object required to communicate with this iButton. |
| newAddress | address of this 1-Wire device |
Reimplemented from OneWireContainer.
| void setupContainer | ( | DSPortAdapter | sourceAdapter, |
| String | newAddress | ||
| ) |
Provide this container the adapter object used to access this device and provide the address of this iButton or 1-Wire device.
| sourceAdapter | adapter object required to communicate with this iButton. |
| newAddress | address of this 1-Wire device |
Reimplemented from OneWireContainer.
| void setupContainer | ( | DSPortAdapter | sourceAdapter, |
| byte[] | newAddress | ||
| ) |
Provide this container the adapter object used to access this device and provide the address of this iButton or 1-Wire device.
| sourceAdapter | adapter object required to communicate with this iButton. |
| newAddress | address of this 1-Wire device |
Reimplemented from OneWireContainer.
1.7.3