, including all inherited members.
| adapter | OneWireContainer | [protected] |
| address | OneWireContainer | [protected] |
| ALARM_HIGH | TemperatureContainer | [static] |
| ALARM_LOW | TemperatureContainer | [static] |
| CONVERT_TEMPERATURE_COMMAND | OneWireContainer28 | [static] |
| convertToFahrenheit(float celsiusTemperature) | OneWireContainer28 | |
| COPY_SCRATCHPAD_COMMAND | OneWireContainer28 | [static] |
| copyScratchpad() | OneWireContainer28 | |
| doSpeed() | OneWireContainer | |
| doTemperatureConvert(byte[] state) | OneWireContainer28 | |
| equals(Object obj) | OneWireContainer | |
| getAdapter() | OneWireContainer | |
| getAddress() | OneWireContainer | |
| getAddressAsLong() | OneWireContainer | |
| getAddressAsString() | OneWireContainer | |
| getAlternateNames() | OneWireContainer28 | |
| getDescription() | OneWireContainer28 | |
| getMaxSpeed() | OneWireContainer | |
| getMaxTemperature() | OneWireContainer28 | |
| getMemoryBanks() | OneWireContainer | |
| getMinTemperature() | OneWireContainer28 | |
| getName() | OneWireContainer28 | |
| getTemperature(byte[] state) | OneWireContainer28 | |
| getTemperatureAlarm(int alarmType, byte[] state) | OneWireContainer28 | |
| getTemperatureAlarmResolution() | OneWireContainer28 | |
| getTemperatureResolution(byte[] state) | OneWireContainer28 | |
| getTemperatureResolutions() | OneWireContainer28 | |
| hashCode() | OneWireContainer | |
| hasSelectableTemperatureResolution() | OneWireContainer28 | |
| hasTemperatureAlarms() | OneWireContainer28 | |
| isAlarming() | OneWireContainer | |
| isExternalPowerSupplied() | OneWireContainer28 | |
| isPresent() | OneWireContainer | |
| OneWireContainer() | OneWireContainer | |
| OneWireContainer(DSPortAdapter sourceAdapter, byte[] newAddress) | OneWireContainer | |
| OneWireContainer(DSPortAdapter sourceAdapter, long newAddress) | OneWireContainer | |
| OneWireContainer(DSPortAdapter sourceAdapter, String newAddress) | OneWireContainer | |
| OneWireContainer28() | OneWireContainer28 | |
| OneWireContainer28(DSPortAdapter sourceAdapter, byte[] newAddress) | OneWireContainer28 | |
| OneWireContainer28(DSPortAdapter sourceAdapter, long newAddress) | OneWireContainer28 | |
| OneWireContainer28(DSPortAdapter sourceAdapter, String newAddress) | OneWireContainer28 | |
| READ_POWER_SUPPLY_COMMAND | OneWireContainer28 | [static] |
| READ_SCRATCHPAD_COMMAND | OneWireContainer28 | [static] |
| readDevice() | OneWireContainer28 | |
| readScratchpad() | OneWireContainer28 | |
| RECALL_E2MEMORY_COMMAND | OneWireContainer28 | [static] |
| recallE2() | OneWireContainer28 | |
| RESOLUTION_10_BIT | OneWireContainer28 | [static] |
| RESOLUTION_11_BIT | OneWireContainer28 | [static] |
| RESOLUTION_12_BIT | OneWireContainer28 | [static] |
| RESOLUTION_9_BIT | OneWireContainer28 | [static] |
| setSpeed(int newSpeed, boolean fallBack) | OneWireContainer | |
| setTemperatureAlarm(int alarmType, double alarmValue, byte[] state) | OneWireContainer28 | |
| setTemperatureResolution(double resolution, byte[] state) | OneWireContainer28 | |
| setupContainer(DSPortAdapter sourceAdapter, byte[] newAddress) | OneWireContainer | |
| setupContainer(DSPortAdapter sourceAdapter, long newAddress) | OneWireContainer | |
| setupContainer(DSPortAdapter sourceAdapter, String newAddress) | OneWireContainer | |
| speed | OneWireContainer | [protected] |
| speedFallBackOK | OneWireContainer | [protected] |
| toString() | OneWireContainer | |
| WRITE_SCRATCHPAD_COMMAND | OneWireContainer28 | [static] |
| writeDevice(byte[] state) | OneWireContainer28 | |
| writeScratchpad(byte[] data) | OneWireContainer28 | |