, including all inherited members.
| adapter | OneWireContainer | [protected] |
| address | OneWireContainer | [protected] |
| canDisableClock() | OneWireContainer24 | |
| doSpeed() | OneWireContainer | |
| equals(Object obj) | OneWireContainer | |
| getAdapter() | OneWireContainer | |
| getAddress() | OneWireContainer | |
| getAddressAsLong() | OneWireContainer | |
| getAddressAsString() | OneWireContainer | |
| getAlternateNames() | OneWireContainer27 | |
| getClock(byte[] state) | OneWireContainer24 | |
| getClockAlarm(byte[] state) | OneWireContainer24 | |
| getClockResolution() | OneWireContainer24 | |
| getDescription() | OneWireContainer27 | |
| getInterruptInterval(byte[] state) | OneWireContainer27 | |
| getMaxSpeed() | OneWireContainer | |
| getMemoryBanks() | OneWireContainer | |
| getName() | OneWireContainer27 | |
| hasClockAlarm() | OneWireContainer24 | |
| hashCode() | OneWireContainer | |
| INTERRUPT_INTERVAL_1 | OneWireContainer27 | [static] |
| INTERRUPT_INTERVAL_131072 | OneWireContainer27 | [static] |
| INTERRUPT_INTERVAL_2048 | OneWireContainer27 | [static] |
| INTERRUPT_INTERVAL_32 | OneWireContainer27 | [static] |
| INTERRUPT_INTERVAL_4 | OneWireContainer27 | [static] |
| INTERRUPT_INTERVAL_4096 | OneWireContainer27 | [static] |
| INTERRUPT_INTERVAL_64 | OneWireContainer27 | [static] |
| INTERRUPT_INTERVAL_65536 | OneWireContainer27 | [static] |
| isAlarming() | OneWireContainer | |
| isClockAlarmEnabled(byte[] state) | OneWireContainer24 | |
| isClockAlarming(byte[] state) | OneWireContainer24 | |
| isClockRunning(byte[] state) | OneWireContainer24 | |
| isInterruptEnabled(byte[] state) | OneWireContainer27 | |
| isPresent() | OneWireContainer | |
| OneWireContainer() | OneWireContainer | |
| OneWireContainer(DSPortAdapter sourceAdapter, byte[] newAddress) | OneWireContainer | |
| OneWireContainer(DSPortAdapter sourceAdapter, long newAddress) | OneWireContainer | |
| OneWireContainer(DSPortAdapter sourceAdapter, String newAddress) | OneWireContainer | |
| OneWireContainer24() | OneWireContainer24 | |
| OneWireContainer24(DSPortAdapter sourceAdapter, byte[] newAddress) | OneWireContainer24 | |
| OneWireContainer24(DSPortAdapter sourceAdapter, long newAddress) | OneWireContainer24 | |
| OneWireContainer24(DSPortAdapter sourceAdapter, String newAddress) | OneWireContainer24 | |
| OneWireContainer27() | OneWireContainer27 | |
| OneWireContainer27(DSPortAdapter sourceAdapter, byte[] newAddress) | OneWireContainer27 | |
| OneWireContainer27(DSPortAdapter sourceAdapter, long newAddress) | OneWireContainer27 | |
| OneWireContainer27(DSPortAdapter sourceAdapter, String newAddress) | OneWireContainer27 | |
| readDevice() | OneWireContainer24 | |
| setClock(long time, byte[] state) | OneWireContainer24 | |
| setClockAlarm(long time, byte[] state) | OneWireContainer24 | |
| setClockAlarmEnable(boolean alarmEnable, byte[] state) | OneWireContainer24 | |
| setClockRunEnable(boolean runEnable, byte[] state) | OneWireContainer24 | |
| setInterruptEnable(boolean iEnable, byte[] state) | OneWireContainer27 | |
| setInterruptInterval(byte intervalValue, byte[] state) | OneWireContainer27 | |
| setSpeed(int newSpeed, boolean fallBack) | OneWireContainer | |
| setupContainer(DSPortAdapter sourceAdapter, byte[] newAddress) | OneWireContainer | |
| setupContainer(DSPortAdapter sourceAdapter, long newAddress) | OneWireContainer | |
| setupContainer(DSPortAdapter sourceAdapter, String newAddress) | OneWireContainer | |
| speed | OneWireContainer | [protected] |
| speedFallBackOK | OneWireContainer | [protected] |
| toString() | OneWireContainer | |
| writeDevice(byte[] state) | OneWireContainer24 | |