|
1-Wire API for .NET Version 4.00
|
Inherits com::dalsemi::onewire::container::OneWireContainer, and com::dalsemi::onewire::container::ClockContainer.
Inherited by OneWireContainer27.
Public Member Functions | |
| OneWireContainer24 () | |
Create an empty container that is not complete until after a call to setupContainer. | |
| OneWireContainer24 (DSPortAdapter sourceAdapter, byte[] newAddress) | |
| Create a container with the provided adapter instance and the address of the iButton or 1-Wire device. | |
| OneWireContainer24 (DSPortAdapter sourceAdapter, long newAddress) | |
| Create a container with the provided adapter instance and the address of the iButton or 1-Wire device. | |
| OneWireContainer24 (DSPortAdapter sourceAdapter, String newAddress) | |
| Create a container with the provided adapter instance and the address of the iButton or 1-Wire device. | |
| String | getName () |
| Get the Maxim Integrated Products part number of the iButton or 1-Wire Device as a string. | |
| String | getAlternateNames () |
| Get the alternate Maxim Integrated Products part numbers or names. | |
| String | getDescription () |
| Get a short description of the function of this iButton or 1-Wire Device type. | |
| boolean | hasClockAlarm () |
| Query to see if the clock has an alarm feature. | |
| boolean | canDisableClock () |
| Query to see if the clock can be disabled. | |
| long | getClockResolution () |
| Query to get the clock resolution in milliseconds. | |
| byte[] | readDevice () throws OneWireIOException, OneWireException |
| Retrieves the five byte state over the 1-Wire bus. | |
| void | writeDevice (byte[] state) throws OneWireIOException, OneWireException |
| Writes the 1-Wire device sensor state that have been changed by 'set' methods. | |
| long | getClock (byte[] state) |
| Extracts the Real-Time clock value in milliseconds. | |
| long | getClockAlarm (byte[] state) throws OneWireException |
| Extracts the clock alarm value for the Real-Time clock. | |
| boolean | isClockAlarming (byte[] state) |
| Checks if the clock alarm flag has been set. | |
| boolean | isClockAlarmEnabled (byte[] state) |
| Checks if the clock alarm is enabled. | |
| boolean | isClockRunning (byte[] state) |
| Checks if the device's oscillator is enabled. | |
| void | setClock (long time, byte[] state) |
| Sets the Real-Time clock. | |
| void | setClockAlarm (long time, byte[] state) throws OneWireException |
| Sets the clock alarm. | |
| void | setClockAlarmEnable (boolean alarmEnable, byte[] state) throws OneWireException |
| Enables or disables the clock alarm. | |
| void | setClockRunEnable (boolean runEnable, byte[] state) |
| Enables or disables the oscillator, turning the clock 'on' and 'off'. | |
1-Wire container for Real-Time-Clock (RTC) iButton, DS1904 and 1-Wire Chip, DS2415. This container encapsulates the functionality of the iButton family type 24 (hex)
This iButton is used as a portable real-time-clock.
The clock methods can be organized into the following categories. Note that methods that are implemented for the ClockContainer interface are marked with (*):
See the usage examples in ClockContainer for basic clock operations.
http://pdfserv.maxim-ic.com/arpdf/DS1904.pdf http://pdfserv.maxim-ic.com/arpdf/DS2415.pdf
Create an empty container that is not complete until after a call to setupContainer.
This is one of the methods to construct a container. The others are through creating a OneWireContainer with parameters.
| OneWireContainer24 | ( | DSPortAdapter | sourceAdapter, |
| byte[] | newAddress | ||
| ) |
Create a container with the provided adapter instance and the address of the iButton or 1-Wire device.
This is one of the methods to construct a container. The other is through creating a OneWireContainer with NO parameters.
| sourceAdapter | adapter instance used to communicate with this iButton |
| newAddress | Address of this 1-Wire device |
| OneWireContainer24 | ( | DSPortAdapter | sourceAdapter, |
| long | newAddress | ||
| ) |
Create a container with the provided adapter instance and the address of the iButton or 1-Wire device.
This is one of the methods to construct a container. The other is through creating a OneWireContainer with NO parameters.
| sourceAdapter | adapter instance used to communicate with this 1-Wire device |
| newAddress | Address of this 1-Wire device |
| OneWireContainer24 | ( | DSPortAdapter | sourceAdapter, |
| String | newAddress | ||
| ) |
Create a container with the provided adapter instance and the address of the iButton or 1-Wire device.
This is one of the methods to construct a container. The other is through creating a OneWireContainer with NO parameters.
| sourceAdapter | adapter instance used to communicate with this 1-Wire device |
| newAddress | Address of this 1-Wire device |
| boolean canDisableClock | ( | ) |
Query to see if the clock can be disabled.
Implements ClockContainer.
| String getAlternateNames | ( | ) |
Get the alternate Maxim Integrated Products part numbers or names.
A 'family' of 1-Wire Network devices may have more than one part number depending on packaging. There can also be nicknames such as 'Crypto iButton'.
Reimplemented from OneWireContainer.
Reimplemented in OneWireContainer27.
| long getClock | ( | byte[] | state | ) |
Extracts the Real-Time clock value in milliseconds.
| state | current state of the device returned from readDevice() |
Implements ClockContainer.
| long getClockAlarm | ( | byte[] | state | ) | throws OneWireException |
Extracts the clock alarm value for the Real-Time clock.
| state | current state of the device returned from readDevice() |
| OneWireException | if this device does not have clock alarms |
Implements ClockContainer.
| long getClockResolution | ( | ) |
Query to get the clock resolution in milliseconds.
Implements ClockContainer.
| String getDescription | ( | ) |
Get a short description of the function of this iButton or 1-Wire Device type.
Reimplemented from OneWireContainer.
Reimplemented in OneWireContainer27.
| String getName | ( | ) |
Get the Maxim Integrated Products part number of the iButton or 1-Wire Device as a string.
For example 'DS1992'.
Reimplemented from OneWireContainer.
Reimplemented in OneWireContainer27.
| boolean hasClockAlarm | ( | ) |
Query to see if the clock has an alarm feature.
Implements ClockContainer.
| boolean isClockAlarmEnabled | ( | byte[] | state | ) |
Checks if the clock alarm is enabled.
| state | current state of the device returned from readDevice() |
Implements ClockContainer.
| boolean isClockAlarming | ( | byte[] | state | ) |
Checks if the clock alarm flag has been set.
This will occur when the value of the Real-Time clock equals the value of the clock alarm.
| state | current state of the device returned from readDevice() |
Implements ClockContainer.
| boolean isClockRunning | ( | byte[] | state | ) |
Checks if the device's oscillator is enabled.
The clock will not increment if the clock oscillator is not enabled.
| state | current state of the device returned from readDevice() |
Implements ClockContainer.
| byte [] readDevice | ( | ) | throws OneWireIOException, OneWireException |
Retrieves the five byte state over the 1-Wire bus.
This state array must be passed to the Get/Set methods as well as the WriteDevice method.
| OneWireIOException | on a 1-Wire communication error such as reading an incorrect CRC from a 1-Wire device. This could be caused by a physical interruption in the 1-Wire Network due to shorts or a newly arriving 1-Wire device issuing a 'presence pulse'. |
| OneWireException | on a communication or setup error with the 1-Wire adapter |
Implements OneWireSensor.
| void setClock | ( | long | time, |
| byte[] | state | ||
| ) |
Sets the Real-Time clock.
The method writeDevice(byte[]) must be called to finalize changes to the device. Note that multiple 'set' methods can be called before one call to writeDevice(byte[]).
| time | new value for the Real-Time clock, in milliseconds since some reference time (ie. 12:00am, January 1st, 1970) |
| state | current state of the device returned from readDevice() |
Implements ClockContainer.
| void setClockAlarm | ( | long | time, |
| byte[] | state | ||
| ) | throws OneWireException |
Sets the clock alarm.
The method writeDevice(byte[]) must be called to finalize changes to the device. Note that multiple 'set' methods can be called before one call to writeDevice(byte[]). Also note that not all clock devices have alarms. Check to see if this device has alarms first by calling the hasClockAlarm() method.
| time | - new value for the Real-Time clock alarm, in milliseconds since January 1, 1970 |
| state | current state of the device returned from readDevice() |
| OneWireException | if this device does not have clock alarms |
Implements ClockContainer.
| void setClockAlarmEnable | ( | boolean | alarmEnable, |
| byte[] | state | ||
| ) | throws OneWireException |
Enables or disables the clock alarm.
The method writeDevice(byte[]) must be called to finalize changes to the device. Note that multiple 'set' methods can be called before one call to writeDevice(byte[]). Also note that not all clock devices have alarms. Check to see if this device has alarms first by calling the hasClockAlarm() method.
| alarmEnable | true to enable the clock alarm |
| state | current state of the device returned from readDevice() |
| OneWireException | if this device does not have clock alarms |
Implements ClockContainer.
| void setClockRunEnable | ( | boolean | runEnable, |
| byte[] | state | ||
| ) |
Enables or disables the oscillator, turning the clock 'on' and 'off'.
The method writeDevice(byte[]) must be called to finalize changes to the device. Note that multiple 'set' methods can be called before one call to writeDevice(byte[]). Also note that not all clock devices can disable their oscillators. Check to see if this device can disable its oscillator first by calling the canDisableClock() method.
| runEnable | true to enable the clock oscillator |
| state | current state of the device returned from readDevice() |
Implements ClockContainer.
| void writeDevice | ( | byte[] | state | ) | throws OneWireIOException, OneWireException |
Writes the 1-Wire device sensor state that have been changed by 'set' methods.
Only the state registers that changed are updated. This is done by referencing a field information appended to the state data.
| state | 1-Wire device sensor state |
| OneWireIOException | on a 1-Wire communication error such as reading an incorrect CRC from a 1-Wire device. This could be caused by a physical interruption in the 1-Wire Network due to shorts or a newly arriving 1-Wire device issuing a 'presence pulse'. |
| OneWireException | on a communication or setup error with the 1-Wire adapter |
Implements OneWireSensor.
1.7.3