|
1-Wire API for .NET Version 4.00
|
Inherits com::dalsemi::onewire::container::OneWireContainer, and com::dalsemi::onewire::container::ADContainer.
Public Member Functions | |
| OneWireContainer20 () | |
| Default constructor. | |
| OneWireContainer20 (DSPortAdapter sourceAdapter, byte[] newAddress) | |
| Creates a container with a provided adapter object and the address of the 1-Wire device. | |
| OneWireContainer20 (DSPortAdapter sourceAdapter, long newAddress) | |
| Creates a container with a provided adapter object and the address of the 1-Wire device. | |
| OneWireContainer20 (DSPortAdapter sourceAdapter, String newAddress) | |
| Creates a container with a provided adapter object and the address of the 1-Wire device. | |
| String | getName () |
| Gets the name of this 1-Wire device. | |
| String | getAlternateNames () |
| Gets any other possible names for this 1-Wire device. | |
| String | getDescription () |
| Gets a brief description of the functionality of this 1-Wire device. | |
| int | getMaxSpeed () |
| Gets the maximum speed this 1-Wire device can communicate at. | |
| Enumeration | getMemoryBanks () |
| Gets an enumeration of memory banks. | |
| int | getNumberADChannels () |
| Queries to get the number of channels supported by this A/D. | |
| boolean | hasADAlarms () |
| Queries to see if this A/D measuring device has high/low alarms. | |
| double[] | getADRanges (int channel) |
| Queries to get an array of available ranges for the specified A/D channel. | |
| double[] | getADResolutions (int channel, double range) |
| Queries to get an array of available resolutions based on the specified range on the specified A/D channel. | |
| boolean | canADMultiChannelRead () |
| Queries to see if this A/D supports doing multiple voltage conversions at the same time. | |
| byte[] | readDevice () throws OneWireIOException, OneWireException |
| Retrieves the entire A/D control/status and alarm pages. | |
| void | writeDevice (byte[] state) throws OneWireIOException, OneWireException |
| Writes the bytes in the provided A/D register pages that have been changed by the 'set' methods. | |
| double[] | getADVoltage (byte[] state) throws OneWireIOException, OneWireException |
| Reads the voltage values. | |
| double | getADVoltage (int channel, byte[] state) throws OneWireIOException, OneWireException |
| Reads a channels voltage value. | |
| void | doADConvert (int channel, byte[] state) throws OneWireIOException, OneWireException |
| Performs voltage conversion on specified channel. | |
| void | doADConvert (boolean[] doConvert, byte[] state) throws OneWireIOException, OneWireException |
| Performs voltage conversion on all specified channels. | |
| void | doADConvert (int channel, int preset, byte[] state) throws OneWireIOException, OneWireException, IllegalArgumentException |
| Performs voltage conversion on specified channel. | |
| void | doADConvert (boolean[] doConvert, int[] preset, byte[] state) throws OneWireIOException, OneWireException |
| Performs voltage conversion on all specified channels. | |
| double | getADAlarm (int channel, int alarmType, byte[] state) |
| Extracts the alarm voltage value of the specified channel from the provided state buffer. | |
| boolean | getADAlarmEnable (int channel, int alarmType, byte[] state) |
| Extracts the alarm enable value of the specified channel from the provided state buffer. | |
| boolean | hasADAlarmed (int channel, int alarmType, byte[] state) |
| Checks the alarm event value of the specified channel from the provided state buffer. | |
| double | getADResolution (int channel, byte[] state) |
| Extracts the conversion resolution of the specified channel from the provided state buffer expressed in volts. | |
| double | getADRange (int channel, byte[] state) |
| Extracts the input voltage range of the specified channel from the provided state buffer. | |
| boolean | isOutputEnabled (int channel, byte[] state) throws IllegalArgumentException |
| Detects if the output is enabled for the specified channel from the provided register buffer. | |
| boolean | getOutputState (int channel, byte[] state) throws IllegalArgumentException |
| Detects if the output is enabled for the specified channel from the provided register buffer. | |
| boolean | getDevicePOR (byte[] state) |
| Detects if this device has seen a Power-On-Reset (POR). | |
| boolean | isPowerExternal (byte[] state) |
| Extracts the state of the external power indicator from the provided register buffer. | |
| void | setADAlarm (int channel, int alarmType, double alarm, byte[] state) |
| Sets the alarm voltage value of the specified channel in the provided state buffer. | |
| void | setADAlarmEnable (int channel, int alarmType, boolean alarmEnable, byte[] state) |
| Sets the alarm enable value of the specified channel in the provided state buffer. | |
| void | setADResolution (int channel, double resolution, byte[] state) |
| Sets the conversion resolution value for the specified channel in the provided state buffer. | |
| void | setADRange (int channel, double range, byte[] state) |
| Sets the input range for the specified channel in the provided state buffer. | |
| void | setOutput (int channel, boolean outputEnable, boolean outputState, byte[] state) |
| Sets the output enable and state for the specified channel in the provided register buffer. | |
| void | setPower (boolean external, byte[] state) |
| Sets or clears the external power flag in the provided register buffer. | |
Static Public Member Functions | |
| static double | interpretVoltage (long rawVoltage, double range) |
| Converts a raw voltage long value for the DS2450 into a valid voltage. | |
| static int | voltageToInt (double voltage, double range) |
| Converts a voltage double value to the DS2450 specific int value. | |
Static Public Attributes | |
| static final int | BITMAP_OFFSET = 24 |
| Offset of BITMAP in array returned from read state. | |
| static final int | ALARM_OFFSET = 8 |
| Offset of ALARMS in array returned from read state. | |
| static final int | EXPOWER_OFFSET = 20 |
| Offset of external power offset in array returned from read state. | |
| static final int | CHANNELA = 0 |
| Channel A number. | |
| static final int | CHANNELB = 1 |
| Channel B number. | |
| static final int | CHANNELC = 2 |
| Channel C number. | |
| static final int | CHANNELD = 3 |
| Channel D number. | |
| static final int | NO_PRESET = 0 |
| No preset value. | |
| static final int | PRESET_TO_ZEROS = 1 |
| Preset value to zeros. | |
| static final int | PRESET_TO_ONES = 2 |
| Preset value to ones. | |
| static final int | NUM_CHANNELS = 4 |
| Number of channels. | |
1-Wire® container that encapsulates the functionality of the 1-Wire family type 20 (hex), Maxim Integrated Products part number: DS2450, 1-Wire Quad A/D Converter.
Example device setup
byte[] state = owd.readDevice();
owd.setResolution(OneWireContainer20.CHANNELA, 16, state);
owd.setResolution(OneWireContainer20.CHANNELB, 8, state);
owd.setRange(OneWireContainer20.CHANNELA, 5.12, state);
owd.setRange(OneWireContainer20.CHANNELB, 2.56, state);
owd.writeDevice();
Example device read
owd.doADConvert(OneWireContainer20.CHANNELA, state);
owd.doADConvert(OneWireContainer20.CHANNELB, state);
double chAVolatge = owd.getADVoltage(OneWireContainer20.CHANNELA, state);
double chBVoltage = owd.getADVoltage(OneWireContainer20.CHANNELB, state);
When converting analog voltages to digital, the user of the device must gaurantee that the voltage seen by the channel of the quad A/D does not exceed the selected input range of the device. If this happens, the device will default to reading 0 volts. There is NO way to know if the device is reading a higher than specified voltage or NO voltage.
http://pdfserv.maxim-ic.com/arpdf/DS2450.pdf
| OneWireContainer20 | ( | DSPortAdapter | sourceAdapter, |
| byte[] | newAddress | ||
| ) |
Creates a container with a provided adapter object and the address of the 1-Wire device.
| sourceAdapter | adapter required to communicate with this device |
| newAddress | address of this 1-Wire device |
| OneWireContainer20 | ( | DSPortAdapter | sourceAdapter, |
| long | newAddress | ||
| ) |
Creates a container with a provided adapter object and the address of the 1-Wire device.
| sourceAdapter | adapter required to communicate with this device |
| newAddress | address of this 1-Wire device |
| OneWireContainer20 | ( | DSPortAdapter | sourceAdapter, |
| String | newAddress | ||
| ) |
Creates a container with a provided adapter object and the address of the 1-Wire device.
| sourceAdapter | adapter required to communicate with this device |
| newAddress | address of this 1-Wire device |
| boolean canADMultiChannelRead | ( | ) |
Queries to see if this A/D supports doing multiple voltage conversions at the same time.
true if can do multi-channel voltage reads Implements ADContainer.
| void doADConvert | ( | boolean[] | doConvert, |
| byte[] | state | ||
| ) | throws OneWireIOException, OneWireException |
Performs voltage conversion on all specified channels.
The method getADVoltage() can be used to read the result of the conversion. This A/D must support multi-channel read canMultiChannelRead() if there are more then 1 channel is specified.
| doConvert | which channels to perform conversion on. |
| state | current state of this device returned from readDevice() |
| OneWireIOException | Data was not written correctly |
| OneWireException | Could not find part |
Implements ADContainer.
| void doADConvert | ( | int | channel, |
| int | preset, | ||
| byte[] | state | ||
| ) | throws OneWireIOException, OneWireException, IllegalArgumentException |
Performs voltage conversion on specified channel.
The method getADVoltage() can be used to read the result of the conversion.
| channel | 0,1,2,3 representing the channels A,B,C,D |
| preset | preset value: NO_PRESET (0), PRESET_TO_ZEROS (1), and PRESET_TO_ONES (2) |
| state | state of this device returned from readDevice() |
| OneWireIOException | Data could not be written correctly |
| OneWireException | Could not find part |
| IllegalArgumentException | Invalid channel number passed |
| void doADConvert | ( | boolean[] | doConvert, |
| int[] | preset, | ||
| byte[] | state | ||
| ) | throws OneWireIOException, OneWireException |
Performs voltage conversion on all specified channels.
The method getADVoltage() can be used to read the result of the conversion.
| doConvert | which channels to perform conversion on |
| preset | preset values NO_PRESET (0), PRESET_TO_ZEROS (1), and PRESET_TO_ONES (2) |
| state | current state of this device returned from readDevice() |
| OneWireIOException | Data could not be written correctly |
| OneWireException | Could not find part |
| void doADConvert | ( | int | channel, |
| byte[] | state | ||
| ) | throws OneWireIOException, OneWireException |
Performs voltage conversion on specified channel.
The method getADVoltage() can be used to read the result of the conversion.
| channel | channel in the range [0 to (getNumberChannels() - 1)] |
| state | current state of this device returned from readDevice() |
| OneWireIOException | Data was not written correctly |
| OneWireException | Could not find part |
Implements ADContainer.
| double getADAlarm | ( | int | channel, |
| int | alarmType, | ||
| byte[] | state | ||
| ) |
Extracts the alarm voltage value of the specified channel from the provided state buffer.
The state buffer is retrieved from the readDevice() method.
| channel | channel in the range [0 to (getNumberChannels() - 1)] |
| alarmType | desired alarm, ALARM_HIGH (1) or ALARM_LOW (0) |
| state | current state of this device returned from readDevice() |
| IllegalArgumentException | Invalid channel number passed |
Implements ADContainer.
| boolean getADAlarmEnable | ( | int | channel, |
| int | alarmType, | ||
| byte[] | state | ||
| ) |
Extracts the alarm enable value of the specified channel from the provided state buffer.
The state buffer is retrieved from the readDevice() method.
| channel | channel in the range [0 to (getNumberChannels() - 1)] |
| alarmType | desired alarm, ALARM_HIGH (1) or ALARM_LOW (0) |
| state | current state of the state returned from readDevice() |
true if specified alarm is enabled| IllegalArgumentException | Invalid channel number passed |
Implements ADContainer.
| double getADRange | ( | int | channel, |
| byte[] | state | ||
| ) |
Extracts the input voltage range of the specified channel from the provided state buffer.
The state buffer is retrieved from the readDevice() method.
| channel | channel in the range [0 to (getNumberChannels() - 1)] |
| state | current state of the state returned from readDevice() |
| IllegalArgumentException | Invalid channel number passed |
Implements ADContainer.
| double [] getADRanges | ( | int | channel | ) |
Queries to get an array of available ranges for the specified A/D channel.
| channel | channel in the range [0 to (getNumberChannels() - 1)] |
Implements ADContainer.
| double getADResolution | ( | int | channel, |
| byte[] | state | ||
| ) |
Extracts the conversion resolution of the specified channel from the provided state buffer expressed in volts.
The state is retrieved from the readDevice() method.
| channel | channel in the range [0 to (getNumberChannels() - 1)] |
| state | current state of the state returned from readDevice() |
| IllegalArgumentException | Invalid channel number passed |
Implements ADContainer.
| double [] getADResolutions | ( | int | channel, |
| double | range | ||
| ) |
Queries to get an array of available resolutions based on the specified range on the specified A/D channel.
| channel | channel in the range [0 to (getNumberChannels() - 1)] |
| range | specified range |
Implements ADContainer.
| double [] getADVoltage | ( | byte[] | state | ) | throws OneWireIOException, OneWireException |
Reads the voltage values.
Must be used after a doADConvert() method call. Also must include the last valid state from the readDevice() method and this A/D must support multi-channel read canMultiChannelRead() if there are more then 1 channel.
| state | current state of this device returned from readDevice() |
| OneWireIOException | Data was not read correctly |
| OneWireException | Could not find part |
Implements ADContainer.
| double getADVoltage | ( | int | channel, |
| byte[] | state | ||
| ) | throws OneWireIOException, OneWireException |
Reads a channels voltage value.
Must be used after a doADConvert() method call. Also must include the last valid state from the readDevice() method. Note, if more then one channel is to be read then it is more efficient to use the getADVoltage(byte[]) method that returns all channel values.
| channel | channel in the range [0 to (getNumberChannels() - 1)] |
| state | current state of this device returned from readDevice() |
| OneWireIOException | Data was not read correctly |
| OneWireException | Could not find part |
| IllegalArgumentException | Invalid channel number passed |
Implements ADContainer.
| String getAlternateNames | ( | ) |
Gets any other possible names for this 1-Wire device.
Reimplemented from OneWireContainer.
| String getDescription | ( | ) |
Gets a brief description of the functionality of this 1-Wire device.
Reimplemented from OneWireContainer.
| boolean getDevicePOR | ( | byte[] | state | ) |
Detects if this device has seen a Power-On-Reset (POR).
If this has occured it may be necessary to set the state of the device to the desired values. The register buffer is retrieved from the readDevice() method.
| state | current state of the device returned from readDevice() |
false if output is conducting to ground and true if not conducting | int getMaxSpeed | ( | ) |
Gets the maximum speed this 1-Wire device can communicate at.
Reimplemented from OneWireContainer.
| Enumeration getMemoryBanks | ( | ) |
Gets an enumeration of memory banks.
Reimplemented from OneWireContainer.
| String getName | ( | ) |
Gets the name of this 1-Wire device.
Reimplemented from OneWireContainer.
| int getNumberADChannels | ( | ) |
Queries to get the number of channels supported by this A/D.
Channel specific methods will use a channel number specified by an integer from [0 to (getNumberChannels() - 1)].
Implements ADContainer.
| boolean getOutputState | ( | int | channel, |
| byte[] | state | ||
| ) | throws IllegalArgumentException |
Detects if the output is enabled for the specified channel from the provided register buffer.
The register buffer is retrieved from the readDevice() method.
| channel | channel in the range [0 to (getNumberChannels() - 1)] |
| state | current state of the device returned from readDevice() |
false if output is conducting to ground and true if not conducting| IllegalArgumentException | Invalid channel number passed |
| boolean hasADAlarmed | ( | int | channel, |
| int | alarmType, | ||
| byte[] | state | ||
| ) |
Checks the alarm event value of the specified channel from the provided state buffer.
The state buffer is retrieved from the readDevice() method.
| channel | channel in the range [0 to (getNumberChannels() - 1)] |
| alarmType | desired alarm, ALARM_HIGH (1) or ALARM_LOW (0) |
| state | current state of the state returned from readDevice() |
true if specified alarm occurred| IllegalArgumentException | Invalid channel number passed |
Implements ADContainer.
| boolean hasADAlarms | ( | ) |
Queries to see if this A/D measuring device has high/low alarms.
true if it has high/low trips Implements ADContainer.
| static double interpretVoltage | ( | long | rawVoltage, |
| double | range | ||
| ) | [static] |
Converts a raw voltage long value for the DS2450 into a valid voltage.
Requires the max voltage value.
| rawVoltage | raw voltage |
| range | max voltage |
| boolean isOutputEnabled | ( | int | channel, |
| byte[] | state | ||
| ) | throws IllegalArgumentException |
Detects if the output is enabled for the specified channel from the provided register buffer.
The register buffer is retrieved from the readDevice() method.
| channel | channel in the range [0 to (getNumberChannels() - 1)] |
| state | current state of the device returned from readDevice() |
true if output is enabled on specified channel| IllegalArgumentException | Invalid channel number passed |
| boolean isPowerExternal | ( | byte[] | state | ) |
Extracts the state of the external power indicator from the provided register buffer.
Use 'setPower' to set or clear the external power indicator flag. The register buffer is retrieved from the readDevice() method.
| state | current state of the device returned from readDevice() |
true if set to external power operation | byte [] readDevice | ( | ) | throws OneWireIOException, OneWireException |
Retrieves the entire A/D control/status and alarm pages.
It reads this and verifies the data with the onboard CRC generator. Use the byte array returned from this method with static utility methods to extract the status, alarm and other register values. Appended to the data is 2 bytes that represent a bitmap of changed bytes. These bytes are used in the writeADRegisters() in conjuction with the 'set' methods to only write back the changed register bytes.
| OneWireIOException | Data was not read correctly |
| OneWireException | Could not find part |
Implements OneWireSensor.
| void setADAlarm | ( | int | channel, |
| int | alarmType, | ||
| double | alarm, | ||
| byte[] | state | ||
| ) |
Sets the alarm voltage value of the specified channel in the provided state buffer.
The state buffer is retrieved from the readDevice() method. The method writeDevice() must be called to finalize these changes to the device. Note that multiple 'set' methods can be called before one call to writeDevice().
| channel | channel in the range [0 to (getNumberChannels() - 1)] |
| alarmType | desired alarm, ALARM_HIGH (1) or ALARM_LOW (0) |
| alarm | alarm value (will be reduced to 8 bit resolution) |
| state | current state of this device returned from readDevice() |
| IllegalArgumentException | Invalid channel number passed |
Implements ADContainer.
| void setADAlarmEnable | ( | int | channel, |
| int | alarmType, | ||
| boolean | alarmEnable, | ||
| byte[] | state | ||
| ) |
Sets the alarm enable value of the specified channel in the provided state buffer.
The state buffer is retrieved from the readDevice() method. The method writeDevice() must be called to finalize these changes to the device. Note that multiple 'set' methods can be called before one call to writeDevice().
| channel | channel in the range [0 to (getNumberChannels() - 1)] |
| alarmType | desired alarm, ALARM_HIGH (1) or ALARM_LOW (0) |
| alarmEnable | alarm enable value |
| state | current state of this device returned from readDevice() |
| IllegalArgumentException | Invalid channel number passed |
Implements ADContainer.
| void setADRange | ( | int | channel, |
| double | range, | ||
| byte[] | state | ||
| ) |
Sets the input range for the specified channel in the provided state buffer.
The state buffer is retrieved from the readDevice() method. The method writeDevice() must be called to finalize these changes to the device. Note that multiple 'set' methods can be called before one call to writeDevice().
| channel | channel in the range [0 to (getNumberChannels() - 1)] |
| range | max volt range, use getRanges() method to get available ranges |
| state | current state of this device returned from readDevice() |
| IllegalArgumentException | Invalid channel number passed |
Implements ADContainer.
| void setADResolution | ( | int | channel, |
| double | resolution, | ||
| byte[] | state | ||
| ) |
Sets the conversion resolution value for the specified channel in the provided state buffer.
The state buffer is retrieved from the readDevice() method. The method writeDevice() must be called to finalize these changes to the device. Note that multiple 'set' methods can be called before one call to writeDevice().
| channel | channel in the range [0 to (getNumberChannels() - 1)] |
| resolution | resolution to use in volts |
| state | current state of this device returned from readDevice() |
| IllegalArgumentException | Invalid channel number passed |
Implements ADContainer.
| void setOutput | ( | int | channel, |
| boolean | outputEnable, | ||
| boolean | outputState, | ||
| byte[] | state | ||
| ) |
Sets the output enable and state for the specified channel in the provided register buffer.
The register buffer is retrieved from the readDevice() method. The method writeDevice() must be called to finalize these changes to the device. Note that multiple 'set' methods can be called before one call to writeDevice().
| channel | channel in the range [0 to (getNumberChannels() - 1)] |
| outputEnable | true if output is enabled |
| outputState | false if output is conducting to ground and true if not conducting. This parameter is not used if outputEnable is false |
| state | current state of the device returned from readDevice() |
| void setPower | ( | boolean | external, |
| byte[] | state | ||
| ) |
Sets or clears the external power flag in the provided register buffer.
The register buffer is retrieved from the readDevice() method. The method writeDevice() must be called to finalize these changes to the device. Note that multiple 'set' methods can be called before one call to writeDevice().
| external | true if setting external power is used |
| state | current state of this device returned from readDevice() |
| static int voltageToInt | ( | double | voltage, |
| double | range | ||
| ) | [static] |
Converts a voltage double value to the DS2450 specific int value.
Requires the max voltage value.
| voltage | voltage |
| range | max voltage |
| void writeDevice | ( | byte[] | state | ) | throws OneWireIOException, OneWireException |
Writes the bytes in the provided A/D register pages that have been changed by the 'set' methods.
It knows which state has changed by looking at the bitmap fields appended to the register data. Any alarm flags will be automatically cleared. Only VCC powered indicator byte in physical location 0x1C can be written in the calibration memory bank.
| state | register pages |
| OneWireIOException | Data was not written correctly |
| OneWireException | Could not find part |
Implements OneWireSensor.
1.7.3