, including all inherited members.
| adapter | OneWireContainer | [protected] |
| address | OneWireContainer | [protected] |
| ALARM_HIGH | ADContainer | [static] |
| ALARM_LOW | ADContainer | [static] |
| ALARM_OFFSET | OneWireContainer20 | [static] |
| BITMAP_OFFSET | OneWireContainer20 | [static] |
| canADMultiChannelRead() | OneWireContainer20 | |
| CHANNELA | OneWireContainer20 | [static] |
| CHANNELB | OneWireContainer20 | [static] |
| CHANNELC | OneWireContainer20 | [static] |
| CHANNELD | OneWireContainer20 | [static] |
| doADConvert(int channel, byte[] state) | OneWireContainer20 | |
| doADConvert(boolean[] doConvert, byte[] state) | OneWireContainer20 | |
| doADConvert(int channel, int preset, byte[] state) | OneWireContainer20 | |
| doADConvert(boolean[] doConvert, int[] preset, byte[] state) | OneWireContainer20 | |
| doSpeed() | OneWireContainer | |
| equals(Object obj) | OneWireContainer | |
| EXPOWER_OFFSET | OneWireContainer20 | [static] |
| getADAlarm(int channel, int alarmType, byte[] state) | OneWireContainer20 | |
| getADAlarmEnable(int channel, int alarmType, byte[] state) | OneWireContainer20 | |
| getAdapter() | OneWireContainer | |
| getAddress() | OneWireContainer | |
| getAddressAsLong() | OneWireContainer | |
| getAddressAsString() | OneWireContainer | |
| getADRange(int channel, byte[] state) | OneWireContainer20 | |
| getADRanges(int channel) | OneWireContainer20 | |
| getADResolution(int channel, byte[] state) | OneWireContainer20 | |
| getADResolutions(int channel, double range) | OneWireContainer20 | |
| getADVoltage(byte[] state) | OneWireContainer20 | |
| getADVoltage(int channel, byte[] state) | OneWireContainer20 | |
| getAlternateNames() | OneWireContainer20 | |
| getDescription() | OneWireContainer20 | |
| getDevicePOR(byte[] state) | OneWireContainer20 | |
| getMaxSpeed() | OneWireContainer20 | |
| getMemoryBanks() | OneWireContainer20 | |
| getName() | OneWireContainer20 | |
| getNumberADChannels() | OneWireContainer20 | |
| getOutputState(int channel, byte[] state) | OneWireContainer20 | |
| hasADAlarmed(int channel, int alarmType, byte[] state) | OneWireContainer20 | |
| hasADAlarms() | OneWireContainer20 | |
| hashCode() | OneWireContainer | |
| interpretVoltage(long rawVoltage, double range) | OneWireContainer20 | [static] |
| isAlarming() | OneWireContainer | |
| isOutputEnabled(int channel, byte[] state) | OneWireContainer20 | |
| isPowerExternal(byte[] state) | OneWireContainer20 | |
| isPresent() | OneWireContainer | |
| NO_PRESET | OneWireContainer20 | [static] |
| NUM_CHANNELS | OneWireContainer20 | [static] |
| OneWireContainer() | OneWireContainer | |
| OneWireContainer(DSPortAdapter sourceAdapter, byte[] newAddress) | OneWireContainer | |
| OneWireContainer(DSPortAdapter sourceAdapter, long newAddress) | OneWireContainer | |
| OneWireContainer(DSPortAdapter sourceAdapter, String newAddress) | OneWireContainer | |
| OneWireContainer20() | OneWireContainer20 | |
| OneWireContainer20(DSPortAdapter sourceAdapter, byte[] newAddress) | OneWireContainer20 | |
| OneWireContainer20(DSPortAdapter sourceAdapter, long newAddress) | OneWireContainer20 | |
| OneWireContainer20(DSPortAdapter sourceAdapter, String newAddress) | OneWireContainer20 | |
| PRESET_TO_ONES | OneWireContainer20 | [static] |
| PRESET_TO_ZEROS | OneWireContainer20 | [static] |
| readDevice() | OneWireContainer20 | |
| setADAlarm(int channel, int alarmType, double alarm, byte[] state) | OneWireContainer20 | |
| setADAlarmEnable(int channel, int alarmType, boolean alarmEnable, byte[] state) | OneWireContainer20 | |
| setADRange(int channel, double range, byte[] state) | OneWireContainer20 | |
| setADResolution(int channel, double resolution, byte[] state) | OneWireContainer20 | |
| setOutput(int channel, boolean outputEnable, boolean outputState, byte[] state) | OneWireContainer20 | |
| setPower(boolean external, byte[] state) | OneWireContainer20 | |
| setSpeed(int newSpeed, boolean fallBack) | OneWireContainer | |
| setupContainer(DSPortAdapter sourceAdapter, byte[] newAddress) | OneWireContainer | |
| setupContainer(DSPortAdapter sourceAdapter, long newAddress) | OneWireContainer | |
| setupContainer(DSPortAdapter sourceAdapter, String newAddress) | OneWireContainer | |
| speed | OneWireContainer | [protected] |
| speedFallBackOK | OneWireContainer | [protected] |
| toString() | OneWireContainer | |
| voltageToInt(double voltage, double range) | OneWireContainer20 | [static] |
| writeDevice(byte[] state) | OneWireContainer20 | |