|
1-Wire API for .NET Version 4.00
|
Inherits com::dalsemi::onewire::container::OneWireContainer.
Public Member Functions | |
| OneWireContainer1D () | |
Create an empty container that is not complete until after a call to setupContainer. | |
| OneWireContainer1D (DSPortAdapter sourceAdapter, byte[] newAddress) | |
| Create a container with the provided adapter instance and the address of the iButton or 1-Wire device. | |
| OneWireContainer1D (DSPortAdapter sourceAdapter, long newAddress) | |
| Create a container with the provided adapter instance and the address of the iButton or 1-Wire device. | |
| OneWireContainer1D (DSPortAdapter sourceAdapter, String newAddress) | |
| Create a container with the provided adapter instance and the address of the iButton or 1-Wire device. | |
| String | getName () |
| Get the Maxim Integrated Products part number of the iButton or 1-Wire Device as a string. | |
| String | getDescription () |
| Get a short description of the function of this iButton or 1-Wire Device type. | |
| int | getMaxSpeed () |
| Get the maximum speed this iButton or 1-Wire device can communicate at. | |
| Enumeration | getMemoryBanks () |
| Get an enumeration of memory bank instances that implement one or more of the following interfaces: MemoryBank, PagedMemoryBank, and OTPMemoryBank. | |
| long | readCounter (int counterPage) throws OneWireIOException, OneWireException |
| Read the counter value associated with a page on this 1-Wire Device. | |
1-Wire container for 512 byte memory with external counters, DS2423. This container encapsulates the functionality of the 1-Wire family type 1D (hex)
This 1-Wire device is primarily used as a counter with memory.
Each counter is assosciated with a memory page. The counters for pages 12 and 13 are incremented with a write to the memory on that page. The counters for pages 14 and 15 are externally triggered. See the method readCounter to read a counter directly. Note that the the counters may also be read with the PagedMemoryBank interface as 'extra' information on a page read.
The memory can be accessed through the objects that are returned from the getMemoryBanks method.
The following is a list of the MemoryBank instances that are returned:
Read the two external counters of this containers instance 'owd':
System.out.print("Counter on page 14: " + owd.readCounter(14));
System.out.print("Counter on page 15: " + owd.readCounter(15));
See the usage example in OneWireContainer to enumerate the MemoryBanks. See the usage examples in MemoryBank and PagedMemoryBank for bank specific operations.
http://pdfserv.maxim-ic.com/arpdf/DS2422-DS2423.pdf
Create an empty container that is not complete until after a call to setupContainer.
This is one of the methods to construct a container. The others are through creating a OneWireContainer with parameters.
| OneWireContainer1D | ( | DSPortAdapter | sourceAdapter, |
| byte[] | newAddress | ||
| ) |
Create a container with the provided adapter instance and the address of the iButton or 1-Wire device.
This is one of the methods to construct a container. The other is through creating a OneWireContainer with NO parameters.
| sourceAdapter | adapter instance used to communicate with this iButton |
| newAddress | Address of this 1-Wire device |
| OneWireContainer1D | ( | DSPortAdapter | sourceAdapter, |
| long | newAddress | ||
| ) |
Create a container with the provided adapter instance and the address of the iButton or 1-Wire device.
This is one of the methods to construct a container. The other is through creating a OneWireContainer with NO parameters.
| sourceAdapter | adapter instance used to communicate with this 1-Wire device |
| newAddress | Address of this 1-Wire device |
| OneWireContainer1D | ( | DSPortAdapter | sourceAdapter, |
| String | newAddress | ||
| ) |
Create a container with the provided adapter instance and the address of the iButton or 1-Wire device.
This is one of the methods to construct a container. The other is through creating a OneWireContainer with NO parameters.
| sourceAdapter | adapter instance used to communicate with this 1-Wire device |
| newAddress | Address of this 1-Wire device |
| String getDescription | ( | ) |
Get a short description of the function of this iButton or 1-Wire Device type.
Reimplemented from OneWireContainer.
| int getMaxSpeed | ( | ) |
Get the maximum speed this iButton or 1-Wire device can communicate at.
Override this method if derived iButton type can go faster then SPEED_REGULAR(0).
Reimplemented from OneWireContainer.
| Enumeration getMemoryBanks | ( | ) |
Get an enumeration of memory bank instances that implement one or more of the following interfaces: MemoryBank, PagedMemoryBank, and OTPMemoryBank.
Enumeration of memory banks Reimplemented from OneWireContainer.
| String getName | ( | ) |
Get the Maxim Integrated Products part number of the iButton or 1-Wire Device as a string.
For example 'DS1992'.
Reimplemented from OneWireContainer.
| long readCounter | ( | int | counterPage | ) | throws OneWireIOException, OneWireException |
Read the counter value associated with a page on this 1-Wire Device.
| counterPage | page number of the counter to read |
| OneWireIOException | on a 1-Wire communication error such as no 1-Wire device present. This could be caused by a physical interruption in the 1-Wire Network due to shorts or a newly arriving 1-Wire device issuing a 'presence pulse'. |
| OneWireException | on a communication or setup error with the 1-Wire adapter |
1.7.3