|
1-Wire API for .NET Version 4.00
|
Inherits com::dalsemi::onewire::container::OneWireContainer, and com::dalsemi::onewire::container::SwitchContainer.
Public Member Functions | |
| OneWireContainer1C () | |
Creates a new OneWireContainer for communication with a DS28E04. | |
| OneWireContainer1C (DSPortAdapter sourceAdapter, byte[] newAddress) | |
Creates a new OneWireContainer for communication with a DS28E04. | |
| OneWireContainer1C (DSPortAdapter sourceAdapter, long newAddress) | |
Creates a new OneWireContainer for communication with a DS28E04. | |
| OneWireContainer1C (DSPortAdapter sourceAdapter, String newAddress) | |
Creates a new OneWireContainer for communication with a DS28E04. | |
| String | getName () |
Gets the Maxim Integrated Products part number of the iButton or 1-Wire Device as a java.lang.String. | |
| Enumeration | getMemoryBanks () |
| Gets an enumeration of memory bank instances that implement one or more of the following interfaces: MemoryBank, PagedMemoryBank, and OTPMemoryBank. | |
| String | getAlternateNames () |
| Retrieves the alternate Maxim Integrated Products part numbers or names. | |
| String | getDescription () |
| Gets a short description of the function of this iButton or 1-Wire Device type. | |
| int | getNumberChannels (byte[] state) |
| Gets the number of channels supported by this switch. | |
| boolean | isHighSideSwitch () |
| Checks if the channels of this switch are 'high side' switches. | |
| boolean | hasActivitySensing () |
| Checks if the channels of this switch support activity sensing. | |
| boolean | hasLevelSensing () |
| Checks if the channels of this switch support level sensing. | |
| boolean | hasSmartOn () |
| Checks if the channels of this switch support 'smart on'. | |
| boolean | onlySingleChannelOn () |
| Checks if the channels of this switch require that only one channel is on at any one time. | |
| boolean | getLevel (int channel, byte[] state) |
| Checks the sensed level on the indicated channel. | |
| boolean | getLatchState (int channel, byte[] state) |
| Checks the latch state of the indicated channel. | |
| boolean | getSensedActivity (int channel, byte[] state) throws OneWireException |
| Checks if the indicated channel has experienced activity. | |
| void | clearActivity () throws OneWireException |
| Clears the activity latches the next time possible. | |
| void | setLatchState (int channel, boolean latchState, boolean doSmart, byte[] state) |
| Sets the latch state of the indicated channel. | |
| void | setLatchState (byte set, byte[] state) |
| Sets the latch state for all of the channels. | |
| byte[] | readDevice () throws OneWireIOException, OneWireException |
| Retrieves the 1-Wire device sensor state. | |
| byte[] | readRegister () throws OneWireIOException, OneWireException |
| Retrieves the 1-Wire device register mask. | |
| void | writeDevice (byte[] state) throws OneWireIOException, OneWireException |
| Updates the latch state for the 2 general purpose PIO pins. | |
| void | writeRegister (byte[] register) throws OneWireIOException, OneWireException |
| Writes the 1-Wire device register mask that have been changed by 'set' methods. | |
| boolean | isVccPowered (byte[] register) throws OneWireIOException, OneWireException |
| Retrieves the state of the VCC pin. | |
| void | clearPowerOnReset (byte[] register) |
| Checks if the Power On Reset if on and if so clears it. | |
| void | orConditionalSearch (byte[] register) |
| Checks if the 'or' Condition Search is set and if not sets it. | |
| void | andConditionalSearch (byte[] register) |
| Checks if the 'and' Conditional Search is set and if not sets it. | |
| void | setConditionalSearchLogicLevel (byte[] register) |
| Checks if the 'PIO Level' Conditional Search is set for input and if not sets it. | |
| void | setConditionalSearchActivity (byte[] register) |
| Checks if the 'PIO Activity latches' are set for Conditional Search and if not sets it. | |
| void | setChannelMask (int channel, boolean set, byte[] register) |
| Sets the channel passed to the proper state depending on the set parameter for responding to the Conditional Search. | |
| void | setChannelPolarity (int channel, boolean set, byte[] register) |
| Sets the channel passed to the proper state depending on the set parameter for the correct polarity in the Conditional Search. | |
| boolean | getChannelMask (int channel, byte[] register) |
| Retrieves the information if the channel is masked for the Conditional Search. | |
| boolean | getChannelPolarity (int channel, byte[] register) |
| Retrieves the polarity of the channel for the Conditional Search. | |
Static Public Attributes | |
| static final byte | PIO_ACCESS_READ = ( byte ) 0xF5 |
| Reads the PIO logical status in an endless loops. | |
| static final byte | PIO_ACCESS_WRITE = ( byte ) 0x5A |
| Writes the PIO output latch. | |
| static final byte | PIO_ACCESS_PULSE = ( byte ) 0xA5 |
| Generates a pulse on the selected PIOs. | |
| static final byte | RESET_ACTIVITY_LATCHES = ( byte ) 0xC3 |
| Generates a pulse on the selected PIOs. | |
| static final byte | WRITE_REGISTER = ( byte ) 0xCC |
| Writes the value to the Conditional Search registers or Control/Status register. | |
1-Wire® container for a Addressable 1-Wire 4K-bit EEPROM, DS28E04. This container encapsulates the functionality of the 1-Wire family type 1C (hex)
Creates a new OneWireContainer for communication with a DS28E04.
Note that the method setupContainer(com.dalsemi.onewire.adapter.DSPortAdapter,byte[]) must be called to set the correct DSPortAdapter device address.
| OneWireContainer1C | ( | DSPortAdapter | sourceAdapter, |
| byte[] | newAddress | ||
| ) |
Creates a new OneWireContainer for communication with a DS28E04.
| sourceAdapter | adapter object required to communicate with this 1-Wire device |
| newAddress | address of this DS28E04 |
| OneWireContainer1C | ( | DSPortAdapter | sourceAdapter, |
| long | newAddress | ||
| ) |
Creates a new OneWireContainer for communication with a DS28E04.
| sourceAdapter | adapter object required to communicate with this 1-Wire device |
| newAddress | address of this DS28E04 |
| OneWireContainer1C | ( | DSPortAdapter | sourceAdapter, |
| String | newAddress | ||
| ) |
Creates a new OneWireContainer for communication with a DS28E04.
| sourceAdapter | adapter object required to communicate with this 1-Wire device |
| newAddress | address of this DS28E04 |
| void andConditionalSearch | ( | byte[] | register | ) |
Checks if the 'and' Conditional Search is set and if not sets it.
| register | current register for conditional search, which if returned from readRegister() |
| void clearActivity | ( | ) | throws OneWireException |
Clears the activity latches the next time possible.
For example, on a DS2406/07, this happens the next time the status is read with readDevice().
| OneWireException | if this device does not support activity sensing |
Implements SwitchContainer.
| void clearPowerOnReset | ( | byte[] | register | ) |
Checks if the Power On Reset if on and if so clears it.
| register | current register for conditional search, which if returned from readRegister() |
| String getAlternateNames | ( | ) |
Retrieves the alternate Maxim Integrated Products part numbers or names.
A 'family' of MicroLAN devices may have more than one part number depending on packaging. There can also be nicknames such as "Crypto iButton".
Reimplemented from OneWireContainer.
| boolean getChannelMask | ( | int | channel, |
| byte[] | register | ||
| ) |
Retrieves the information if the channel is masked for the Conditional Search.
| channel | current channel to set |
| register | current register for conditional search, which if returned from readRegister() |
true if the channel is masked and false other wise. | boolean getChannelPolarity | ( | int | channel, |
| byte[] | register | ||
| ) |
Retrieves the polarity of the channel for the Conditional Search.
| channel | current channel to set |
| register | current register for conditional search, which if returned from readRegister() |
true if the channel is masked and false other wise. | String getDescription | ( | ) |
Gets a short description of the function of this iButton or 1-Wire Device type.
Reimplemented from OneWireContainer.
| boolean getLatchState | ( | int | channel, |
| byte[] | state | ||
| ) |
Checks the latch state of the indicated channel.
| channel | channel to execute this operation, in the range [0 to (getNumberChannels(byte[]) - 1)] |
| state | current state of the device returned from readDevice() |
true if channel latch is 'on' or conducting and false if channel latch is 'off' and not conducting. Note that the actual output when the latch is 'on' is returned from the isHighSideSwitch() method.Implements SwitchContainer.
| boolean getLevel | ( | int | channel, |
| byte[] | state | ||
| ) |
Checks the sensed level on the indicated channel.
To avoid an exception, verify that this switch has level sensing with the hasLevelSensing(). Level sensing means that the device can sense the logic level on its PIO pin.
| channel | channel to execute this operation, in the range [0 to (getNumberChannels(byte[]) - 1)] |
| state | current state of the device returned from readDevice() |
true if level sensed is 'high' and false if level sensed is 'low'Implements SwitchContainer.
| Enumeration getMemoryBanks | ( | ) |
Gets an enumeration of memory bank instances that implement one or more of the following interfaces: MemoryBank, PagedMemoryBank, and OTPMemoryBank.
Enumeration of memory banks Reimplemented from OneWireContainer.
| String getName | ( | ) |
Gets the Maxim Integrated Products part number of the iButton or 1-Wire Device as a java.lang.String.
Reimplemented from OneWireContainer.
| int getNumberChannels | ( | byte[] | state | ) |
Gets the number of channels supported by this switch.
Channel specific methods will use a channel number specified by an integer from [0 to (getNumberChannels(byte[]) - 1)]. Note that all devices of the same family will not necessarily have the same number of channels.
| state | current state of the device returned from readDevice() |
Implements SwitchContainer.
| boolean getSensedActivity | ( | int | channel, |
| byte[] | state | ||
| ) | throws OneWireException |
Checks if the indicated channel has experienced activity.
This occurs when the level on the PIO pins changes. To clear the activity that is reported, call clearActivity(). To avoid an exception, verify that this device supports activity sensing by calling the method hasActivitySensing().
| channel | channel to execute this operation, in the range [0 to (getNumberChannels(byte[]) - 1)] |
| state | current state of the device returned from readDevice() |
true if activity was detected and false if no activity was detected| OneWireException | if this device does not have activity sensing |
Implements SwitchContainer.
| boolean hasActivitySensing | ( | ) |
Checks if the channels of this switch support activity sensing.
If this method returns true then the method getSensedActivity(int,byte[]) can be used.
true if channels support activity sensingImplements SwitchContainer.
| boolean hasLevelSensing | ( | ) |
Checks if the channels of this switch support level sensing.
If this method returns true then the method getLevel(int,byte[]) can be used.
true if channels support level sensingImplements SwitchContainer.
| boolean hasSmartOn | ( | ) |
Checks if the channels of this switch support 'smart on'.
Smart on is the ability to turn on a channel such that only 1-Wire device on this channel are awake and ready to do an operation. This greatly reduces the time to discover the device down a branch. If this method returns true then the method setLatchState(int,boolean,boolean,byte[]) can be used with the doSmart parameter true.
true if channels support 'smart on'Implements SwitchContainer.
| boolean isHighSideSwitch | ( | ) |
Checks if the channels of this switch are 'high side' switches.
This indicates that when 'on' or true, the switch output is connect to the 1-Wire data. If this method returns false then when the switch is 'on' or true, the switch is connected to ground.
true if the switch is a 'high side' switch, false if the switch is a 'low side' switchImplements SwitchContainer.
| boolean isVccPowered | ( | byte[] | register | ) | throws OneWireIOException, OneWireException |
Retrieves the state of the VCC pin.
If the pin is powered 'TRUE' is returned else 'FALSE' is returned if the pin is grounded.
true if VCC is powered and false if it is grounded.| OneWireIOException | on a 1-Wire communication error such as reading an incorrect CRC from a 1-Wire device. This could be caused by a physical interruption in the 1-Wire Network due to shorts or a newly arriving 1-Wire device issuing a 'presence pulse'. |
| OneWireException | on a communication or setup error with the 1-Wire adapter |
| boolean onlySingleChannelOn | ( | ) |
Checks if the channels of this switch require that only one channel is on at any one time.
If this method returns true then the method setLatchState(int,boolean,boolean,byte[]) will not only affect the state of the given channel but may affect the state of the other channels as well to insure that only one channel is on at a time.
true if only one channel can be on at a time.Implements SwitchContainer.
| void orConditionalSearch | ( | byte[] | register | ) |
Checks if the 'or' Condition Search is set and if not sets it.
| register | current register for conditional search, which if returned from readRegister() |
| byte [] readDevice | ( | ) | throws OneWireIOException, OneWireException |
Retrieves the 1-Wire device sensor state.
This state is returned as a byte array. Pass this byte array to the 'get' and 'set' methods. If the device state needs to be changed then call the 'writeDevice' to finalize the changes.
| OneWireIOException | on a 1-Wire communication error such as reading an incorrect CRC from a 1-Wire device. This could be caused by a physical interruption in the 1-Wire Network due to shorts or a newly arriving 1-Wire device issuing a 'presence pulse'. |
| OneWireException | on a communication or setup error with the 1-Wire adapter |
Implements OneWireSensor.
| byte [] readRegister | ( | ) | throws OneWireIOException, OneWireException |
Retrieves the 1-Wire device register mask.
This register is returned as a byte array. Pass this byte array to the 'get' and 'set' methods. If the device register mask needs to be changed then call the 'writeRegister' to finalize the changes.
| OneWireIOException | on a 1-Wire communication error such as reading an incorrect CRC from a 1-Wire device. This could be caused by a physical interruption in the 1-Wire Network due to shorts or a newly arriving 1-Wire device issuing a 'presence pulse'. |
| OneWireException | on a communication or setup error with the 1-Wire adapter |
| void setChannelMask | ( | int | channel, |
| boolean | set, | ||
| byte[] | register | ||
| ) |
Sets the channel passed to the proper state depending on the set parameter for responding to the Conditional Search.
| channel | current channel to set |
| set | whether to turn the channel on/off for Conditional Search |
| register | current register for conditional search, which if returned from readRegister() |
| void setChannelPolarity | ( | int | channel, |
| boolean | set, | ||
| byte[] | register | ||
| ) |
Sets the channel passed to the proper state depending on the set parameter for the correct polarity in the Conditional Search.
| channel | current channel to set |
| set | whether to turn the channel on/off for polarity Conditional Search |
| register | current register for conditional search, which if returned from readRegister() |
| void setConditionalSearchActivity | ( | byte[] | register | ) |
Checks if the 'PIO Activity latches' are set for Conditional Search and if not sets it.
| register | current register for conditional search, which if returned from readRegister() |
| void setConditionalSearchLogicLevel | ( | byte[] | register | ) |
Checks if the 'PIO Level' Conditional Search is set for input and if not sets it.
| pinActivity | if true, the activity latch for the pin is used for the conditional search. Otherwise, the sensed level of the pin is used for the conditional search. |
| register | current register for conditional search, which if returned from readRegister() |
| void setLatchState | ( | byte | set, |
| byte[] | state | ||
| ) |
Sets the latch state for all of the channels.
The method writeDevice() must be called to finalize changes to the device. Note that multiple 'set' methods can be called before one call to writeDevice().
| set | the state to set all of the channels, in the range [0 to (getNumberChannels(byte[]) - 1)] |
| state | current state of the device returned from readDevice() |
| void setLatchState | ( | int | channel, |
| boolean | latchState, | ||
| boolean | doSmart, | ||
| byte[] | state | ||
| ) |
Sets the latch state of the indicated channel.
The method writeDevice() must be called to finalize changes to the device. Note that multiple 'set' methods can be called before one call to writeDevice().
| channel | channel to execute this operation, in the range [0 to (getNumberChannels(byte[]) - 1)] |
| latchState | true to set the channel latch 'on' (conducting) and false to set the channel latch 'off' (not conducting). Note that the actual output when the latch is 'on' is returned from the isHighSideSwitch() method. |
| doSmart | If latchState is 'on'/true then doSmart indicates if a 'smart on' is to be done. To avoid an exception check the capabilities of this device using the hasSmartOn() method. |
| state | current state of the device returned from readDevice() |
Implements SwitchContainer.
| void writeDevice | ( | byte[] | state | ) | throws OneWireIOException, OneWireException |
Updates the latch state for the 2 general purpose PIO pins.
This has the side-effect of also sampling the PIO pins level after updating the latch, so the state buffer is updated with this new level information.
| state | 1-Wire device sensor state |
| OneWireIOException | on a 1-Wire communication error such as reading an incorrect CRC from a 1-Wire device. This could be caused by a physical interruption in the 1-Wire Network due to shorts or a newly arriving 1-Wire device issuing a 'presence pulse'. |
| OneWireException | on a communication or setup error with the 1-Wire adapter |
Implements OneWireSensor.
| void writeRegister | ( | byte[] | register | ) | throws OneWireIOException, OneWireException |
Writes the 1-Wire device register mask that have been changed by 'set' methods.
| register | 1-Wire device sensor state |
| OneWireIOException | on a 1-Wire communication error such as reading an incorrect CRC from a 1-Wire device. This could be caused by a physical interruption in the 1-Wire Network due to shorts or a newly arriving 1-Wire device issuing a 'presence pulse'. |
| OneWireException | on a communication or setup error with the 1-Wire adapter |
1.7.3