, including all inherited members.
| adapter | OneWireContainer | [protected] |
| address | OneWireContainer | [protected] |
| CHANNEL_A_ONLY | OneWireContainer12 | [static] |
| CHANNEL_B_ONLY | OneWireContainer12 | [static] |
| CHANNEL_BOTH | OneWireContainer12 | [static] |
| CHANNEL_NONE | OneWireContainer12 | [static] |
| channelAccess(byte[] inbuffer, boolean toggleRW, boolean readInitially, int CRCMode, int channelMode, boolean clearActivity, boolean interleave) | OneWireContainer12 | |
| clearActivity() | OneWireContainer12 | |
| CRC_DISABLE | OneWireContainer12 | [static] |
| CRC_EVERY_32_BYTES | OneWireContainer12 | [static] |
| CRC_EVERY_8_BYTES | OneWireContainer12 | [static] |
| CRC_EVERY_BYTE | OneWireContainer12 | [static] |
| DONT_CHANGE | OneWireContainer12 | [static] |
| doSpeed() | OneWireContainer | |
| equals(Object obj) | OneWireContainer | |
| getAdapter() | OneWireContainer | |
| getAddress() | OneWireContainer | |
| getAddressAsLong() | OneWireContainer | |
| getAddressAsString() | OneWireContainer | |
| getAlternateNames() | OneWireContainer12 | |
| getDescription() | OneWireContainer12 | |
| getLatchState(int channel, byte[] state) | OneWireContainer12 | |
| getLevel(int channel, byte[] state) | OneWireContainer12 | |
| getMaxSpeed() | OneWireContainer | |
| getMemoryBanks() | OneWireContainer12 | |
| getName() | OneWireContainer12 | |
| getNumberChannels(byte[] state) | OneWireContainer12 | |
| getSensedActivity(int channel, byte[] state) | OneWireContainer12 | |
| hasActivitySensing() | OneWireContainer12 | |
| hashCode() | OneWireContainer | |
| hasLevelSensing() | OneWireContainer12 | |
| hasSmartOn() | OneWireContainer12 | |
| isAlarming() | OneWireContainer | |
| isHighSideSwitch() | OneWireContainer12 | |
| isPowerSupplied(byte[] state) | OneWireContainer12 | |
| isPresent() | OneWireContainer | |
| OneWireContainer() | OneWireContainer | |
| OneWireContainer(DSPortAdapter sourceAdapter, byte[] newAddress) | OneWireContainer | |
| OneWireContainer(DSPortAdapter sourceAdapter, long newAddress) | OneWireContainer | |
| OneWireContainer(DSPortAdapter sourceAdapter, String newAddress) | OneWireContainer | |
| OneWireContainer12() | OneWireContainer12 | |
| OneWireContainer12(DSPortAdapter sourceAdapter, byte[] newAddress) | OneWireContainer12 | |
| OneWireContainer12(DSPortAdapter sourceAdapter, long newAddress) | OneWireContainer12 | |
| OneWireContainer12(DSPortAdapter sourceAdapter, String newAddress) | OneWireContainer12 | |
| onlySingleChannelOn() | OneWireContainer12 | |
| POLARITY_ONE | OneWireContainer12 | [static] |
| POLARITY_ZERO | OneWireContainer12 | [static] |
| readDevice() | OneWireContainer12 | |
| setLatchState(int channel, boolean latchState, boolean doSmart, byte[] state) | OneWireContainer12 | |
| setSearchConditions(byte channel, byte source, byte polarity, byte[] state) | OneWireContainer12 | |
| setSpeed(int newSpeed, boolean fallBack) | OneWireContainer | |
| setSpeedCheck(boolean doSpeedCheck) | OneWireContainer12 | |
| setupContainer(DSPortAdapter sourceAdapter, byte[] newAddress) | OneWireContainer | |
| setupContainer(DSPortAdapter sourceAdapter, long newAddress) | OneWireContainer | |
| setupContainer(DSPortAdapter sourceAdapter, String newAddress) | OneWireContainer | |
| SOURCE_ACTIVITY_LATCH | OneWireContainer12 | [static] |
| SOURCE_FLIP_FLOP | OneWireContainer12 | [static] |
| SOURCE_PIO | OneWireContainer12 | [static] |
| speed | OneWireContainer | [protected] |
| speedFallBackOK | OneWireContainer | [protected] |
| toString() | OneWireContainer | |
| writeDevice(byte[] state) | OneWireContainer12 | |