This is the complete list of members for
OneWireContainer10, including all inherited members.
| adapter | OneWireContainer | [protected] |
| address | OneWireContainer | [protected] |
| ALARM_HIGH | TemperatureContainer | [static] |
| ALARM_LOW | TemperatureContainer | [static] |
| convertToCelsius(double fahrenheitTemperature) | OneWireContainer10 | [static] |
| convertToFahrenheit(double celsiusTemperature) | OneWireContainer10 | [static] |
| doSpeed() | OneWireContainer | |
| doTemperatureConvert(byte[] state) | OneWireContainer10 | |
| equals(Object obj) | OneWireContainer | |
| getAdapter() | OneWireContainer | |
| getAddress() | OneWireContainer | |
| getAddressAsLong() | OneWireContainer | |
| getAddressAsString() | OneWireContainer | |
| getAlternateNames() | OneWireContainer10 | |
| getDescription() | OneWireContainer10 | |
| getMaxSpeed() | OneWireContainer | |
| getMaxTemperature() | OneWireContainer10 | |
| getMemoryBanks() | OneWireContainer | |
| getMinTemperature() | OneWireContainer10 | |
| getName() | OneWireContainer10 | |
| getTemperature(byte[] state) | OneWireContainer10 | |
| getTemperatureAlarm(int alarmType, byte[] state) | OneWireContainer10 | |
| getTemperatureAlarmResolution() | OneWireContainer10 | |
| getTemperatureResolution(byte[] state) | OneWireContainer10 | |
| getTemperatureResolutions() | OneWireContainer10 | |
| hashCode() | OneWireContainer | |
| hasSelectableTemperatureResolution() | OneWireContainer10 | |
| hasTemperatureAlarms() | OneWireContainer10 | |
| isAlarming() | OneWireContainer | |
| isPresent() | OneWireContainer | |
| OneWireContainer() | OneWireContainer | |
| OneWireContainer(DSPortAdapter sourceAdapter, byte[] newAddress) | OneWireContainer | |
| OneWireContainer(DSPortAdapter sourceAdapter, long newAddress) | OneWireContainer | |
| OneWireContainer(DSPortAdapter sourceAdapter, String newAddress) | OneWireContainer | |
| OneWireContainer10() | OneWireContainer10 | |
| OneWireContainer10(DSPortAdapter sourceAdapter, byte[] newAddress) | OneWireContainer10 | |
| OneWireContainer10(DSPortAdapter sourceAdapter, long newAddress) | OneWireContainer10 | |
| OneWireContainer10(DSPortAdapter sourceAdapter, String newAddress) | OneWireContainer10 | |
| readDevice() | OneWireContainer10 | |
| RESOLUTION_MAXIMUM | OneWireContainer10 | [static] |
| RESOLUTION_NORMAL | OneWireContainer10 | [static] |
| setSpeed(int newSpeed, boolean fallBack) | OneWireContainer | |
| setTemperatureAlarm(int alarmType, double alarmValue, byte[] state) | OneWireContainer10 | |
| setTemperatureResolution(double resolution, byte[] state) | OneWireContainer10 | |
| setupContainer(DSPortAdapter sourceAdapter, byte[] newAddress) | OneWireContainer | |
| setupContainer(DSPortAdapter sourceAdapter, long newAddress) | OneWireContainer | |
| setupContainer(DSPortAdapter sourceAdapter, String newAddress) | OneWireContainer | |
| speed | OneWireContainer | [protected] |
| speedFallBackOK | OneWireContainer | [protected] |
| toString() | OneWireContainer | |
| writeDevice(byte[] state) | OneWireContainer10 | |