|
1-Wire API for .NET Version 4.00
|
Inherits com::dalsemi::onewire::container::OneWireContainer.
Public Member Functions | |
| OneWireContainer01 () | |
| Create an empty container. | |
| OneWireContainer01 (DSPortAdapter sourceAdapter, byte[] newAddress) | |
| Create a container with a provided adapter object and the address of the iButton or 1-Wire device. | |
| OneWireContainer01 (DSPortAdapter sourceAdapter, long newAddress) | |
| Create a container with a provided adapter object and the address of the iButton or 1-Wire device. | |
| OneWireContainer01 (DSPortAdapter sourceAdapter, String newAddress) | |
| Create a container with a provided adapter object and the address of the iButton or 1-Wire device. | |
| String | getName () |
Retrieves the Maxim Integrated Products part number of the 1-Wire device as a String. | |
| String | getAlternateNames () |
| Retrieves the alternate Maxim Integrated Products part numbers or names. | |
| String | getDescription () |
| Retrieves a short description of the function of the 1-Wire device type. | |
1-Wire® container that encapsulates the functionality of the 1-Wire family type 01 (hex), Maxim Integrated Products part number: DS1990A, Serial Number.
This 1-Wire device is used as a unique serial number.
http://pdfserv.maxim-ic.com/arpdf/DS1990A.pdf
http://pdfserv.maxim-ic.com/arpdf/DS2401.pdf
http://pdfserv.maxim-ic.com/arpdf/DS1420.pdf
Create an empty container.
Must call setupContainer before using this new container.
This is one of the methods to construct a container. The others are through creating a OneWireContainer with parameters.
| OneWireContainer01 | ( | DSPortAdapter | sourceAdapter, |
| byte[] | newAddress | ||
| ) |
Create a container with a provided adapter object and the address of the iButton or 1-Wire device.
This is one of the methods to construct a container. The other is through creating a OneWireContainer with NO parameters.
| sourceAdapter | adapter object required to communicate with this iButton. |
| newAddress | address of this 1-Wire device |
| OneWireContainer01 | ( | DSPortAdapter | sourceAdapter, |
| long | newAddress | ||
| ) |
Create a container with a provided adapter object and the address of the iButton or 1-Wire device.
This is one of the methods to construct a container. The other is through creating a OneWireContainer with NO parameters.
| sourceAdapter | adapter object required to communicate with this iButton. |
| newAddress | address of this 1-Wire device |
| OneWireContainer01 | ( | DSPortAdapter | sourceAdapter, |
| String | newAddress | ||
| ) |
Create a container with a provided adapter object and the address of the iButton or 1-Wire device.
This is one of the methods to construct a container. The other is through creating a OneWireContainer with NO parameters.
| sourceAdapter | adapter object required to communicate with this iButton. |
| newAddress | address of this 1-Wire device |
| String getAlternateNames | ( | ) |
Retrieves the alternate Maxim Integrated Products part numbers or names.
A 'family' of 1-Wire Network devices may have more than one part number depending on packaging. There can also be nicknames such as 'Crypto iButton'.
Reimplemented from OneWireContainer.
| String getDescription | ( | ) |
Retrieves a short description of the function of the 1-Wire device type.
Reimplemented from OneWireContainer.
| String getName | ( | ) |
Retrieves the Maxim Integrated Products part number of the 1-Wire device as a String.
For example 'Crypto iButton' or 'DS1992'.
Reimplemented from OneWireContainer.
1.7.3