|
1-Wire API for .NET Version 4.00
|
A OneWireContainer encapsulates the DSPortAdapter, the 1-Wire® network address, and methods to manipulate a specific 1-Wire device.
More...
Inherited by OneWireContainer01, OneWireContainer02, OneWireContainer04, OneWireContainer05, OneWireContainer06, OneWireContainer08, OneWireContainer09, OneWireContainer0A, OneWireContainer0B, OneWireContainer0C, OneWireContainer0F, OneWireContainer10, OneWireContainer12, OneWireContainer13, OneWireContainer14, OneWireContainer18, OneWireContainer1A, OneWireContainer1C, OneWireContainer1D, OneWireContainer1F, OneWireContainer20, OneWireContainer21, OneWireContainer23, OneWireContainer24, OneWireContainer28, OneWireContainer29, OneWireContainer2C, OneWireContainer2D, OneWireContainer30, OneWireContainer33, OneWireContainer37, OneWireContainer3A, OneWireContainer41, OneWireContainer42, and OneWireContainer43.
Public Member Functions | |
| OneWireContainer () | |
| Create an empty container. | |
| OneWireContainer (DSPortAdapter sourceAdapter, byte[] newAddress) | |
| Create a container with a provided adapter object and the address of the iButton or 1-Wire device. | |
| OneWireContainer (DSPortAdapter sourceAdapter, long newAddress) | |
| Create a container with a provided adapter object and the address of the iButton or 1-Wire device. | |
| OneWireContainer (DSPortAdapter sourceAdapter, String newAddress) | |
| Create a container with a provided adapter object and the address of the iButton or 1-Wire device. | |
| void | setupContainer (DSPortAdapter sourceAdapter, byte[] newAddress) |
| Provides this container with the adapter object used to access this device and the address of the iButton or 1-Wire device. | |
| void | setupContainer (DSPortAdapter sourceAdapter, long newAddress) |
| Provides this container with the adapter object used to access this device and the address of the iButton or 1-Wire device. | |
| void | setupContainer (DSPortAdapter sourceAdapter, String newAddress) |
| Provides this container with the adapter object used to access this device and the address of the iButton or 1-Wire device. | |
| DSPortAdapter | getAdapter () |
| Retrieves the port adapter object used to create this container. | |
| String | getName () |
Retrieves the Maxim Integrated Products part number of the 1-Wire device as a String. | |
| String | getAlternateNames () |
| Retrieves the alternate Maxim Integrated Products part numbers or names. | |
| String | getDescription () |
| Retrieves a short description of the function of the 1-Wire device type. | |
| void | setSpeed (int newSpeed, boolean fallBack) |
| Sets the maximum speed for this container. | |
| int | getMaxSpeed () |
| Returns the maximum speed this iButton or 1-Wire device can communicate at. | |
| byte[] | getAddress () |
| Gets the 1-Wire Network address of this device as an array of bytes. | |
| String | getAddressAsString () |
| Gets this device's 1-Wire Network address as a String. | |
| long | getAddressAsLong () |
| Gets this device's 1-Wire Network address as a long. | |
| Enumeration | getMemoryBanks () |
Returns an Enumeration of MemoryBank. | |
| boolean | isPresent () throws OneWireIOException,OneWireException |
| Verifies that the iButton or 1-Wire device is present on the 1-Wire Network. | |
| boolean | isAlarming () throws OneWireIOException,OneWireException |
| Verifies that the iButton or 1-Wire device is present on the 1-Wire Network and in an alarm state. | |
| void | doSpeed () throws OneWireIOException, OneWireException |
| Go to the specified speed for this container. | |
| int | hashCode () |
| Returns a hash code value for the object. | |
| boolean | equals (Object obj) |
| Indicates whether some other object is "equal to" this one. | |
| String | toString () |
| Returns a string representation of the object. | |
Protected Attributes | |
| DSPortAdapter | adapter |
| Reference to the adapter that is needed to communicate with this iButton or 1-Wire device. | |
| byte[] | address |
| 1-Wire Network Address of this iButton or 1-Wire device. | |
| int | speed |
| Communication speed requested. | |
| boolean | speedFallBackOK |
| Flag to indicate that falling back to a slower speed then requested is OK. | |
A OneWireContainer encapsulates the DSPortAdapter, the 1-Wire® network address, and methods to manipulate a specific 1-Wire device.
A 1-Wire device may be in the form of a stainless steel armored can, called an iButton®, or in standard IC plastic packaging.
General 1-Wire device container class with basic communication functions. This class should only be used if a device specific class is not available or known. Most OneWireContainer classes will extend this basic class.
1-Wire devices with memory can be accessed through the objects that are returned from the getMemoryBanks method. See the usage example below.
Enumerate memory banks retrieved from the OneWireContainer instance 'owd' and cast to the highest interface. See the interface descriptions MemoryBank, PagedMemoryBank, and OTPMemoryBank for specific examples.
MemoryBank mb;
PagedMemoryBank pg_mb;
OTPMemoryBank otp_mb; for(Enumeration bank_enum = owd.getMemoryBanks();
bank_enum.hasMoreElements(); )
{
// get the next memory bank, cast to MemoryBank
mb = (MemoryBank)bank_enum.nextElement(); // check if has paged services
if (mb instanceof PagedMemoryBank)
pg_mb = (PagedMemoryBank)mb; // check if has One-Time-Programable services
if (mb instanceof OTPMemoryBank)
otp_mb = (OTPMemoryBank)mb;
}
| OneWireContainer | ( | ) |
Create an empty container.
Must call setupContainer before using this new container.
This is one of the methods to construct a container. The others are through creating a OneWireContainer with parameters.
| OneWireContainer | ( | DSPortAdapter | sourceAdapter, |
| byte[] | newAddress | ||
| ) |
Create a container with a provided adapter object and the address of the iButton or 1-Wire device.
This is one of the methods to construct a container. The other is through creating a OneWireContainer with NO parameters.
| sourceAdapter | adapter object required to communicate with this iButton. |
| newAddress | address of this 1-Wire device |
| OneWireContainer | ( | DSPortAdapter | sourceAdapter, |
| long | newAddress | ||
| ) |
Create a container with a provided adapter object and the address of the iButton or 1-Wire device.
This is one of the methods to construct a container. The other is through creating a OneWireContainer with NO parameters.
| sourceAdapter | adapter object required to communicate with this iButton. |
| newAddress | address of this 1-Wire device |
| OneWireContainer | ( | DSPortAdapter | sourceAdapter, |
| String | newAddress | ||
| ) |
Create a container with a provided adapter object and the address of the iButton or 1-Wire device.
This is one of the methods to construct a container. The other is through creating a OneWireContainer with NO parameters.
| sourceAdapter | adapter object required to communicate with this iButton. |
| newAddress | address of this 1-Wire device |
| void doSpeed | ( | ) | throws OneWireIOException, OneWireException |
Go to the specified speed for this container.
This method uses the containers selected speed (method setSpeed(speed, fallback)) and will optionally fall back to a slower speed if communciation failed. Only call this method once to get the device into the desired speed as long as the device is still responding.
| OneWireIOException | WHEN selected speed fails and fallback is false |
| OneWireException | WHEN hypterdrive is selected speed |
| boolean equals | ( | Object | obj | ) |
Indicates whether some other object is "equal to" this one.
| obj | the reference object with which to compare. |
true if this object is the same as the obj argument; false otherwise. | DSPortAdapter getAdapter | ( | ) |
Retrieves the port adapter object used to create this container.
| byte [] getAddress | ( | ) |
Gets the 1-Wire Network address of this device as an array of bytes.
| long getAddressAsLong | ( | ) |
Gets this device's 1-Wire Network address as a long.
| String getAddressAsString | ( | ) |
Gets this device's 1-Wire Network address as a String.
| String getAlternateNames | ( | ) |
Retrieves the alternate Maxim Integrated Products part numbers or names.
A 'family' of 1-Wire Network devices may have more than one part number depending on packaging. There can also be nicknames such as 'Crypto iButton'.
Reimplemented in OneWireContainer01, OneWireContainer02, OneWireContainer04, OneWireContainer05, OneWireContainer09, OneWireContainer0B, OneWireContainer0F, OneWireContainer10, OneWireContainer12, OneWireContainer13, OneWireContainer14, OneWireContainer18, OneWireContainer1A, OneWireContainer1C, OneWireContainer1F, OneWireContainer20, OneWireContainer21, OneWireContainer22, OneWireContainer23, OneWireContainer24, OneWireContainer27, OneWireContainer28, OneWireContainer29, OneWireContainer2C, OneWireContainer2D, OneWireContainer30, OneWireContainer33, OneWireContainer37, OneWireContainer3A, OneWireContainer41, OneWireContainer42, and OneWireContainer43.
| String getDescription | ( | ) |
Retrieves a short description of the function of the 1-Wire device type.
Reimplemented in OneWireContainer01, OneWireContainer02, OneWireContainer04, OneWireContainer05, OneWireContainer06, OneWireContainer08, OneWireContainer09, OneWireContainer0A, OneWireContainer0B, OneWireContainer0C, OneWireContainer0F, OneWireContainer10, OneWireContainer12, OneWireContainer13, OneWireContainer14, OneWireContainer18, OneWireContainer1A, OneWireContainer1C, OneWireContainer1D, OneWireContainer1F, OneWireContainer20, OneWireContainer21, OneWireContainer22, OneWireContainer23, OneWireContainer24, OneWireContainer27, OneWireContainer28, OneWireContainer29, OneWireContainer2C, OneWireContainer2D, OneWireContainer30, OneWireContainer33, OneWireContainer37, OneWireContainer3A, OneWireContainer41, OneWireContainer42, and OneWireContainer43.
| int getMaxSpeed | ( | ) |
Returns the maximum speed this iButton or 1-Wire device can communicate at.
Override this method if derived iButton type can go faster then SPEED_REGULAR(0).
Reimplemented in OneWireContainer0A, OneWireContainer0C, OneWireContainer0F, OneWireContainer18, OneWireContainer1A, OneWireContainer1D, OneWireContainer20, OneWireContainer21, OneWireContainer23, OneWireContainer29, OneWireContainer2C, OneWireContainer2D, OneWireContainer33, OneWireContainer37, OneWireContainer3A, OneWireContainer41, OneWireContainer42, and OneWireContainer43.
| Enumeration getMemoryBanks | ( | ) |
Returns an Enumeration of MemoryBank.
Default is no memory banks.
Reimplemented in OneWireContainer04, OneWireContainer06, OneWireContainer08, OneWireContainer09, OneWireContainer0A, OneWireContainer0B, OneWireContainer0C, OneWireContainer0F, OneWireContainer12, OneWireContainer13, OneWireContainer14, OneWireContainer18, OneWireContainer1A, OneWireContainer1C, OneWireContainer1D, OneWireContainer20, OneWireContainer21, OneWireContainer23, OneWireContainer29, OneWireContainer2D, OneWireContainer30, OneWireContainer33, OneWireContainer37, OneWireContainer41, OneWireContainer42, and OneWireContainer43.
| String getName | ( | ) |
Retrieves the Maxim Integrated Products part number of the 1-Wire device as a String.
For example 'Crypto iButton' or 'DS1992'.
Reimplemented in OneWireContainer01, OneWireContainer02, OneWireContainer04, OneWireContainer05, OneWireContainer06, OneWireContainer08, OneWireContainer09, OneWireContainer0A, OneWireContainer0B, OneWireContainer0C, OneWireContainer0F, OneWireContainer10, OneWireContainer12, OneWireContainer13, OneWireContainer14, OneWireContainer18, OneWireContainer1A, OneWireContainer1C, OneWireContainer1D, OneWireContainer1F, OneWireContainer20, OneWireContainer21, OneWireContainer22, OneWireContainer23, OneWireContainer24, OneWireContainer27, OneWireContainer28, OneWireContainer29, OneWireContainer2C, OneWireContainer2D, OneWireContainer30, OneWireContainer33, OneWireContainer37, OneWireContainer3A, OneWireContainer41, OneWireContainer42, and OneWireContainer43.
| int hashCode | ( | ) |
Returns a hash code value for the object.
This method is supported for the benefit of hashtables such as those provided by java.util.Hashtable.
| boolean isAlarming | ( | ) | throws OneWireIOException,OneWireException |
Verifies that the iButton or 1-Wire device is present on the 1-Wire Network and in an alarm state.
This does not apply to all device types.
true if device present and in alarm condition| OneWireIOException | on a 1-Wire communication error such as a read back verification fails. |
| OneWireException | if adapter is not open |
| boolean isPresent | ( | ) | throws OneWireIOException,OneWireException |
Verifies that the iButton or 1-Wire device is present on the 1-Wire Network.
true if device present on the 1-Wire Network| OneWireIOException | on a 1-Wire communication error such as a read back verification fails. |
| OneWireException | if adapter is not open |
| void setSpeed | ( | int | newSpeed, |
| boolean | fallBack | ||
| ) |
Sets the maximum speed for this container.
Note this may be slower then the devices maximum speed. This method can be used by an application to restrict the communication rate due 1-Wire line conditions.
| newSpeed |
|
| fallBack | boolean indicating it is OK to fall back to a slower speed if true |
| void setupContainer | ( | DSPortAdapter | sourceAdapter, |
| byte[] | newAddress | ||
| ) |
Provides this container with the adapter object used to access this device and the address of the iButton or 1-Wire device.
| sourceAdapter | adapter object required to communicate with this iButton |
| newAddress | address of this 1-Wire device |
Reimplemented in OneWireContainer18, OneWireContainer21, OneWireContainer2D, OneWireContainer33, OneWireContainer37, OneWireContainer41, and OneWireContainer43.
| void setupContainer | ( | DSPortAdapter | sourceAdapter, |
| String | newAddress | ||
| ) |
Provides this container with the adapter object used to access this device and the address of the iButton or 1-Wire device.
| sourceAdapter | adapter object required to communicate with this iButton |
| newAddress | address of this 1-Wire device |
Reimplemented in OneWireContainer2D, OneWireContainer33, OneWireContainer37, OneWireContainer41, and OneWireContainer43.
| void setupContainer | ( | DSPortAdapter | sourceAdapter, |
| long | newAddress | ||
| ) |
Provides this container with the adapter object used to access this device and the address of the iButton or 1-Wire device.
| sourceAdapter | adapter object required to communicate with this iButton |
| newAddress | address of this 1-Wire device |
Reimplemented in OneWireContainer21, OneWireContainer2D, OneWireContainer33, OneWireContainer37, OneWireContainer41, and OneWireContainer43.
| String toString | ( | ) |
Returns a string representation of the object.
byte [] address [protected] |
1-Wire Network Address of this iButton or 1-Wire device.
Family code is byte at offset 0.
int speed [protected] |
Communication speed requested.
1.7.3