|
1-Wire API for .NET Version 4.00
|
Memory bank class for the NVRAM section of iButtons and 1-Wire devices. More...
Inherits com::dalsemi::onewire::container::PagedMemoryBank.
Inherited by MemoryBankNVCRC.
Public Member Functions | |
| MemoryBankNV (OneWireContainer ibutton, ScratchPad scratch) | |
| Memory bank contstuctor. | |
| String | getBankDescription () |
| Query to see get a string description of the current memory bank. | |
| boolean | isGeneralPurposeMemory () |
| Query to see if the current memory bank is general purpose user memory. | |
| boolean | isReadWrite () |
| Query to see if current memory bank is read/write. | |
| boolean | isWriteOnce () |
| Query to see if current memory bank is write write once such as with EPROM technology. | |
| boolean | isReadOnly () |
| Query to see if current memory bank is read only. | |
| boolean | isNonVolatile () |
| Query to see if current memory bank non-volatile. | |
| boolean | needsProgramPulse () |
| Query to see if current memory bank pages need the adapter to have a 'ProgramPulse' in order to write to the memory. | |
| boolean | needsPowerDelivery () |
| Query to see if current memory bank pages need the adapter to have a 'PowerDelivery' feature in order to write to the memory. | |
| int | getStartPhysicalAddress () |
| Query to get the starting physical address of this bank. | |
| int | getSize () |
| Query to get the memory bank size in bytes. | |
| void | setWriteVerification (boolean doReadVerf) |
| Set the write verification for the 'write()' method. | |
| int | getNumberPages () |
| Query to get the number of pages in current memory bank. | |
| int | getPageLength () |
| Query to get page length in bytes in current memory bank. | |
| int | getMaxPacketDataLength () |
| Query to get Maximum data page length in bytes for a packet read or written in the current memory bank. | |
| boolean | hasPageAutoCRC () |
| Query to see if current memory bank pages can be read with the contents being verified by a device generated CRC. | |
| boolean | haveExtraInfo () |
| Query to see if current memory bank pages when read deliver extra information outside of the normal data space. | |
| boolean | hasExtraInfo () |
| Checks to see if this memory bank's pages deliver extra information outside of the normal data space, when read. | |
| int | getExtraInfoLength () |
| Query to get the length in bytes of extra information that is read when read a page in the current memory bank. | |
| String | getExtraInfoDescription () |
| Query to get a string description of what is contained in the Extra Informationed return when reading pages in the current memory bank. | |
| void | read (int startAddr, boolean readContinue, byte[] readBuf, int offset, int len) throws OneWireIOException, OneWireException |
| Read memory in the current bank with no CRC checking (device or data). | |
| void | write (int startAddr, byte[] writeBuf, int offset, int len) throws OneWireIOException, OneWireException |
| Write memory in the current bank. | |
| void | readPage (int page, boolean readContinue, byte[] readBuf, int offset) throws OneWireIOException, OneWireException |
| Read page in the current bank with no CRC checking (device or data). | |
| void | readPage (int page, boolean readContinue, byte[] readBuf, int offset, byte[] extraInfo) throws OneWireIOException, OneWireException |
| Read page with extra information in the current bank with no CRC checking (device or data). | |
| int | readPagePacket (int page, boolean readContinue, byte[] readBuf, int offset) throws OneWireIOException, OneWireException |
| Read a Universal Data Packet. | |
| int | readPagePacket (int page, boolean readContinue, byte[] readBuf, int offset, byte[] extraInfo) throws OneWireIOException, OneWireException |
| Read a Universal Data Packet and extra information. | |
| void | writePagePacket (int page, byte[] writeBuf, int offset, int len) throws OneWireIOException, OneWireException |
| Write a Universal Data Packet. | |
| void | readPageCRC (int page, boolean readContinue, byte[] readBuf, int offset) throws OneWireIOException, OneWireException |
| Read a complete memory page with CRC verification provided by the device. | |
| void | readPageCRC (int page, boolean readContinue, byte[] readBuf, int offset, byte[] extraInfo) throws OneWireIOException, OneWireException |
| Read a complete memory page with CRC verification provided by the device with extra information. | |
Static Public Attributes | |
| static final byte | READ_MEMORY_COMMAND = ( byte ) 0xF0 |
| Read Memory Command. | |
Protected Attributes | |
| ScratchPad | sp |
| ScratchPad memory bank. | |
| OneWireContainer | ib |
| Reference to the OneWireContainer this bank resides on. | |
| byte[] | ffBlock |
| block of 0xFF's used for faster read pre-fill of 1-Wire blocks | |
| int | size |
| Size of memory bank in bytes. | |
| String | bankDescription |
| Memory bank descriptions. | |
| boolean | generalPurposeMemory |
| Memory bank usage flags. | |
| boolean | readWrite |
| Flag if memory bank is read/write. | |
| boolean | writeOnce |
| Flag if memory bank is write once (EPROM) | |
| boolean | readOnly |
| Flag if memory bank is read only. | |
| boolean | nonVolatile |
| Flag if memory bank is non volatile (will not erase when power removed) | |
| boolean | programPulse |
| Flag if memory bank needs program Pulse to write. | |
| boolean | powerDelivery |
| Flag if memory bank needs power delivery to write. | |
| int | startPhysicalAddress |
| Starting physical address in memory bank. | |
| boolean | writeVerification |
| Flag if read back verification is enabled in 'write()'. | |
| int | numberPages |
| Number of pages in memory bank. | |
| int | pageLength |
| page length in memory bank | |
| int | maxPacketDataLength |
| Max data length in page packet in memory bank. | |
| boolean | pageAutoCRC |
| Flag if memory bank has page auto-CRC generation. | |
| boolean | extraInfo |
| Flag if reading a page in memory bank provides optional extra information (counter, tamper protection, SHA-1...) | |
| int | extraInfoLength |
| Length of extra information when reading a page in memory bank. | |
| String | extraInfoDescription |
| Extra information descriptoin when reading page in memory bank. | |
Memory bank class for the NVRAM section of iButtons and 1-Wire devices.
| MemoryBankNV | ( | OneWireContainer | ibutton, |
| ScratchPad | scratch | ||
| ) |
Memory bank contstuctor.
Requires reference to the OneWireContainer this memory bank resides on. DEFAULT: DS1993 main memory
| ibutton | ibutton container that this memory bank resides in |
| scratchPad | memory bank referece for scratchpad, used when writing |
| String getBankDescription | ( | ) |
Query to see get a string description of the current memory bank.
Implements MemoryBank.
| String getExtraInfoDescription | ( | ) |
Query to get a string description of what is contained in the Extra Informationed return when reading pages in the current memory bank.
See 'hasExtraInfo()'.
Implements PagedMemoryBank.
| int getExtraInfoLength | ( | ) |
Query to get the length in bytes of extra information that is read when read a page in the current memory bank.
See 'hasExtraInfo()'.
Implements PagedMemoryBank.
| int getMaxPacketDataLength | ( | ) |
Query to get Maximum data page length in bytes for a packet read or written in the current memory bank.
See the 'ReadPagePacket()' and 'WritePagePacket()' methods. This method is only usefull if the current memory bank is general purpose memory.
Implements PagedMemoryBank.
| int getNumberPages | ( | ) |
Query to get the number of pages in current memory bank.
Implements PagedMemoryBank.
| int getPageLength | ( | ) |
Query to get page length in bytes in current memory bank.
Implements PagedMemoryBank.
| int getSize | ( | ) |
Query to get the memory bank size in bytes.
Implements MemoryBank.
| int getStartPhysicalAddress | ( | ) |
Query to get the starting physical address of this bank.
Physical banks are sometimes sub-divided into logical banks due to changes in attributes.
Implements MemoryBank.
| boolean hasExtraInfo | ( | ) |
Checks to see if this memory bank's pages deliver extra information outside of the normal data space, when read.
Examples of this may be a redirection byte, counter, tamper protection bytes, or SHA-1 result. If this method returns true then the methods with an 'extraInfo' parameter can be used: readPage, readPageCRC, and readPagePacket.
true if reading the this memory bank's pages provides extra informationImplements PagedMemoryBank.
| boolean hasPageAutoCRC | ( | ) |
Query to see if current memory bank pages can be read with the contents being verified by a device generated CRC.
This is used to see if the 'ReadPageCRC()' can be used.
Implements PagedMemoryBank.
| boolean haveExtraInfo | ( | ) |
Query to see if current memory bank pages when read deliver extra information outside of the normal data space.
Examples of this may be a redirection byte, counter, tamper protection bytes, or SHA-1 result. If this method returns true then the methods 'ReadPagePacket()' and 'readPageCRC()' with 'extraInfo' parameter can be used.
Implements PagedMemoryBank.
| boolean isGeneralPurposeMemory | ( | ) |
Query to see if the current memory bank is general purpose user memory.
If it is NOT then it is Memory-Mapped and writing values to this memory will affect the behavior of the 1-Wire device.
Implements MemoryBank.
| boolean isNonVolatile | ( | ) |
Query to see if current memory bank non-volatile.
Memory is non-volatile if it retains its contents even when removed from the 1-Wire network.
Implements MemoryBank.
| boolean isReadOnly | ( | ) |
Query to see if current memory bank is read only.
Implements MemoryBank.
| boolean isReadWrite | ( | ) |
Query to see if current memory bank is read/write.
Implements MemoryBank.
| boolean isWriteOnce | ( | ) |
Query to see if current memory bank is write write once such as with EPROM technology.
Implements MemoryBank.
| boolean needsPowerDelivery | ( | ) |
Query to see if current memory bank pages need the adapter to have a 'PowerDelivery' feature in order to write to the memory.
Implements MemoryBank.
| boolean needsProgramPulse | ( | ) |
Query to see if current memory bank pages need the adapter to have a 'ProgramPulse' in order to write to the memory.
Implements MemoryBank.
| void read | ( | int | startAddr, |
| boolean | readContinue, | ||
| byte[] | readBuf, | ||
| int | offset, | ||
| int | len | ||
| ) | throws OneWireIOException, OneWireException |
Read memory in the current bank with no CRC checking (device or data).
The resulting data from this API may or may not be what is on the 1-Wire device. It is recommends that the data contain some kind of checking (CRC) like in the readPagePacket() method or have the 1-Wire device provide the CRC as in readPageCRC(). readPageCRC() however is not supported on all memory types, see 'hasPageAutoCRC()'. If neither is an option then this method could be called more then once to at least verify that the same thing is read consistantly.
| startAddr | starting physical address |
| readContinue | if 'true' then device read is continued without re-selecting. This can only be used if the new read() continious where the last one led off and it is inside a 'beginExclusive/endExclusive' block. |
| readBuf | byte array to place read data into |
| offset | offset into readBuf to place data |
| len | length in bytes to read |
| OneWireIOException | |
| OneWireException |
Implements MemoryBank.
Reimplemented in MemoryBankNVCRCPW.
| void readPage | ( | int | page, |
| boolean | readContinue, | ||
| byte[] | readBuf, | ||
| int | offset | ||
| ) | throws OneWireIOException, OneWireException |
Read page in the current bank with no CRC checking (device or data).
The resulting data from this API may or may not be what is on the 1-Wire device. It is recommends that the data contain some kind of checking (CRC) like in the readPagePacket() method or have the 1-Wire device provide the CRC as in readPageCRC(). readPageCRC() however is not supported on all memory types, see 'hasPageAutoCRC()'. If neither is an option then this method could be called more then once to at least verify that the same thing is read consistantly.
| page | page number to read packet from |
| readContinue | if 'true' then device read is continued without re-selecting. This can only be used if the new readPage() continious where the last one led off and it is inside a 'beginExclusive/endExclusive' block. |
| readBuf | byte array to place read data into |
| offset | offset into readBuf to place data |
| OneWireIOException | |
| OneWireException |
Implements PagedMemoryBank.
Reimplemented in MemoryBankNVCRC.
| void readPage | ( | int | page, |
| boolean | readContinue, | ||
| byte[] | readBuf, | ||
| int | offset, | ||
| byte[] | extraInfo | ||
| ) | throws OneWireIOException, OneWireException |
Read page with extra information in the current bank with no CRC checking (device or data).
The resulting data from this API may or may not be what is on the 1-Wire device. It is recommends that the data contain some kind of checking (CRC) like in the readPagePacket() method or have the 1-Wire device provide the CRC as in readPageCRC(). readPageCRC() however is not supported on all memory types, see 'hasPageAutoCRC()'. If neither is an option then this method could be called more then once to at least verify that the same thing is read consistantly. See the method 'hasExtraInfo()' for a description of the optional extra information some devices have.
| page | page number to read packet from |
| readContinue | if 'true' then device read is continued without re-selecting. This can only be used if the new readPage() continious where the last one led off and it is inside a 'beginExclusive/endExclusive' block. |
| readBuf | byte array to place read data into |
| offset | offset into readBuf to place data |
| extraInfo | byte array to put extra info read into |
| OneWireIOException | |
| OneWireException |
Implements PagedMemoryBank.
Reimplemented in MemoryBankNVCRC.
| void readPageCRC | ( | int | page, |
| boolean | readContinue, | ||
| byte[] | readBuf, | ||
| int | offset, | ||
| byte[] | extraInfo | ||
| ) | throws OneWireIOException, OneWireException |
Read a complete memory page with CRC verification provided by the device with extra information.
Not supported by all devices. See the method 'hasPageAutoCRC()'. See the method 'hasExtraInfo()' for a description of the optional extra information.
| page | page number to read |
| readContinue | if 'true' then device read is continued without re-selecting. This can only be used if the new readPagePacket() continious where the last one stopped and it is inside a 'beginExclusive/endExclusive' block. |
| readBuf | byte array to put data read. Must have at least 'getMaxPacketDataLength()' elements. |
| offset | offset into readBuf to place data |
| extraInfo | byte array to put extra info read into |
| OneWireIOException | |
| OneWireException |
Implements PagedMemoryBank.
Reimplemented in MemoryBankNVCRC, and MemoryBankNVCRCPW.
| void readPageCRC | ( | int | page, |
| boolean | readContinue, | ||
| byte[] | readBuf, | ||
| int | offset | ||
| ) | throws OneWireIOException, OneWireException |
Read a complete memory page with CRC verification provided by the device.
Not supported by all devices. See the method 'hasPageAutoCRC()'.
| page | page number to read |
| readContinue | if 'true' then device read is continued without re-selecting. This can only be used if the new readPagePacket() continious where the last one stopped and it is inside a 'beginExclusive/endExclusive' block. |
| readBuf | byte array to put data read. Must have at least 'getMaxPacketDataLength()' elements. |
| offset | offset into readBuf to place data |
| OneWireIOException | |
| OneWireException |
Implements PagedMemoryBank.
Reimplemented in MemoryBankNVCRC.
| int readPagePacket | ( | int | page, |
| boolean | readContinue, | ||
| byte[] | readBuf, | ||
| int | offset, | ||
| byte[] | extraInfo | ||
| ) | throws OneWireIOException, OneWireException |
Read a Universal Data Packet and extra information.
See the method 'readPagePacket()' for a description of the packet structure. See the method 'hasExtraInfo()' for a description of the optional extra information some devices have.
| page | page number to read packet from |
| readContinue | if 'true' then device read is continued without re-selecting. This can only be used if the new readPagePacket() continious where the last one stopped and it is inside a 'beginExclusive/endExclusive' block. |
| readBuf | byte array to put data read. Must have at least 'getMaxPacketDataLength()' elements. |
| offset | offset into readBuf to place data |
| extraInfo | byte array to put extra info read into |
| OneWireIOException | |
| OneWireException |
Implements PagedMemoryBank.
Reimplemented in MemoryBankNVCRC.
| int readPagePacket | ( | int | page, |
| boolean | readContinue, | ||
| byte[] | readBuf, | ||
| int | offset | ||
| ) | throws OneWireIOException, OneWireException |
Read a Universal Data Packet.
The Universal Data Packet always starts on page boundaries but can end anywhere in the page. The structure specifies the length of data bytes not including the length byte and the CRC16 bytes. There is one length byte. The CRC16 is first initialized to the page number. This provides a check to verify the page that was intended is being read. The CRC16 is then calculated over the length and data bytes. The CRC16 is then inverted and stored low byte first followed by the high byte. This is structure is used by this method to verify the data but is not returned, only the data payload is returned.
| page | page number to read packet from |
| readContinue | if 'true' then device read is continued without re-selecting. This can only be used if the new readPagePacket() continious where the last one stopped and it is inside a 'beginExclusive/endExclusive' block. |
| readBuf | byte array to put data read. Must have at least 'getMaxPacketDataLength()' elements. |
| offset | offset into readBuf to place data |
| OneWireIOException | |
| OneWireException |
Implements PagedMemoryBank.
| void setWriteVerification | ( | boolean | doReadVerf | ) |
Set the write verification for the 'write()' method.
| doReadVerf | true (default) verify write in 'write' false, don't verify write (used on Write-Once bit manipulation) |
Implements MemoryBank.
| void write | ( | int | startAddr, |
| byte[] | writeBuf, | ||
| int | offset, | ||
| int | len | ||
| ) | throws OneWireIOException, OneWireException |
Write memory in the current bank.
It is recommended that when writing data that some structure in the data is created to provide error free reading back with read(). Or the method 'writePagePacket()' could be used which automatically wraps the data in a length and CRC.
When using on Write-Once devices care must be taken to write into into empty space. If write() is used to write over an unlocked page on a Write-Once device it will fail. If write verification is turned off with the method 'setWriteVerification(false)' then the result will be an 'AND' of the existing data and the new data.
| startAddr | starting address |
| writeBuf | byte array containing data to write |
| offset | offset into writeBuf to get data |
| len | length in bytes to write |
| OneWireIOException | |
| OneWireException |
Implements MemoryBank.
Reimplemented in MemoryBankNVCRCPW.
| void writePagePacket | ( | int | page, |
| byte[] | writeBuf, | ||
| int | offset, | ||
| int | len | ||
| ) | throws OneWireIOException, OneWireException |
Write a Universal Data Packet.
See the method 'readPagePacket()' for a description of the packet structure.
| page | page number to write packet to |
| writeBuf | data byte array to write |
| offset | offset into writeBuf where data to write is |
| len | number of bytes to write |
| OneWireIOException | |
| OneWireException |
Implements PagedMemoryBank.
int startPhysicalAddress [protected] |
Starting physical address in memory bank.
Needed for different types of memory in the same logical memory bank. This can be used to seperate them into two virtual memory banks. Example: DS2406 status page has mixed EPROM and Volatile RAM.
1.7.3