This is the complete list of members for
MemoryBankEEPROMstatus, including all inherited members.
| bankDescription | MemoryBankEEPROMstatus | [protected] |
| CHANNEL_ACCESS_WRITE | MemoryBankEEPROMstatus | [static] |
| checkSpeed() | MemoryBankEEPROMstatus | |
| COPY_SCRATCHPAD_COMMAND | MemoryBankEEPROMstatus | [static] |
| copyScratchpad(byte[] es_data) | MemoryBankEEPROMstatus | |
| doSetSpeed | MemoryBankEEPROMstatus | [protected] |
| ffBlock | MemoryBankEEPROMstatus | [protected] |
| forceVerify() | MemoryBankEEPROMstatus | |
| generalPurposeMemory | MemoryBankEEPROMstatus | [protected] |
| getBankDescription() | MemoryBankEEPROMstatus | |
| getExtraInfoDescription() | MemoryBankEEPROMstatus | |
| getExtraInfoLength() | MemoryBankEEPROMstatus | |
| getMaxPacketDataLength() | MemoryBankEEPROMstatus | |
| getNumberPages() | MemoryBankEEPROMstatus | |
| getPageLength() | MemoryBankEEPROMstatus | |
| getSize() | MemoryBankEEPROMstatus | |
| getStartPhysicalAddress() | MemoryBankEEPROMstatus | |
| hasExtraInfo() | MemoryBankEEPROMstatus | |
| hasPageAutoCRC() | MemoryBankEEPROMstatus | |
| ib | MemoryBankEEPROMstatus | [protected] |
| isGeneralPurposeMemory() | MemoryBankEEPROMstatus | |
| isNonVolatile() | MemoryBankEEPROMstatus | |
| isReadOnly() | MemoryBankEEPROMstatus | |
| isReadWrite() | MemoryBankEEPROMstatus | |
| isWriteOnce() | MemoryBankEEPROMstatus | |
| maxPacketDataLength | MemoryBankEEPROMstatus | [protected] |
| MemoryBankEEPROMstatus(OneWireContainer ibutton) | MemoryBankEEPROMstatus | |
| needsPowerDelivery() | MemoryBankEEPROMstatus | |
| needsProgramPulse() | MemoryBankEEPROMstatus | |
| nonVolatile | MemoryBankEEPROMstatus | [protected] |
| numberPages | MemoryBankEEPROMstatus | [protected] |
| pageAutoCRC | MemoryBankEEPROMstatus | [protected] |
| pageLength | MemoryBankEEPROMstatus | [protected] |
| powerDelivery | MemoryBankEEPROMstatus | [protected] |
| programPulse | MemoryBankEEPROMstatus | [protected] |
| read(int startAddr, boolean readContinue, byte[] readBuf, int offset, int len) | MemoryBankEEPROMstatus | |
| READ_MEMORY_COMMAND | MemoryBankEEPROMstatus | [static] |
| READ_SCRATCHPAD_COMMAND | MemoryBankEEPROMstatus | [static] |
| readOnly | MemoryBankEEPROMstatus | [protected] |
| readScratchpad(byte[] readBuf, int offset, int len, byte[] es_data) | MemoryBankEEPROMstatus | |
| readWrite | MemoryBankEEPROMstatus | [protected] |
| setWriteVerification(boolean doReadVerf) | MemoryBankEEPROMstatus | |
| size | MemoryBankEEPROMstatus | [protected] |
| startPhysicalAddress | MemoryBankEEPROMstatus | [protected] |
| write(int startAddr, byte[] writeBuf, int offset, int len) | MemoryBankEEPROMstatus | |
| WRITE_SCRATCHPAD_COMMAND | MemoryBankEEPROMstatus | [static] |
| writeOnce | MemoryBankEEPROMstatus | [protected] |
| writeScratchpad(int addr, byte[] out_buf, int offset, int len) | MemoryBankEEPROMstatus | |
| writeVerification | MemoryBankEEPROMstatus | [protected] |