|
1-Wire API for .NET Version 4.00
|
This class provides a default object for the Thermal type of a tagged 1-Wire device. More...
Inherits com::dalsemi::onewire::application::tag::TaggedDevice, and com::dalsemi::onewire::application::tag::TaggedSensor.
Public Member Functions | |
| Thermal () | |
| Creates an object for the device. | |
| Thermal (DSPortAdapter adapter, String netAddress) | |
| Creates an object for the device with the supplied address and device type connected to the supplied port adapter. | |
| String | readSensor () throws OneWireException |
| The readSensor method returns a temperature in degrees Celsius. | |
This class provides a default object for the Thermal type of a tagged 1-Wire device.
| Thermal | ( | DSPortAdapter | adapter, |
| String | netAddress | ||
| ) |
Creates an object for the device with the supplied address and device type connected to the supplied port adapter.
| adapter | The adapter serving the sensor. |
| netAddress | The 1-Wire network address of the sensor. |
| String readSensor | ( | ) | throws OneWireException |
The readSensor method returns a temperature in degrees Celsius.
| . |
1.7.3