|
1-Wire API for .NET Version 4.00
|
Public Member Functions | |
| SAXParser () | |
| Construct the SAX parser. | |
| void | setLocale (Locale locale) throws SAXException |
| Set the locale for errors and warnings. | |
| void | setEntityResolver (EntityResolver resolver) |
| Register a custom entity resolver. | |
| void | setDTDHandler (DTDHandler handler) |
| Register a DTD event handler. | |
| void | setDocumentHandler (DocumentHandler handler) |
| Register a document event handler. | |
| void | setErrorHandler (ErrorHandler handler) |
| Register an error event handler. | |
| void | parse (InputSource inputSource) throws SAXException, IOException |
| Parse an XML document. | |
| void | parse (String systemID) throws SAXException, IOException |
| Parse an XML document specified by system identifier or URL. | |
A SAX parser.
This class encapsulates the underlying parser implementation. We support only the SAX1 interface for now.
Specify the SAXParser implementation by adding the property SAXParser.ClassName to the onewire.properties file with the fully qualified classname of an implementation of org.xml.sax.Parser. The default classname used is for nanoxml's parser: nanoxml.sax.SAXParser.
| void parse | ( | InputSource | inputSource | ) | throws SAXException, IOException |
Parse an XML document.
| source | Source of the document to parse. |
| inputSource |
| SAXException | Any SAX exception, possibly wrapping another exception. |
| IOException | If an I/O error occurred while reading the document. |
| void parse | ( | String | systemID | ) | throws SAXException, IOException |
Parse an XML document specified by system identifier or URL.
| systemID | The system ID or URL of the document to parse. |
| SAXException | Any SAX exception, possibly wrapping another exception. |
| IOException | If an I/O error occurred while reading the document. |
| void setDocumentHandler | ( | DocumentHandler | handler | ) |
Register a document event handler.
If one is not registered, all document events reported by the parser will be ignored.
| handler | The document handler to use. |
| void setDTDHandler | ( | DTDHandler | handler | ) |
Register a DTD event handler.
If one is not registered, all DTD events reported by the parser will be ignored.
| handler | The DTD handler to use. |
| void setEntityResolver | ( | EntityResolver | resolver | ) |
Register a custom entity resolver.
If one is not registered, the parser will resolve system identifiers in an implementation dependent way.
| resolver | The entity resolver to use. |
| void setErrorHandler | ( | ErrorHandler | handler | ) |
Register an error event handler.
If one is not registered, all error events except for fatalError are ignored. A fatalError thorws a org.xml.sax.SAXException.
| handler | The error handler to use. |
| void setLocale | ( | Locale | locale | ) | throws SAXException |
Set the locale for errors and warnings.
| locale | The locale to use. |
| SAXException | If the locale is not supported. |
1.7.3