|
1-Wire API for .NET Version 4.00
|
This class provides a default object for the Level type of a tagged 1-Wire device. More...
Inherits com::dalsemi::onewire::application::tag::TaggedDevice, and com::dalsemi::onewire::application::tag::TaggedSensor.
Public Member Functions | |
| Level () | |
| Creates an object for the device. | |
| Level (DSPortAdapter adapter, String netAddress) | |
| Creates an object for the device with the supplied address and device type connected to the supplied port adapter. | |
| String | readSensor () throws OneWireException |
| The readSensor method returns the <max> or <min> string of the Sensor (in this case, a switch). | |
This class provides a default object for the Level type of a tagged 1-Wire device.
| Level | ( | DSPortAdapter | adapter, |
| String | netAddress | ||
| ) |
Creates an object for the device with the supplied address and device type connected to the supplied port adapter.
| adapter | The adapter serving the sensor. |
| netAddress | The 1-Wire network address of the sensor. |
| String readSensor | ( | ) | throws OneWireException |
The readSensor method returns the <max> or <min> string of the Sensor (in this case, a switch).
The elements <max> and <min> represent conducting and non-conducting states of the switch, respectively.
| . |
1.7.3