|
1-Wire API for .NET Version 4.00
|
This class provides a default object for the Event type of a tagged 1-Wire device. More...
Inherits com::dalsemi::onewire::application::tag::TaggedDevice, and com::dalsemi::onewire::application::tag::TaggedSensor.
Public Member Functions | |
| Event () | |
| Creates an object for the device. | |
| Event (DSPortAdapter adapter, String netAddress) | |
| Creates an object for the device with the supplied address and device type connected to the supplied port adapter. | |
| String | readSensor () throws OneWireException |
| The readSensor method returns the "max" string if the Sensor (a switch) has had activity since last time it was checked for activity. | |
This class provides a default object for the Event type of a tagged 1-Wire device.
| Event | ( | DSPortAdapter | adapter, |
| String | netAddress | ||
| ) |
Creates an object for the device with the supplied address and device type connected to the supplied port adapter.
| adapter | The adapter serving the sensor. |
| netAddress | The 1-Wire network address of the sensor. |
| String readSensor | ( | ) | throws OneWireException |
The readSensor method returns the "max" string if the Sensor (a switch) has had activity since last time it was checked for activity.
| . |
1.7.3