Public Member Functions |
| | SHAiButtonCoprVM (byte[] RomID, int l_signPageNumber, int l_authPageNumber, int l_wspcPageNumber, int l_version, int l_encCode, byte l_serviceFileExt, byte[] l_serviceFilename, byte[] l_providerName, byte[] l_bindData, byte[] l_bindCode, byte[] l_auxData, byte[] l_initialSignature, byte[] l_signingChlg, byte[] l_signingSecret, byte[] l_authSecret) throws OneWireException, OneWireIOException |
| | SHAiButtonCoprVM (String filename) throws OneWireException, OneWireIOException |
| | SHAiButtonCoprVM (String filename, byte[] sign_secret, byte[] auth_secret) throws OneWireException, OneWireIOException |
| | SHAiButtonCoprVM (OneWireContainer owc, String filename) throws OneWireException, OneWireIOException |
| | SHAiButtonCoprVM (OneWireContainer owc, String filename, byte[] sign_secret, byte[] auth_secret) throws OneWireException, OneWireIOException |
| | SHAiButtonCoprVM (OneWireContainer18 owc, String filename, byte[] sign_secret, byte[] auth_secret) throws OneWireException, OneWireIOException |
| boolean | save (String filename, boolean saveSecretData) throws OneWireException, OneWireIOException |
| boolean | save (OneWireContainer owc, String filename, boolean saveSecretData) throws OneWireException, OneWireIOException |
| boolean | load (String filename) |
| boolean | load (OneWireContainer owc, String filename) |
| boolean | load (OneWireContainer18 owc, String filename) |
| boolean | createDataSignature (byte[] accountData, byte[] signScratchpad, byte[] mac_buffer, int macStart) throws OneWireException, OneWireIOException |
| synchronized boolean | generateChallenge (int offset, byte[] ch, int start) throws OneWireIOException, OneWireException |
| boolean | verifyAuthentication (byte[] fullBindCode, byte[] pageData, byte[] scratchpad, byte[] verify_mac, byte authCmd) throws OneWireIOException, OneWireException |
| boolean | createDataSignatureAuth (byte[] accountData, byte[] signScratchpad, byte[] mac_buffer, int macStart, byte[] fullBindCode) throws OneWireException, OneWireIOException |
| boolean | verifySignature (byte[] pageData, byte[] scratchpad, byte[] verify_mac) throws OneWireIOException, OneWireException |
| synchronized boolean | bindSecretToiButton (int pageNum, byte[] bindData, byte[] bindCode, int secretNum) |
| boolean | installMasterSecret (int pageNum, byte[] secret, int secretNum) |
| String | toString () |
| | Returns a string representing the 1-Wire address of this SHAiButton.
|
Protected Attributes |
|
byte[][] | secretPage = new byte[8][8] |
| | 8 8-byte Secrets for this simulated SHAiButton
|
|
byte[] | address = new byte[8] |
| | 1-Wire Address for this simulated device
|
Class for simulating an instance of a SHA iButton Coprocessor involved in SHA Transactions. The Coprocessor is used for digitally signing transaction data as well as generating random challenges for users and verifying their response.
With this class, no DS1963S SHA iButton is necessary for the coprocessor in SHA Transactions. The simulated Coprocessor iButton verifies signatures and signs data for User iButtons.
This class makes use of several performance enhancements for TINI. For instance, most methods are synchronized to access instance variable byte arrays rather than creating new byte arrays every time a transaction is performed. This could hurt performance in multi-threaded applications, but the usefulness of having several threads contending to talk to a single iButton is questionable since the methods in com.dalsemi.onewire.adapter.DSPortAdapter beginExclusive(boolean) and endExclusive() should be used.
- See also:
- SHATransaction
-
SHAiButtonUser
-
SHAiButtonCopr
- Version:
- 1.00
- Author:
- SKH
| synchronized boolean bindSecretToiButton |
( |
int |
pageNum, |
|
|
byte[] |
bindData, |
|
|
byte[] |
bindCode, |
|
|
int |
secretNum |
|
) |
| |
Binds an installed secret to this virtual DS1963S by using well-known binding data and this DS1963S's (unique?) address. This makes the secret unique for this iButton. Coprocessor iButtons use this method to recreate the iButton's secret to verify authentication. Roving iButtons use this method to finalize their secret keys.
Note that unlike in the installMasterSecret() method, the page number does not need to be equivalent to the secret_number modulo 8. The new secret (installed secret + binding code) is generated from this page but can be copied into another secret. User iButtons should bind to the same page the secret was installed on. Coprocessor iButtons must copy to a new secret to preserve the general system authentication secret.
The binding should be either 7 bytes long or 15 bytes long. A 15-length byte array is unaltered and placed in the scratchpad for the binding. A 7-length byte array is combined with the page number and DS1963S unique address and then placed in the scratchpad. Coprocessors should use a pre-formatted 15-length byte array. User iButtons should let the method format for them (i.e. use the 7-length byte array option).
- Parameters:
-
| page | the page number that has the master secret already installed |
| bind_data | 32 bytes of binding data used to bind the iButton to the system |
| bind_code | the 7-byte or 15-byte binding code |
| secret_number | secret number to copy the resulting secret to |
- Returns:
true if successful
- See also:
- installMasterSecret(int,byte[],int)
Given a 32-byte array for page data and a 32-byte array for scratchpad content, this function will create a 20-byte signature for the data based on SHA-1. The format of the calculation of the data signature is as follows: First 4-bytes of signing secret, 32-bytes of accountData, 12 bytes of scratchpad data starting at index 8, last 4-bytes of signing secret, 3 bytes of scratchpad data starting at index 20, and the rest is padding as specified for standard SHA-1. This is all laid out, in detail, in the DS1963S data sheet.
The resulting 20-byte signature is copied into mac_buffer starting at macStart. If you're updating a signature that already exists in the accountData array, it is acceptable to call the method like so:
copr.createDataSignature(accountData, spad, accountData, 8);
assuming that the signature starts at index 8 of the accountData array.
- Parameters:
-
| accountData | the 32-byte data page for which the signature is generated. |
| signScratchpad | the 32-byte scratchpad contents for which the signature is generated. This will contain parameters such as the user's write cycle counter for the page, the user's 1-wire address, and the page number where account data is stored. |
| mac_buffer | used to return the 20-byte signature generated by signing the page using the coprocessor's system signing secret. |
| macStart | the offset into mac_buffer where copying should start. |
- Returns:
true if successful, false if an error occurred (use getLastError() for more information on the type of error)
- Exceptions:
-
| OneWireIOException | on a 1-Wire communication error such as reading an incorrect CRC from a 1-Wire device. This could be caused by a physical interruption in the 1-Wire Network due to shorts or a newly arriving 1-Wire device issuing a 'presence pulse'. |
| OneWireException | on a communication or setup error with the 1-Wire adapter |
- See also:
- OneWireContainer18.SHAFunction(byte,int)
-
#getLastError()
| boolean createDataSignatureAuth |
( |
byte[] |
accountData, |
|
|
byte[] |
signScratchpad, |
|
|
byte[] |
mac_buffer, |
|
|
int |
macStart, |
|
|
byte[] |
fullBindCode |
|
) |
| throws OneWireException, OneWireIOException |
Creates a data signature, but instead of using the signing secret, it uses the authentication secret, bound for a particular button.
fullBindCode is ignored by the Coprocessor VM. Instead of binding the secret to the signing page, the coprocessor VM "cheats" and lets you sign the workspace page, where (presumably) the secret is already bound.
- Parameters:
-
| accountData | the 32-byte data page for which the signature is generated. |
| signScratchpad | the 32-byte scratchpad contents for which the signature is generated. This will contain parameters such as the user's write cycle counter for the page, the user's 1-wire address, and the page number where account data is stored. |
| mac_buffer | used to return the 20-byte signature generated by signing the page using the coprocessor's system signing secret. |
| macStart | the offset into mac_buffer where copying should start. |
| fullBindCode | ignored by simulated coprocessor |
- Returns:
true if successful, false if an error occurred (use getLastError() for more information on the type of error)
- Exceptions:
-
| OneWireIOException | on a 1-Wire communication error such as reading an incorrect CRC from a 1-Wire device. This could be caused by a physical interruption in the 1-Wire Network due to shorts or a newly arriving 1-Wire device issuing a 'presence pulse'. |
| OneWireException | on a communication or setup error with the 1-Wire adapter |
- See also:
- OneWireContainer18.SHAFunction(byte,int)
-
createDataSignature(byte[],byte[],byte[],int)
-
#getLastError()
Generates a 3 byte random challenge in the iButton, sufficient to be used as a challenge to be answered by a User iButton. The user answers the challenge with an authenticated read of it's account data.
The DS1963S will generate 20 bytes of pseudo random data, though only 3 bytes are needed for the challenge. Programs can add more 'randomness' by selecting different bytes from the 20 bytes of random data using the offset parameter.
The random number generator is actually the DS1963S's SHA engine, which requires page data to compute a hash. Select a page number with the page_number parameter.
- Parameters:
-
| offset | offset into the 20 random bytes to draw random data from (must be in range 0-16) |
| ch | buffer for the challenge to be returned (must be of length 3 or more) |
| start | the starting index into array ch to begin copying the challenge bytes. |
- Returns:
true if successful, false if an error occurred (use getLastError() for more information on the type of error)
- Exceptions:
-
| OneWireIOException | on a 1-Wire communication error such as reading an incorrect CRC from a 1-Wire device. This could be caused by a physical interruption in the 1-Wire Network due to shorts or a newly arriving 1-Wire device issuing a 'presence pulse'. |
| OneWireException | on a communication or setup error with the 1-Wire adapter |
- See also:
- SHAiButtonUser.readAccountData(byte[],int,byte[],int,byte[],int)
-
#getLastError()
| boolean installMasterSecret |
( |
int |
pageNum, |
|
|
byte[] |
secret, |
|
|
int |
secretNum |
|
) |
| |
Installs a secret on this virtual DS1963S. The secret is written in partial phrases of 47 bytes (32 bytes to a memory page, 15 bytes to the scratchpad) and is cumulative until the entire secret is processed. Secrets are associated with a page number. See the datasheet for more information on this association.
In most cases, page should be equal to secret_number or secret_number+8, based on the association of secrets and page numbers. A secret is 8 bytes and there are 8 secrets. These 8 secrets are associated with the first 16 pages of memory.
On TINI, this method will be slightly faster if the secret's length is divisible by 47. However, since secret key generation is a part of initialization, it is probably not necessary.
- Parameters:
-
| page | the page number used to write the partial secrets to |
| secret | the entire secret to be installed |
| secret_number | the secret 'page' to use (0 - 7) |
- Returns:
true if successful
- See also:
- bindSecretToiButton(int,byte[],byte[],int)
Determines if a SHAiButtonUser belongs to the system defined by this Coprocessor iButton.See the usage example in this class for initializing a Coprocessor iButton.
The first step in user authentication is to recreate the user's unique secret on the coprocessor button using bindSecretToiButton(int,byte[],byte[],int). Then the coprocessor signs the pageData to produce a MAC. If the MAC matches that produced by the user, the user belongs to the system.
The TMEX formatted page with the user's account data is in the 32-byte parameter pageData. If the verification is successful, the data data signature must still be verified with the verifySignature() method.
Failure of this method does not necessarily mean that the User iButton does not belong to the system. It is possible that a communication disruption here could cause a CRC error that would be indistinguishable from a failed authentication. However, repeated attempts should reveal whether it was truly a communication problem or a User iButton that does not belong to the system.
- Parameters:
-
| fullBindCode | 15-byte binding code used to recreate user iButtons unique secret in the coprocessor. |
| pageData | 32-byte buffer containing the data page holding the user's account data. |
| scratchpad | the 32-byte scratchpad contents for which the signature is generated. This will contain parameters such as the user's write cycle counter for the page, the user's 1-wire address, and the page number where account data is stored. |
| verify_mac | the 20-byte buffer containing the user's authentication response to the coprocessor's challenge. |
- Returns:
true if the operation was successful and the user's MAC matches that generated by the coprocessor.
- Exceptions:
-
| OneWireIOException | on a 1-Wire communication error such as reading an incorrect CRC from a 1-Wire device. This could be caused by a physical interruption in the 1-Wire Network due to shorts or a newly arriving 1-Wire device issuing a 'presence pulse'. |
| OneWireException | on a communication or setup error with the 1-Wire adapter |
- See also:
- generateChallenge(int,byte[],int)
-
verifySignature(byte[],byte[],byte[])
-
bindSecretToiButton(int,byte[],byte[],int)
-
OneWireContainer18.SHAFunction(byte,int)
-
OneWireContainer18.matchScratchPad(byte[])
-
#getLastError()