|
1-Wire API for .NET Version 4.00
|
Inherited by SHAiButtonCoprVM.
Public Member Functions | |
| SHAiButtonCopr (OneWireContainer18 l_owc, String coprFilename, boolean l_formatDevice, int l_signPageNumber, int l_authPageNumber, int l_wspcPageNumber, int l_version, int l_encCode, byte l_serviceFileExt, byte[] l_serviceFilename, byte[] l_providerName, byte[] l_bindData, byte[] l_bindCode, byte[] l_auxData, byte[] l_initialSignature, byte[] l_signingChlg, byte[] l_signingSecret, byte[] l_authSecret) throws OneWireException, OneWireIOException | |
| SHAiButtonCopr (OneWireContainer18 owc, String coprFilename) throws OneWireException, OneWireIOException | |
Protected Member Functions | |
| SHAiButtonCopr () | |
Protected Attributes | |
| int | lastError |
| Last error code raised. | |
| OneWireContainer18 | ibc = null |
| Reference to the OneWireContainer. | |
| byte[] | address = null |
| Cache of 1-Wire Address. | |
| int | authPageNumber = -1 |
| Page used for generating user authentication secret. | |
| String | auxData |
| Any auxilliary data stored on this coprocessor. | |
| byte[] | bindCode = new byte [7] |
| 7 bytes of binding data for scratchpad to bind secret installation | |
| byte[] | bindData = new byte [32] |
| 32 bytes of binding data to bind secret installation | |
| boolean | DS1961Scompatible = false |
| Specifies whether or not this coprocessor is compatible with the DS1961S. | |
| int | encCode = -1 |
| Code used to specify encryption type. | |
| byte[] | filename = new byte[5] |
| Filename, including extension, for user's service file. | |
| byte[] | initialSignature = new byte [20] |
| 20 byte initial signature, used for signing user account data | |
| String | providerName |
| The Provider name of the coprocessor's service. | |
| byte[] | signingChallenge = new byte [3] |
| 3 byte challenge, used for signing user account data | |
| int | signPageNumber = 8 |
| Page used for signing user account data. | |
| int | version = -1 |
| Code used to specify encryption type. | |
| int | wspcPageNumber = -1 |
| Page used for generating user's validation MAC. | |
Static Package Attributes | |
| static final boolean | DEBUG = false |
| Turns on extra debugging output. | |
Class for holding instances of SHA iButton Coprocessors involved in SHA Transactions. The Coprocessor is used for digitally signing transaction data as well as generating random challenges for users and verifying their response.
A DS1963S SHA iButton can be a SHAiButtonCopr or a SHAiButtonUser. A Coprocessor iButton verifiessignatures and signs data for User iButtons. A Coprocessor might be located inside a vending machine, where a person would bring their User iButton. When the User iButton is pressed to the Blue Dot to perform a transaction, the Coprocessor would first verify that this button belongs to the system, i.e. that it knows the same authentication secret (example: a Visa terminal making sure the iButton had a Visa account installed). Then the Coprocessor would verify the signed data, probably money, to make sure it was valid. If someone tried to overwrite the money file, even with a previously valid money file (an attempt to 'restore' a previous amount of money), the signed file would be invalid because the signature includes the write cycle counter, which is incremented every time a page is written to. The write cycle counter is read-only and does not roll over, so the previous amount of money could not be restored by rolling the write counter. The Coprocessor verifies the money, then signs a new data file that contains the new amount of money.
There are two secrets involved with the transaction process. The first secret is the authentication secret. It is used to validate a User iButton to a system. The Coprocessor iButton has the system authentication secret installed. On User iButtons, the system authentication secret is merged with binding data and the unique address of the User iButton to create a unique device authentication secret. The second secret is a signing secret. This secret only exists on the Coprocessor iButton, and is used to sign and verify transaction data (i.e. money). These secrets are inaccessible outside the iButton. Once they are installed, they cannot be retrieved.
This class makes use of several performance enhancements for TINI. For instance, most methods are synchronized to access instance variable byte arrays rather than creating new byte arrays every time a transaction is performed. This could hurt performance in multi-threaded applications, but the usefulness of having several threads contending to talk to a single iButton is questionable since the methods in com.dalsemi.onewire.adapter.DSPortAdapter beginExclusive(boolean) and endExclusive() should be used.
| SHAiButtonCopr | ( | ) | [protected] |
No default construct for user apps. Coprocessors, unlike users, are immutable classes, so there is no setiButton for User applications.
| SHAiButtonCopr | ( | OneWireContainer18 | l_owc, |
| String | coprFilename, | ||
| boolean | l_formatDevice, | ||
| int | l_signPageNumber, | ||
| int | l_authPageNumber, | ||
| int | l_wspcPageNumber, | ||
| int | l_version, | ||
| int | l_encCode, | ||
| byte | l_serviceFileExt, | ||
| byte[] | l_serviceFilename, | ||
| byte[] | l_providerName, | ||
| byte[] | l_bindData, | ||
| byte[] | l_bindCode, | ||
| byte[] | l_auxData, | ||
| byte[] | l_initialSignature, | ||
| byte[] | l_signingChlg, | ||
| byte[] | l_signingSecret, | ||
| byte[] | l_authSecret | ||
| ) | throws OneWireException, OneWireIOException |
Sets up this coprocessor object based on the provided parameters and saves all of these parameters as the contents of the file coprFilename stored on owc. Then, the system secret and authentication secret are installed on the coprocessor button.
For the proper format of the coprocessor data file, see the document entitled "Implementing Secured D-Identification and E-Payment Applications using SHA iButtons". For the format of TMEX file structures, see Application Note 114.
| l_owc | The DS1963S used as a coprocessor. |
| coprFilename | The TMEX filename where coprocessor configuration data is stored. Usually, "COPR.0". |
| l_formatDevice | boolean indicating whether or not the TMEX filesystem of this device should be formatted before the coprocessor data file is stored. |
| l_signPageNumber | page number used for signing user account data. (Should be page 8, but page 0 is acceptable if you don't need the TMEX directory structure) |
| l_authPageNumber | page number used for recreating user secret. |
| l_wspcPageNumber | page number used for storing user secret and recreating authentication MAC. |
| l_version | version of the service provided by this coprocessor. |
| l_encCode | refers to a type of encryption used for user account data stored on user buttons. |
| l_serviceFileExt | the file extension used for the service file. (An extension of decimal 102 is reserved for Money files). |
| l_serviceFilename | the 4-byte name of the user's account data file. |
| l_providerName | the name of the provider of this service |
| l_bindData | the binding data used to finalize secret installation on user buttons. |
| l_bindCode | the binding code used to finalize secret installation on user buttons. |
| l_auxData | any auxilliary or miscellaneous data to be stored on the coprocessor. |
| l_initialSignature | the 20-byte initial MAC placed in user account data before generating actual MAC. |
| l_signingChlg | the 3-byte challenge used for signing user account data. |
| l_signingSecret | the system signing secret used by the service being installed on this coprocessor. |
| l_authSecret | the system authentication secret used by the service being installed on this coprocessor. |
| OneWireIOException | on a 1-Wire communication error such as reading an incorrect CRC from a 1-Wire device. This could be caused by a physical interruption in the 1-Wire Network due to shorts or a newly arriving 1-Wire device issuing a 'presence pulse'. |
| OneWireException | on a communication or setup error with the 1-Wire adapter |
| SHAiButtonCopr | ( | OneWireContainer18 | owc, |
| String | coprFilename | ||
| ) | throws OneWireException, OneWireIOException |
Sets up this coprocessor object based on the contents of the file coprFilename stored on owc. This sets all the properties of the object as a consequence of what's in the coprocessor file.
For the proper format of the coprocessor data file, see the document entitled "Implementing Secured D-Identification and E-Payment Applications using SHA iButtons". For the format of TMEX file structures, see Application Note 114.
| owc | The DS1963S used as a coprocessor |
| coprFilename | The TMEX filename where coprocessor configuration data is stored. Usually, "COPR.0". |
| OneWireIOException | on a 1-Wire communication error such as reading an incorrect CRC from a 1-Wire device. This could be caused by a physical interruption in the 1-Wire Network due to shorts or a newly arriving 1-Wire device issuing a 'presence pulse'. |
| OneWireException | on a communication or setup error with the 1-Wire adapter |
boolean DS1961Scompatible = false [protected] |
Specifies whether or not this coprocessor is compatible with the DS1961S.
This entails the use of a specifically padded authentication secret.
1.7.3