|
1-Wire API for .NET Version 4.00
|
Represents an encapsulated exception from a particular Device Monitor. More...
Inherits java::lang::Exception.
Public Member Functions | |
| AbstractDeviceMonitor | getMonitor () |
| Returns the monitor which generated this event. | |
| DSPortAdapter | getAdapter () |
| Returns DSPortAdapter the monitor was using when the event was generated. | |
| Exception | getException () |
| Returns the wrapped exception that was generated during a 1-Wire search. | |
| void | throwException () throws Exception |
| Throws the wrapped exception to the calling object. | |
| String | toString () |
| Converts this object to a String. | |
Protected Attributes | |
| AbstractDeviceMonitor | deviceMonitor = null |
| The monitor which generated the event. | |
| DSPortAdapter | adapter = null |
| The DSPortAdapter the monitor was using at the time of event. | |
| Exception | exception |
| The exception that was generated by the search. | |
Package Functions | |
| DeviceMonitorException (AbstractDeviceMonitor deviceMonitor, DSPortAdapter adapter, Exception exception) | |
| Creates a new DeviceMonitor event with the specified characteristics. | |
Represents an encapsulated exception from a particular Device Monitor.
The state of this exception includes the device monitor object from which the exception was thrown, the DSPortAdapter object that was being used by the monitor, and the exact exception that was thrown.
| DeviceMonitorException | ( | AbstractDeviceMonitor | deviceMonitor, |
| DSPortAdapter | adapter, | ||
| Exception | exception | ||
| ) | [package] |
Creates a new DeviceMonitor event with the specified characteristics.
| source | The monitor which generated the exception |
| adapter | The DSPortAdapter the monitor was using |
| exception | The actual exception which was thrown |
| DSPortAdapter getAdapter | ( | ) |
Returns DSPortAdapter the monitor was using when the event was generated.
| Exception getException | ( | ) |
Returns the wrapped exception that was generated during a 1-Wire search.
| AbstractDeviceMonitor getMonitor | ( | ) |
Returns the monitor which generated this event.
| String toString | ( | ) |
Converts this object to a String.
1.7.3